Balance White#
为此,可以对每个色彩通道(红、绿、蓝色)应用数字增益校正。
要自动纠正色彩偏移,请使用 Balance White Auto 功能。
该功能的使用#
为什么要执行白平衡校正#
相机采集到的图像可能出现偏色,即特定颜色的色调。其原因是不同的光源具有不同的色温。荧光灯会给图像增加偏蓝的色调,而钨丝白炽灯则会增加偏黄的色调。
白平衡功能使您可以通过调整红、绿、蓝色的强度来校正这些色彩偏移。使得白色物体在采集到的图像中呈现白色。
执行白平衡校正#
执行白平衡校正:
- Set the Balance White Auto auto function to
Off
. - 为了获得最佳效果,请在将黑电平设置为 0(零)。
- Set the
BalanceRatioSelector
parameter to one of the available color channels (Red
,Green
, orBlue
). -
Adjust the
BalanceRatio
parameter value for the selected color channel:- 平衡率 = 1:颜色强度保持不变。
- 平衡率 > 1:相对于其他两种颜色,颜色强度增大。
- Balance ratio < 1: The intensity of the color is decreased relative to the other two colors. (This is only possible if your camera model supports balance ratio values lower than 1.)
- 对所有可用的颜色通道重复步骤 3 和 4。
强度成比例增大或降低。例如,如果将一种颜色的平衡率设置为 1.2,则该颜色的强度将增加 20%。
信息
- 如果指定的平衡率小于 1,也会降低色彩可以达到的最大强度。除非要校正一种明显占优势的颜色,否则建议不要将平衡率指定为小于 1 的值。
- 一些色彩增强功能,例如 Light Source Preset 或 Color Transformation 也会影响白平衡设置。如有必要,可以在使用这些功能后手动重新调整白平衡。
外部链接#
示例代码#
ace Classic/U/L GigE 相机#
// Set the red intensity to 108.789%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Red);
camera.BalanceRatioAbs.SetValue(1.08789);
// Set the green intensity to 100%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Green);
camera.BalanceRatioAbs.SetValue(1.0);
// Set the blue intensity to 219.678%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Blue);
camera.BalanceRatioAbs.SetValue(2.19678);
INodeMap& nodemap = camera.GetNodeMap();
// Set the red intensity to 108.789%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Red");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(1.08789);
// Set the green intensity to 100%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Green");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(1.0);
// Set the blue intensity to 219.678%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Blue");
CFloatParameter(nodemap, "BalanceRatioAbs").SetValue(2.19678);
// Set the red intensity to 108.789%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Red);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(1.08789);
// Set the green intensity to 100%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Green);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(1.0);
// Set the blue intensity to 219.678%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Blue);
camera.Parameters[PLCamera.BalanceRatioAbs].SetValue(2.19678);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the red intensity to 108.789% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Red");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 1.08789);
CHECK(errRes);
/* Set the green intensity to 100% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Green");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 1.0);
CHECK(errRes);
/* Set the blue intensity to 219.678% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Blue");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatioAbs", 2.19678);
CHECK(errRes);
# Set the red intensity to 108.789%
camera.BalanceRatioSelector.Value = "Red"
camera.BalanceRatioAbs.Value = 1.08789
# Set the green intensity to 100%
camera.BalanceRatioSelector.Value = "Green"
camera.BalanceRatioAbs.Value = 1.0
# Set the blue intensity to 219.678%
camera.BalanceRatioSelector.Value = "Blue"
camera.BalanceRatioAbs.Value = 2.19678
其他相机#
// Set the red intensity to 108.789%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Red);
camera.BalanceRatio.SetValue(1.08789);
// Set the green intensity to 100%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Green);
camera.BalanceRatio.SetValue(1.0);
// Set the blue intensity to 219.678%
camera.BalanceRatioSelector.SetValue(BalanceRatioSelector_Blue);
camera.BalanceRatio.SetValue(2.19678);
INodeMap& nodemap = camera.GetNodeMap();
// Set the red intensity to 108.789%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Red");
CFloatParameter(nodemap, "BalanceRatio").SetValue(1.08789);
// Set the green intensity to 100%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Green");
CFloatParameter(nodemap, "BalanceRatio").SetValue(1.0);
// Set the blue intensity to 219.678%
CEnumParameter(nodemap, "BalanceRatioSelector").SetValue("Blue");
CFloatParameter(nodemap, "BalanceRatio").SetValue(2.19678);
// Set the red intensity to 108.789%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Red);
camera.Parameters[PLCamera.BalanceRatio].SetValue(1.08789);
// Set the green intensity to 100%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Green);
camera.Parameters[PLCamera.BalanceRatio].SetValue(1.0);
// Set the blue intensity to 219.678%
camera.Parameters[PLCamera.BalanceRatioSelector].SetValue(PLCamera.BalanceRatioSelector.Blue);
camera.Parameters[PLCamera.BalanceRatio].SetValue(2.19678);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the red intensity to 108.789% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Red");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 1.08789);
CHECK(errRes);
/* Set the green intensity to 100% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Green");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 1.0);
CHECK(errRes);
/* Set the blue intensity to 219.678% */
errRes = PylonDeviceFeatureFromString(hdev, "BalanceRatioSelector", "Blue");
CHECK(errRes);
errRes = PylonDeviceSetFloatFeature(hdev, "BalanceRatio", 2.19678);
CHECK(errRes);
# Set the red intensity to 108.789%
camera.BalanceRatioSelector.Value = "Red"
camera.BalanceRatio.Value = 1.08789
# Set the green intensity to 100%
camera.BalanceRatioSelector.Value = "Green"
camera.BalanceRatio.Value = 1.0
# Set the blue intensity to 219.678%
camera.BalanceRatioSelector.Value = "Blue"
camera.BalanceRatio.Value = 2.19678
您也可以使用 pylon Viewer 轻松设置参数。