Counter#
该功能的使用#
The implementation of this feature varies by camera series:
ace 2, boost R, dart M/R, and racer 2 Cameras#
运作原理#
Depending on your camera model, up to three counters are available: Counter 1, Counter 2, and Counter 3.
每个计数器都具有以下特征:
- 从 0 开始。
- 必须先启动才能计数。
- 一旦启动,就可以对特定类型的事件(即“事件源”)进行计数。例如,它可以对已曝光的图像数量进行计数。
- 可以随时重置为 0。
- Its current value can be determined by getting the value of the
CounterValue
parameter. - Its maximum value is defined by the
CounterDuration
parameter value (default: 4 294 967 295). After reaching the maximum value, the counter stops counting and must be reset. - Its current status can be determined by getting the value of the
CounterStatus
parameter. - 每次关闭相机电源后再次打开电源时,它将重置为 0。
获取计数器值#
To determine the current value of a counter, get the value of the CounterValue
parameter. This parameter is read-only.
启动计数器#
要启动计数器,请执行以下操作:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterTriggerSource
parameter to the source that you want to use to start the counter, e.g.,Line2
. - 如果适用,请设置
CounterTriggerActivation
参数设置为以下值:RisingEdge
(default): The counter starts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter starts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter starts when the signal falls or rises.LevelHigh
: The counter starts when the signal is high. When the signal changes to low, the counter status is set toCounterTriggerWait
and must be started again.LevelLow
: The counter starts when the signal is low. When the signal changes to high, the counter status is set toCounterTriggerWait
and must be started again.
- 通过在选定的计数器触发源上发送信号来启动计数器。
When started, the counter's status changes from CounterTriggerWait
to CounterActive
.
信息
- 如果您启动了一个计数器,它不一定会开始计数。计数器是否以及何时计数取决于事件源集。
- The
CounterTriggerActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal likeExposureActive
.
增加计数器计数#
计数器一旦启动,就可以开始增加计数器的数字,也就是可以开始计数。
要增加计数器,请执行以下操作:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterEventSource
parameter to the source that you want to use to increase the counter, e.g.,Line2
. - 如果适用,请设置
CounterEventActivation
参数设置为以下值:RisingEdge
(default): The counter counts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter counts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter counts when the signal falls or rises.
- Set the
CounterDuration
parameter to the desired maximum value. - 通过在选定的计数器事件源上发送信号来增加计数器。
只要相机在所选信号源上检测到信号,计时器就会增加,直至达到定义的最大值。
信息
The CounterEventActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
重置计数器#
您可以随时将计数器重置为 0。
You must reset the counter if it has reached its maximum value (defined by the CounterDuration
parameter value) and you want to reuse it.
通过软件重置#
To reset a counter by software, execute the CounterReset
command.
您也可以将软件信号设置为重置源(请参见下文)。
使用重置源重置#
The CounterResetSource
parameter allows you to specify which source resets the counter.
要使用重置源重置计数器,请执行以下操作:
- Set the
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - Set the
CounterResetSource
parameter to the source that you want to use to reset the counter, e.g.,Line2
. - 如果适用,请设置
CounterResetActivation
参数设置为以下值:RisingEdge
(default): The counter resets when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter resets when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter resets when the signal falls or rises.
- 通过在选定的计数器重置源上发送信号来重置计数器。
When reset, the counter's status changes to CounterTriggerWait
and must be started again.
信息
The CounterResetActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
停止计数器#
要停止计数器,请执行以下任一操作:
获取计数器状态#
To get the current status of a counter, get the value of the CounterStatus
parameter. This parameter is read-only.
可能的值包括:
CounterTriggerWait
: The counter is waiting to be started.CounterActive
: The counter is waiting to be increased by the selected event source or is currently counting.CounterCompleted
: The counter has reached its maximum value defined by theCounterDuration
parameter.CounterIdle
: The counter is idle. A counter is in this state whenever theCounterTriggerSource
parameter is set toOff
, i.e., the counter can't be started.
ace Classic/U/L 相机#
运作原理#
有两个计数器可用:Counter 1 和 Counter 2。
除一种例外情况(见下文)以外,每个计数器都具有以下特征:
- 从 0 开始。
- 对特定类型的事件(即“事件源”)进行计数。例如,它会对所获取的图像数量进行计数。事件源是预设的,无法更改。
- 可以通过检索相关数据块(例如帧 Counter 块)来确定其当前值。
- 其最大值为 4 294 967 295。达到最大值后,计数器将重置为 0,然后继续计数。
- 可以手动重置。
- 每次关闭相机电源后再次打开电源时,它将重置为 0。
例外:在部分相机机型上,Counter 2 可用于控制定序器。该计数器由于其特定用途而具有不同的特征。
获取计数器值#
要确定计数器的当前值,使用 Data Chunks 功能获取相关数据块。
重置计数器#
重置计数器:
Set the CounterSelector
parameter to the desired counter, e.g., Counter2
.
Set the CounterResetSource
parameter to a software source (Software
) or to a hardware source (e.g., Line1
).
根据在步骤 2 中选择的源,执行以下操作:
- If you set a software source, execute the
CounterReset
command. - 如果设置了硬件信号源,则向相机的任一输入线路施加电信号。
附加参数#
- The
CounterEventSource
parameter allows you to get the event source of the currently selected counter, i.e., determine in which case the counter increases. - The
CounterResetActivation
parameter currently serves no function. It is preset toRisingEdge
. This means that if the counter is configured for hardware reset, the counter resets when the hardware trigger signal rises.
详情#
相机型号 | 可用计数器 | 功能 | 事件源 | 相关数据块 | 可以重置 |
---|---|---|---|---|---|
a2A640-240gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A640-240umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1280-80gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1280-125umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-165g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-165g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2048-35gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2048-110umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2440-98g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2440-98g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-105g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-105g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-120cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-120cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-210cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-210cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2560-20gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2560-70umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5mUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-86cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-86cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-44g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-44g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-67cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-67cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-27g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-27g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-42cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-42cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-34g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-34g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-52cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-52cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-22g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-22g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-35cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-35cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
acA640-121gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-300gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-300gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-750uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA640-750um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA720-290gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA720-290gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA720-520uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA720-520um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA800-200gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA800-200gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA800-510uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA800-510um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1280-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1280-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gmNIR | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-75gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-75gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-200uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1300-200um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1440-73gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1440-73gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1440-220uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1440-220um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1600-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1600-20uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1600-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1600-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-25um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-40gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-40uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-48gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-48gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-50gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-50gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-150uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-150um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2000-50gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2000-50gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2000-165uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2000-165um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-25gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-25gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-25gmNIR | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-35gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-35gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-55uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-55um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90umNIR | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-120uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-120um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2440-20gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2440-35uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-14gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-14gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-14uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-14um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gcMED | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gmMED | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-60uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-60um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-16gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3088-16gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3088-57uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3800-10gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3800-10gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3800-14uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3800-14um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4024-8gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4024-8gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4024-29uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4024-29um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-11gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4096-11gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4096-30uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-8gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4112-8gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4112-20uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-5gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA5472-5gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA5472-17uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
boA1936-400cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA1936-400cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA2448-250cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo2448-250cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA2832-190cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo2832-190cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-93cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-93cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-180cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo4096-180cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4112-68cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4112-68cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4500-45cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4500-45cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4504-100cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4504-100cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5120-150cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-150cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-230cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-230cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5320-150cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5320-150cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5328-100cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5328-100cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA6500-36cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA6500-36cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA8100-16cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA8100-16cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA9344-30cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-30cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-70cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-70cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA13440-17cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA720-520uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA720-520um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1280-54uc | 不支持 Counter 功能 | – | – | – | – |
daA1280-54um | 不支持 Counter 功能 | – | – | – | – |
daA1440-220uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1440-220um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1600-60uc | 不支持 Counter 功能 | – | – | – | – |
daA1600-60um | 不支持 Counter 功能 | – | – | – | – |
daA1920-15um | 不支持 Counter 功能 | – | – | – | – |
daA1920-30uc | 不支持 Counter 功能 | – | – | – | – |
daA1920-30um | 不支持 Counter 功能 | – | – | – | – |
daA1920-160uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1920-160um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2448-70uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2448-70um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2500-14uc | 不支持 Counter 功能 | – | – | – | – |
daA2500-14um | 不支持 Counter 功能 | – | – | – | – |
daA3840-45uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA3840-45um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA720-290gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA720-290gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1440-73gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1440-73gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1920-51gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1920-51gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
puA1280-54uc | 不支持 Counter 功能 | – | – | – | – |
puA1280-54um | 不支持 Counter 功能 | – | – | – | – |
puA1600-60uc | 不支持 Counter 功能 | – | – | – | – |
puA1600-60um | 不支持 Counter 功能 | – | – | – | – |
puA1920-30uc | 不支持 Counter 功能 | – | – | – | – |
puA1920-30um | 不支持 Counter 功能 | – | – | – | – |
puA2500-14uc | 不支持 Counter 功能 | – | – | – | – |
puA2500-14um | 不支持 Counter 功能 | – | – | – | – |
r2L2048-29gc | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-58gm | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-62cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L2048-62g5c | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-172cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L2048-172g5m | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-14gc | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-29gm | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-42cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L4096-42g5c | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-84cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L4096-84g5m | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L8192-200cm | Counter 1 Counter 2 Counter 3 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
r2L16384-120cm | Counter 1 Counter 2 Counter 3 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
示例代码#
ace 2, boost R, dart M/R, and racer 2 Cameras#
// Select Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.SetValue(CounterTriggerSource_SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.SetValue(CounterEventSource_Line1);
camera.CounterEventActivation.SetValue(CounterEventActivation_RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.SetValue(CounterResetSource_Line2);
camera.CounterResetActivation.SetValue(CounterEventActivation_FallingEdge);
// Set the maximum value of the counter to 1000
camera.CounterDuration.SetValue(1000);
// Manually reset the counter
camera.CounterReset.Execute();
// Get the current status of the counter
CounterStatusEnums counterStatus = camera.CounterStatus.GetValue();
// Get the current value of the counter
int64_t i = camera.CounterValue.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
// Specify that the counter starts when a software signal is sent via channel 1
CEnumParameter(nodemap, "CounterTriggerSource").SetValue("SoftwareSignal1");
// Specify that the counter increases whenever a rising signal is detected on Line 1
CEnumParameter(nodemap, "CounterEventSource").SetValue("Line1");
CEnumParameter(nodemap, "CounterEventActivation").SetValue("RisingEdge");
// Specify that the counter is reset whenever a falling signal is detected on Line 2
CEnumParameter(nodemap, "CounterResetSource").SetValue("Line2");
CEnumParameter(nodemap, "CounterResetActivation").SetValue("FallingEdge");
// Set the maximum value of the counter to 1000
CIntegerParameter(nodemap, "CounterDuration").SetValue(1000);
// Manually reset the counter
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the current status of the counter
String_t counterStatus = CEnumParameter(nodemap, "CounterStatus").GetValue();
// Get the current value of the counter
int64_t i = CIntegerParameter(nodemap, "CounterValue").GetValue();
// Select Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.Parameters[PLCamera.CounterTriggerSource].SetValue(PLCamera.CounterTriggerSource.SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.Parameters[PLCamera.CounterEventSource].SetValue(PLCamera.CounterEventSource.Line1);
camera.Parameters[PLCamera.CounterEventActivation].SetValue(PLCamera.CounterEventActivation.RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Line2);
camera.Parameters[PLCamera.CounterResetActivation].SetValue(PLCamera.CounterEventActivation.FallingEdge);
// Set the maximum value of the counter to 1000
camera.Parameters[PLCamera.CounterDuration].SetValue(1000);
// Manually reset the counter
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the current status of the counter
string counterStatus = camera.Parameters[PLCamera.CounterStatus].GetValue();
// Get the current value of the counter
Int64 i = camera.Parameters[PLCamera.CounterValue].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char counterStatus_str[64] = {0};
int64_t i = 0;
/* Select Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
/* Specify that the counter starts when a software signal is sent via channel 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterTriggerSource", "SoftwareSignal1");
CHECK(errRes);
/* Specify that the counter increases whenever a rising signal is detected on Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventSource", "Line1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventActivation", "RisingEdge");
CHECK(errRes);
/* Specify that the counter is reset whenever a falling signal is detected on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Line2");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetActivation", "FallingEdge");
CHECK(errRes);
/* Set the maximum value of the counter to 1000 */
errRes = PylonDeviceSetIntegerFeature(hdev, "CounterDuration", 1000);
CHECK(errRes);
/* Manually reset the counter */
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the current status of the counter */
len = sizeof(counterStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterStatus", counterStatus_str, &len);
CHECK(errRes);
/* Get the current value of the counter */
errRes = PylonDeviceGetIntegerFeature(hdev, "CounterValue", &i);
CHECK(errRes);
# Select Counter 1
camera.CounterSelector.Value = "Counter1"
# Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.Value = "SoftwareSignal1"
# Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.Value = "Line1"
camera.CounterEventActivation.Value = "RisingEdge"
# Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.Value = "Line2"
camera.CounterResetActivation.Value = "FallingEdge"
# Set the maximum value of the counter to 1000
camera.CounterDuration.Value = 1000
# Manually reset the counter
camera.CounterReset.Execute()
# Get the current status of the counter
counterStatus = camera.CounterStatus.Value
# Get the current value of the counter
i = camera.CounterValue.Value
ace Classic/U/L 相机#
// Reset Counter 1 via software command
camera.CounterSelector.SetValue(CounterSelector_Counter1);
camera.CounterResetSource.SetValue(CounterResetSource_Software);
camera.CounterReset.Execute();
// Get the event source of Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
CounterEventSourceEnums e = camera.CounterEventSource.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Reset Counter 1 via software command
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
CEnumParameter(nodemap, "CounterResetSource").SetValue("Software");
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the event source of Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
String_t e = CEnumParameter(nodemap, "CounterEventSource").GetValue();
// Reset Counter 1 via software command
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Software);
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the event source of Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
string e = camera.Parameters[PLCamera.CounterEventSource].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Reset Counter 1 via software command */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Software");
CHECK(errRes);
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the event source of Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterEventSource", e_str, &len);
CHECK(errRes);
您也可以使用 pylon Viewer 轻松设置参数。