Counter#
该功能的使用#
The implementation of this feature varies by camera series:
ace 2, boost R, dart M/R, and racer 2 Cameras#
运作原理#
Depending on your camera model, up to three counters are available: Counter 1, Counter 2, and Counter 3.
每个计数器都具有以下特征:
- 从 0 开始。
- 必须先启动才能计数。
- 一旦启动,就可以对特定类型的事件(即“事件源”)进行计数。例如,它可以对已曝光的图像数量进行计数。
- 可以随时重置为 0。
- Its current value can be determined by getting the value of the
CounterValue
parameter. - Its maximum value is defined by the
CounterDuration
parameter value (default: 4 294 967 295). After reaching the maximum value, the counter stops counting and must be 重置. - Its current status can be determined by getting the value of the
CounterStatus
parameter. - 每次关闭相机电源后再次打开电源时,它将重置为 0。
获取计数器值#
To determine the current value of a counter, get the value of the CounterValue
parameter. This parameter is read-only.
启动计数器#
要启动计数器,请执行以下操作:
- 设置
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - 设置
CounterTriggerSource
parameter to the source that you want to use to start the counter, e.g.,Line2
. - 如果适用,请设置
CounterTriggerActivation
参数设置为以下值:RisingEdge
(default): The counter starts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter starts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter starts when the signal falls or rises.LevelHigh
: The counter starts when the signal is high. When the signal changes to low, the counter status is set toCounterTriggerWait
and must be started again.LevelLow
: The counter starts when the signal is low. When the signal changes to high, the counter status is set toCounterTriggerWait
and must be started again.
- 通过在选定的计数器触发源上发送信号来启动计数器。
When started, the counter's status changes from CounterTriggerWait
to CounterActive
.
信息
- 如果您启动了一个计数器,它不一定会开始计数。计数器是否以及何时计数取决于事件源集。
- 即:
CounterTriggerActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal likeExposureActive
.
增加计数器计数#
计数器一旦启动,就可以开始增加计数器的数字,也就是可以开始计数。
要增加计数器,请执行以下操作:
- 设置
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - 设置
CounterEventSource
parameter to the source that you want to use to increase the counter, e.g.,Line2
. - 如果适用,请设置
CounterEventActivation
参数设置为以下值:RisingEdge
(default): The counter counts when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter counts when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter counts when the signal falls or rises.
- 设置
CounterDuration
parameter to the desired maximum value. - 通过在选定的计数器事件源上发送信号来增加计数器。
只要相机在所选信号源上检测到信号,计时器就会增加,直至达到定义的最大值。
信息
即: CounterEventActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
重置计数器#
您可以随时将计数器重置为 0。
You must reset the counter if it has reached its maximum value (defined by the CounterDuration
parameter value) and you want to reuse it.
通过软件重置#
To reset a counter by software, execute the CounterReset
command.
您也可以将软件信号设置为重置源(请参见下文)。
使用重置源重置#
即: CounterResetSource
parameter allows you to specify which source resets the counter.
要使用重置源重置计数器,请执行以下操作:
- 设置
CounterSelector
parameter to the desired counter, e.g.,Counter2
. - 设置
CounterResetSource
parameter to the source that you want to use to reset the counter, e.g.,Line2
. - 如果适用,请设置
CounterResetActivation
参数设置为以下值:RisingEdge
(default): The counter resets when the signal rises, i.e., when the signal status changes from low to high.FallingEdge
: The counter resets when the signal falls, i.e., when the signal status changes from high to low.AnyEdge
: The counter resets when the signal falls or rises.
- 通过在选定的计数器重置源上发送信号来重置计数器。
When reset, the counter's status changes to CounterTriggerWait
and must be started again.
信息
即: CounterResetActivation
parameter is only available for event sources that can be high (1) or low (0), i.e., an I/O signal or an "Active" signal like ExposureActive
.
停止计数器#
要停止计数器,请执行以下任一操作:
获取计数器状态#
To get the current status of a counter, get the value of the CounterStatus
parameter. This parameter is read-only.
可能的值包括:
CounterTriggerWait
: The counter is waiting to be started.CounterActive
: The counter is waiting to be increased by the selected event source or is currently counting.CounterCompleted
: The counter has reached its maximum value defined by theCounterDuration
parameter.CounterIdle
: The counter is idle. A counter is in this state whenever theCounterTriggerSource
parameter is set to熄灭
, i.e., the counter can't be started.
ace Classic/U/L 相机#
运作原理#
有两个计数器可用:Counter 1 和 Counter 2。
除一种例外情况(见下文)以外,每个计数器都具有以下特征:
- 从 0 开始。
- 对特定类型的事件(即“事件源”)进行计数。例如,它会对所获取的图像数量进行计数。事件源是预设的,无法更改。
- 可以通过检索相关数据块(例如帧 Counter 块)来确定其当前值。
- 其最大值为 4 294 967 295。达到最大值后,计数器将重置为 0,然后继续计数。
- 可以手动重置。
- 每次关闭相机电源后再次打开电源时,它将重置为 0。
例外:在部分相机机型上,Counter 2 可用于控制定序器。该计数器由于其特定用途而具有不同的特征。
获取计数器值#
要确定计数器的当前值,使用 Data Chunks 功能获取相关数据块。
重置计数器#
重置计数器:
设置 CounterSelector
parameter to the desired counter, e.g., Counter2
.
设置 CounterResetSource
parameter to a software source (软件
) or to a hardware source (e.g., Line1
).
根据在步骤 2 中选择的源,执行以下操作:
- If you set a software source, execute the
CounterReset
command. - 如果设置了硬件信号源,则向相机的任一输入线路施加电信号。
附加参数#
- 即:
CounterEventSource
parameter allows you to get the event source of the currently selected counter, i.e., determine in which case the counter increases. - 即:
CounterResetActivation
parameter currently serves no function. It is preset toRisingEdge
. This means that if the counter is configured for hardware reset, the counter resets when the hardware trigger signal rises.
详情#
相机型号 | 可用计数器 | 功能 | 事件源 | 相关数据块 | 可以重置 |
---|---|---|---|---|---|
a2A640-240gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A640-240umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1280-80gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1280-125umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-51gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-160umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-165g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A1920-165g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2048-35gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2048-110umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2440-98g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2440-98g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-23gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-75umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-105g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-105g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-120cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-120cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-210cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2448-210cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2560-20gmSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2560-70umSWIR | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-22gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2590-60umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-20gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2600-64umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-14gmUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-48umUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-67g5mUV | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-86cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A2840-86cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-13gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A3840-45umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-9gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-30umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-44g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-44g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-67cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4096-67cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-12gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4200-40umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-5gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-18umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-27g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-27g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-42cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4504-42cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-6gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A4508-20umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-7gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-23umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-34g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-34g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-52cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5320-52cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gcBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gcPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gmBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-4gmPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15ucBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15ucPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15umBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-15umPRO | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-22g5cBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-22g5mBAS | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-35cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
a2A5328-35cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
acA640-121gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-300gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-300gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA640-750uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA640-750um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA720-290gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA720-290gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA720-520uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA720-520um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA800-200gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA800-200gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA800-510uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA800-510um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1280-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1280-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-60gmNIR | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-75gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-75gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1300-200uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1300-200um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1440-73gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1440-73gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1440-220uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1440-220um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1600-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1600-20uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1600-60gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1600-60gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-25uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-25um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-40gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-40uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-40umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-48gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-48gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-50gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-50gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA1920-150uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-150um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA1920-155umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2000-50gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2000-50gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2000-165uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2000-165um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-25gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-25gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-25gmNIR | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-35gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-35gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2040-55uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-55um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-90umNIR | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-120uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2040-120um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2440-20gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2440-35uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-35umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2440-75umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-14gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-14gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-14uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-14um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-20gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gcMED | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-20gmMED | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA2500-60uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA2500-60um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-16gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3088-16gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3088-57uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3088-57umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3800-10gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3800-10gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA3800-14uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA3800-14um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4024-8gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4024-8gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4024-29uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4024-29um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-11gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4096-11gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4096-30uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-30umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4096-40umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-8gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4112-8gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA4112-20uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-20umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA4112-30umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-5gc | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA5472-5gm | Counter 1 Counter 2 | Counter 1:计算接收到的硬件帧开始触发信号的数量,无论它们是否导致了图像采集 Counter 2:计算采集到的图像数 | Counter 1:帧触发 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:是 |
acA5472-17uc | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17ucMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17um | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
acA5472-17umMED | Counter 1 Counter 2 | Counter 1:计算采集的图像数量 Counter 2:可用于控制定序器 | Counter 1:帧开始 Counter 2:帧开始 | Counter 1:触发输入计数器块 Counter 2:帧计数器块 | Counter 1:是 Counter 2:否 |
boA1936-400cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA1936-400cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA2448-250cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo2448-250cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA2832-190cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo2832-190cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-93cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-93cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4096-180cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
bo4096-180cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4112-68cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4112-68cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4500-45cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4500-45cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4504-100cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA4504-100cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5120-150cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-150cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-230cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5120-230cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA5320-150cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5320-150cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5328-100cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA5328-100cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA6500-36cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA6500-36cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA8100-16cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA8100-16cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
boA9344-30cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-30cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-70cc | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA9344-70cm | 无 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 | 不支持 Counter 功能 |
boA13440-17cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA720-520uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA720-520um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1280-54uc | 不支持 Counter 功能 | – | – | – | – |
daA1280-54um | 不支持 Counter 功能 | – | – | – | – |
daA1440-220uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1440-220um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1600-60uc | 不支持 Counter 功能 | – | – | – | – |
daA1600-60um | 不支持 Counter 功能 | – | – | – | – |
daA1920-15um | 不支持 Counter 功能 | – | – | – | – |
daA1920-30uc | 不支持 Counter 功能 | – | – | – | – |
daA1920-30um | 不支持 Counter 功能 | – | – | – | – |
daA1920-160uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA1920-160um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2448-70uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2448-70um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA2500-14uc | 不支持 Counter 功能 | – | – | – | – |
daA2500-14um | 不支持 Counter 功能 | – | – | – | – |
daA3840-45uc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
daA3840-45um | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA720-290gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA720-290gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1440-73gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1440-73gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1920-51gc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
dmA1920-51gm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
puA1280-54uc | 不支持 Counter 功能 | – | – | – | – |
puA1280-54um | 不支持 Counter 功能 | – | – | – | – |
puA1600-60uc | 不支持 Counter 功能 | – | – | – | – |
puA1600-60um | 不支持 Counter 功能 | – | – | – | – |
puA1920-30uc | 不支持 Counter 功能 | – | – | – | – |
puA1920-30um | 不支持 Counter 功能 | – | – | – | – |
puA2500-14uc | 不支持 Counter 功能 | – | – | – | – |
puA2500-14um | 不支持 Counter 功能 | – | – | – | – |
r2L2048-29gc | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-58gm | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-62cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L2048-62g5c | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L2048-172cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L2048-172g5m | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-14gc | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-29gm | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-42cc | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L4096-42g5c | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L4096-84cm | Counter 1 Counter 2 | 可配置 | 可配置 | 不适用 | Counter 1:是 Counter 2:是 |
r2L4096-84g5m | Counter 1 Counter 2 Counter 3 Counter 4 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes Counter 4: Yes |
r2L8192-200cm | Counter 1 Counter 2 Counter 3 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
r2L16384-120cm | Counter 1 Counter 2 Counter 3 | 可配置 | 可配置 | 不适用 | Counter 1: Yes Counter 2: Yes Counter 3: Yes |
示例代码#
ace 2, boost R, dart M/R, and racer 2 Cameras#
// Select Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.SetValue(CounterTriggerSource_SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.SetValue(CounterEventSource_Line1);
camera.CounterEventActivation.SetValue(CounterEventActivation_RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.SetValue(CounterResetSource_Line2);
camera.CounterResetActivation.SetValue(CounterEventActivation_FallingEdge);
// Set the maximum value of the counter to 1000
camera.CounterDuration.SetValue(1000);
// Manually reset the counter
camera.CounterReset.Execute();
// Get the current status of the counter
CounterStatusEnums counterStatus = camera.CounterStatus.GetValue();
// Get the current value of the counter
int64_t i = camera.CounterValue.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
// Specify that the counter starts when a software signal is sent via channel 1
CEnumParameter(nodemap, "CounterTriggerSource").SetValue("SoftwareSignal1");
// Specify that the counter increases whenever a rising signal is detected on Line 1
CEnumParameter(nodemap, "CounterEventSource").SetValue("Line1");
CEnumParameter(nodemap, "CounterEventActivation").SetValue("RisingEdge");
// Specify that the counter is reset whenever a falling signal is detected on Line 2
CEnumParameter(nodemap, "CounterResetSource").SetValue("Line2");
CEnumParameter(nodemap, "CounterResetActivation").SetValue("FallingEdge");
// Set the maximum value of the counter to 1000
CIntegerParameter(nodemap, "CounterDuration").SetValue(1000);
// Manually reset the counter
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the current status of the counter
String_t counterStatus = CEnumParameter(nodemap, "CounterStatus").GetValue();
// Get the current value of the counter
int64_t i = CIntegerParameter(nodemap, "CounterValue").GetValue();
// Select Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
// Specify that the counter starts when a software signal is sent via channel 1
camera.Parameters[PLCamera.CounterTriggerSource].SetValue(PLCamera.CounterTriggerSource.SoftwareSignal1);
// Specify that the counter increases whenever a rising signal is detected on Line 1
camera.Parameters[PLCamera.CounterEventSource].SetValue(PLCamera.CounterEventSource.Line1);
camera.Parameters[PLCamera.CounterEventActivation].SetValue(PLCamera.CounterEventActivation.RisingEdge);
// Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Line2);
camera.Parameters[PLCamera.CounterResetActivation].SetValue(PLCamera.CounterEventActivation.FallingEdge);
// Set the maximum value of the counter to 1000
camera.Parameters[PLCamera.CounterDuration].SetValue(1000);
// Manually reset the counter
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the current status of the counter
string counterStatus = camera.Parameters[PLCamera.CounterStatus].GetValue();
// Get the current value of the counter
Int64 i = camera.Parameters[PLCamera.CounterValue].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char counterStatus_str[64] = {0};
int64_t i = 0;
/* Select Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
/* Specify that the counter starts when a software signal is sent via channel 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterTriggerSource", "SoftwareSignal1");
CHECK(errRes);
/* Specify that the counter increases whenever a rising signal is detected on Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventSource", "Line1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterEventActivation", "RisingEdge");
CHECK(errRes);
/* Specify that the counter is reset whenever a falling signal is detected on Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Line2");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetActivation", "FallingEdge");
CHECK(errRes);
/* Set the maximum value of the counter to 1000 */
errRes = PylonDeviceSetIntegerFeature(hdev, "CounterDuration", 1000);
CHECK(errRes);
/* Manually reset the counter */
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the current status of the counter */
len = sizeof(counterStatus_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterStatus", counterStatus_str, &len);
CHECK(errRes);
/* Get the current value of the counter */
errRes = PylonDeviceGetIntegerFeature(hdev, "CounterValue", &i);
CHECK(errRes);
# Select Counter 1
camera.CounterSelector.Value = "Counter1"
# Specify that the counter starts when a software signal is sent via channel 1
camera.CounterTriggerSource.Value = "SoftwareSignal1"
# Specify that the counter increases whenever a rising signal is detected on Line 1
camera.CounterEventSource.Value = "Line1"
camera.CounterEventActivation.Value = "RisingEdge"
# Specify that the counter is reset whenever a falling signal is detected on Line 2
camera.CounterResetSource.Value = "Line2"
camera.CounterResetActivation.Value = "FallingEdge"
# Set the maximum value of the counter to 1000
camera.CounterDuration.Value = 1000
# Manually reset the counter
camera.CounterReset.Execute()
# Get the current status of the counter
counterStatus = camera.CounterStatus.Value
# Get the current value of the counter
i = camera.CounterValue.Value
ace Classic/U/L 相机#
// Reset Counter 1 via software command
camera.CounterSelector.SetValue(CounterSelector_Counter1);
camera.CounterResetSource.SetValue(CounterResetSource_Software);
camera.CounterReset.Execute();
// Get the event source of Counter 1
camera.CounterSelector.SetValue(CounterSelector_Counter1);
CounterEventSourceEnums e = camera.CounterEventSource.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Reset Counter 1 via software command
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
CEnumParameter(nodemap, "CounterResetSource").SetValue("Software");
CCommandParameter(nodemap, "CounterReset").Execute();
// Get the event source of Counter 1
CEnumParameter(nodemap, "CounterSelector").SetValue("Counter1");
String_t e = CEnumParameter(nodemap, "CounterEventSource").GetValue();
// Reset Counter 1 via software command
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
camera.Parameters[PLCamera.CounterResetSource].SetValue(PLCamera.CounterResetSource.Software);
camera.Parameters[PLCamera.CounterReset].Execute();
// Get the event source of Counter 1
camera.Parameters[PLCamera.CounterSelector].SetValue(PLCamera.CounterSelector.Counter1);
string e = camera.Parameters[PLCamera.CounterEventSource].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Reset Counter 1 via software command */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "CounterResetSource", "Software");
CHECK(errRes);
errRes = PylonDeviceExecuteCommandFeature(hdev, "CounterReset");
CHECK(errRes);
/* Get the event source of Counter 1 */
errRes = PylonDeviceFeatureFromString(hdev, "CounterSelector", "Counter1");
CHECK(errRes);
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "CounterEventSource", e_str, &len);
CHECK(errRes);
您也可以使用 pylon Viewer 轻松设置参数。