- Global DEPRECATED (Sgc_DirectRegisterWriteMemWithTimeOut(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, const unsigned char *data, const uint32_t buflen, uint32_t timeoutInMilliseconds))
this function is replaced by Sgc_DirectRegisterWriteMemWithTimeOut64
- Global DEPRECATED (Sgc_DirectRegisterReadMemWithTimeOut(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, unsigned char *data, uint32_t *buflen, uint32_t timeoutInMilliseconds))
this function is replaced by Sgc_DirectRegisterReadMemWithTimeOut64()
- Global DEPRECATED (Sgc_DirectRegisterWrite(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, const uint32_t data, const unsigned int switchByteOrder))
this function is replaced by Sgc_DirectRegisterWrite64()
- Global DEPRECATED (Sgc_DirectRegisterRead(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, uint32_t *data))
this function is replaced by Sgc_DirectRegisterRead64()
- Global DEPRECATED (Sgc_CxpDisconnect(SgcCameraHandle *cameraHandle))
this function is replaced by Sgc_LinkDisconnect()
- Global DEPRECATED (Sgc_CxpConnect(SgcBoardHandle *boardHandle, SgcCameraHandle *cameraHandle))
this function is replaced by Sgc_LinkConnect()
- Global DEPRECATED (Sgc_DirectRegisterWriteMem(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, const unsigned char *data, const uint32_t buflen))
this function is replaced by Sgc_DirectRegisterWriteMem64()
- Global DEPRECATED (Sgc_DirectRegisterReadMem(SgcBoardHandle *boardHandle, const unsigned int port, const uint32_t address, unsigned char *data, uint32_t *buflen))
Use Sgc_DirectRegisterReadMem64
- Global Fg_setExsync (Fg_Struct *Fg, int Flag, const unsigned int CamPort)
This function internally calls Fg_setParameter() with parameter FG_EXSYNCON and passes Flag as value. You should use that interface as this has slightly less overhead.
- Global Fg_setFlash (Fg_Struct *Fg, int Flag, const unsigned int CamPort)
This function internally calls Fg_setParameter() with parameter FG_FLASHON and passes Flag as value. You should use that interface as this has slightly less overhead.
- Global getLastErrorNumber ()
- This function is only here to maintain interface compatibility. It will only call Fg_getLastErrorNumber(NULL) internally. Do not use it as it will eventually go away.
- Global IoOpenImage (const char *filename)
In new code you should use IoImageOpen() as this does the same operation but returns an error code if what went wrong.
- Global IoOpenImageExt (const char *filename, unsigned char **data, int *width, int *height, int *bits)
In new code you should use IoImageOpen() and query the image settings by the appropiate functions.
- Global PN_MICROENABLE4BASE
- old name for PN_MICROENABLE4AD1CL, maintained only for source compatibility
- Global PN_MICROENABLE4BASEx4
- name for a prototype never used
- Global PN_MICROENABLE4FULLx1
- old name for PN_MICROENABLE4VD1CL, maintained only for source compatibility
- Global PN_MICROENABLE4FULLx4
- old name for PN_MICROENABLE4VD4CL, maintained only for source compatibility
- Global PN_MICROENABLE4GIGEx4
- old name for PN_MICROENABLE4VQ4GE, maintained only for source compatibility
- Global PN_MICROENABLE5_ABACUS_4G
- old name for PN_MICROENABLE5_ABACUS_4G_PROTOTYPE, maintained only for source compatibility
- Global PN_MICROENABLE5AQ8CXP4
- old name for PN_MICROENABLE5AQ8CXP6B, maintained only for source compatibility
- Global PN_MICROENABLE5VF8CL
- old name for PN_MICROENABLE5VD8CL, maintained only for source compatibility
- Global PN_MICROENABLE5VQ8CXP4
- old name for PN_MICROENABLE5VQ8CXP6B, maintained only for source compatibility
|