跳转到内容

Temperature State#

相机的 Temperature State 功能指示相机的内部温度是正常还是过高。

当温度过高时,需要立即冷却。

使用 Device Temperature 功能可确定相机的当前温度。

该功能的使用#

运作原理#

有关内部温度的信息通过以下参数提供:

  • The DeviceTemperature parameter value shows the current temperature at various locations within the camera. For more information, see the Device Temperature topic.
  • 即: TemperatureState 参数值告诉您相机的当前内部温度状态:
    • Ok: The device temperature is within the normal operating temperature range.
    • Critical: The device temperature is close to or at the allowed maximum. Provide cooling.
    • Error: The device temperature is above the allowed maximum. Provide cooling immediately.

根据您的相机型号,可以使用以下附加参数:

  • The BslTemperatureStatusErrorCount parameter indicates how often the temperature state changed to Error.
  • The BslTemperatureMax parameter indicates the maximum temperature the camera reached during operation.

When the TemperatureState parameter value is Critical or Error, the camera provides a set of mechanisms that alert the user and help to protect the camera.

这些机制会在不同的 device temperature 下生效,具体取决于警报级别以及相机是在升温还是在冷却

信息

Normal camera operation requires that the temperature state stays at Ok and the housing temperature stays within the allowed range. To ensure this, follow the guidelines set out in the "Environmental Requirements" section of your camera topic. You can find your camera topic in the "Models" section.

在高温下,相机可能会损坏,相机的寿命会缩短,并且图像质量可能会下降。频繁的高温事故也会缩短使用寿命。

升温路径和冷却路径

加热路径#

临界温度阈值#

当设备温度达到临界温度阈值时,相机即将过热。

在这种情况下,将发生以下情况:

  • The TemperatureState parameter value changes to Critical.
  • 相机发送一个临界温度事件。

信息

仅在 device temperature 降至临界温度阈值以下至少 4°C 之后,才能发送另一个临界温度事件。

超温阈值#

当设备温度达到过温阈值时,则表明相机过热。必须立即对相机进行冷却,否则,相机可能会发生不可挽回的损坏。

在这种情况下,将发生以下情况:

  • The TemperatureState parameter value changes to Error.
  • 相机的电流消耗会降低。
  • 图像采集更改:
    • On ace 2, boost, dart M/R, and racer 2 cameras, image acquisition stops and can't be started until the device has cooled down.
    • 在其他相机上,出现测试图像 2
  • 相机发送一个超温事件。
  • 如果您的相机型号具有错误代码功能,则相机会报告超温错误代码。
  • If available, the BslTemperatureStatusErrorCount parameter increases by 1.

信息

仅在 device temperature 降至超温阈值以下至少 4°C 之后,才能发送另一个超温事件。

冷却路径#

超温阈值#

当设备温度降至超温阈值以下时,将发生以下情况:

  • The TemperatureState parameter value changes from Error to Critical.

当设备温度下降到低于超温阈值 4°C 时,将发生以下情况:

  • On ace 2, boost, dart M/R, and racer 2 cameras, image acquisition can be started again.
  • On other cameras, test image 2 disappears. Image acquisition resumes with the same settings and features as before the camera entered the Error state. The exception is the Sequencer feature which you have to re-enable manually.
临界温度阈值#

当设备温度降至临界温度阈值以下时,将发生以下情况:

  • The TemperatureState parameter value changes to Ok.

相机的温度状态和内部温度正常,因此相机可以正常工作。

确定温度状态#

  1. Get the TemperatureState parameter value.
  2. If the parameter value is Critical or Error, you must cool the camera until the parameter value is Ok.

充分利用 Temperature State 功能:

  • 使用 Device Temperature 功能确定确切的核心板或传感器板温度。
  • 启用 Event Notification 功能在相机温度过高时接收事件。
  • If the Error Code feature is available on your camera model, read the LastError parameter value to determine whether the camera was too hot.

详情#

显示所有相机型号

相机型号 临界温度阈值 超温阈值 附加参数
a2A640-240gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A640-240umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1280-80gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1280-125umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-51gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-160umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-165g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A1920-165g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-35gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2048-110umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2440-98g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2440-98g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-23gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-75umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-105g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-105g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-120cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-120cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-210cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2448-210cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2560-20gmSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2560-70umSWIR 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-22gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2590-60umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-20gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2600-64umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-14gmUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-48umUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-67g5mUV 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-86cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A2840-86cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-13gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A3840-45umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-9gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-30umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-44g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-44g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-67cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4096-67cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-12gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4200-40umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-5gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-18umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-27g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-27g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-42cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4504-42cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-6gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A4508-20umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-7gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-23umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-34g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-34g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-52cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5320-52cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gcBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gcPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gmBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-4gmPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15ucBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15ucPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15umBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-15umPRO 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-22g5cBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-22g5mBAS 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-35cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
a2A5328-35cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
acA640-121gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA640-300gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA640-300gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA640-750uc 75 °C (167 °F) 81 °C (177.8 °F)
acA640-750um 75 °C (167 °F) 81 °C (177.8 °F)
acA720-290gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA720-290gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA720-520uc 75 °C (167 °F) 81 °C (177.8 °F)
acA720-520um 75 °C (167 °F) 81 °C (177.8 °F)
acA800-200gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA800-200gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA800-510uc 75 °C (167 °F) 81 °C (177.8 °F)
acA800-510um 75 °C (167 °F) 81 °C (177.8 °F)
acA1280-60gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1280-60gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1300-60gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1300-60gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1300-60gmNIR 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1300-75gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1300-75gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1300-200uc 75 °C (167 °F) 81 °C (177.8 °F)
acA1300-200um 75 °C (167 °F) 81 °C (177.8 °F)
acA1440-73gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1440-73gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1440-220uc 75 °C (167 °F) 81 °C (177.8 °F)
acA1440-220um 75 °C (167 °F) 81 °C (177.8 °F)
acA1600-20gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1600-20uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1600-60gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1600-60gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1920-25gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1920-25gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1920-25uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1920-25um 不支持 Temperature State 功能 不支持 Temperature State 功能
acA1920-40gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-40gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-40uc 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-40ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-40um 75 °C (167.0 °F) 81 °C (177.8 °F)
acA1920-40umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-48gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-48gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-50gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-50gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA1920-150uc 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-150um 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-155uc 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-155ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-155um 75 °C (167 °F) 81 °C (177.8 °F)
acA1920-155umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA2000-50gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2000-50gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2000-165uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2000-165um 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-25gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-25gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-25gmNIR 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-35gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2040-35gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2040-55uc 75 °C (167 °F) 81 °C (177.8 °F)
acA2040-55um 75 °C (167 °F) 81 °C (177.8 °F)
acA2040-90uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-90um 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-90umNIR 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2040-120uc 75 °C (167 °F) 81 °C (177.8 °F)
acA2040-120um 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-20gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2440-20gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2440-35uc 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-35ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-35um 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-35umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-75uc 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-75ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-75um 75 °C (167 °F) 81 °C (177.8 °F)
acA2440-75umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA2500-14gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2500-14gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2500-14uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2500-14um 不支持 Temperature State 功能 不支持 Temperature State 功能
acA2500-20gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2500-20gcMED 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2500-20gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2500-20gmMED 72 °C (161.6 °F) 78 °C (172.4 °F)
acA2500-60uc 75 °C (167 °F) 81 °C (177.8 °F)
acA2500-60um 75 °C (167 °F) 81 °C (177.8 °F)
acA3088-16gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA3088-16gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA3088-57uc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA3088-57ucMED 290°C (554°F) 300°C (572°F)
acA3088-57um The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA3088-57umMED 290°C (554°F) 300°C (572°F)
acA3800-10gc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA3800-10gm 不支持 Temperature State 功能 不支持 Temperature State 功能
acA3800-14uc 不支持 Temperature State 功能 不支持 Temperature State 功能
acA3800-14um 不支持 Temperature State 功能 不支持 Temperature State 功能
acA4024-8gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4024-8gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4024-29uc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4024-29um The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4096-11gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4096-11gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4096-30uc 80 °C (176 °F) 86 °C (186.8 °F)
acA4096-30ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4096-30um 80 °C (176 °F) 86 °C (186.8 °F)
acA4096-30umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4096-40uc 80 °C (176 °F) 86 °C (186.8 °F)
acA4096-40ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4096-40um 80 °C (176 °F) 86 °C (186.8 °F)
acA4096-40umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4112-8gc The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4112-8gm The Temperature State feature is implemented, but non-functional. The parameters are available, but the temperature state never changes to Critical or Over Temperature. -
acA4112-20uc 80 °C (176 °F) 86 °C (186.8 °F)
acA4112-20ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4112-20um 80 °C (176 °F) 86 °C (186.8 °F)
acA4112-20umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4112-30uc 80 °C (176 °F) 86 °C (186.8 °F)
acA4112-30ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA4112-30um 80 °C (176 °F) 86 °C (186.8 °F)
acA4112-30umMED 75 °C (167 °F) 81 °C (177.8 °F)
acA5472-5gc 72 °C (161.6 °F) 78 °C (172.4 °F)
acA5472-5gm 72 °C (161.6 °F) 78 °C (172.4 °F)
acA5472-17uc 75 °C (167 °F) 81 °C (177.8 °F)
acA5472-17ucMED 75 °C (167 °F) 81 °C (177.8 °F)
acA5472-17um 75 °C (167 °F) 81 °C (177.8 °F)
acA5472-17umMED 75 °C (167 °F) 81 °C (177.8 °F)
boA1936-400cc 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
boA1936-400cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
boA2448-250cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
bo2448-250cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA2832-190cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
bo2832-190cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-93cc 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-93cm 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4096-180cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
bo4096-180cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4112-68cc 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4112-68cm 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4500-45cc 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4500-45cm 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA4504-100cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA4504-100cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5120-150cc 85 °C (185 °F) 90 °C (194 °F)
boA5120-150cm 85 °C (185 °F) 90 °C (194 °F)
boA5120-230cc 85 °C (185 °F) 90 °C (194 °F)
boA5120-230cm 85 °C (185 °F) 90 °C (194 °F)
boA5320-150cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5320-150cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5328-100cc 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA5328-100cm 82 °C (179.6 °F) / 85 °C (185 °F)a 87°C (188.6°F)/90°C (194°F)a BslTemperatureMax
BslTemperatureStatusErrorCount
boA6500-36cc 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA6500-36cm 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA8100-16cc 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA8100-16cm 不支持 Temperature State 功能 不支持 Temperature State 功能 BslTemperatureMax
BslTemperatureStatusErrorCount
boA9344-30cc 85 °C (185 °F) 90 °C (194 °F)
boA9344-30cm 85 °C (185 °F) 90 °C (194 °F)
boA9344-70cc 85 °C (185 °F) 90 °C (194 °F)
boA9344-70cm 85 °C (185 °F) 90 °C (194 °F)
boA13440-17cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA720-520uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA720-520um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1280-54uc 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1280-54um 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1440-220uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1440-220um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1600-60uc 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1600-60um 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1920-15um 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1920-30uc 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1920-30um 不支持 Temperature State 功能 不支持 Temperature State 功能
daA1920-160uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA1920-160um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2448-70uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2448-70um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA2500-14uc 不支持 Temperature State 功能 不支持 Temperature State 功能
daA2500-14um 不支持 Temperature State 功能 不支持 Temperature State 功能
daA3840-45uc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
daA3840-45um 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA720-290gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA720-290gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1440-73gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1440-73gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1920-51gc 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
dmA1920-51gm 85 °C (185 °F) 100 °C (212 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
puA1280-54uc 不支持 Temperature State 功能 不支持 Temperature State 功能
puA1280-54um 不支持 Temperature State 功能 不支持 Temperature State 功能
puA1600-60uc 不支持 Temperature State 功能 不支持 Temperature State 功能
puA1600-60um 不支持 Temperature State 功能 不支持 Temperature State 功能
puA1920-30uc 不支持 Temperature State 功能 不支持 Temperature State 功能
puA1920-30um 不支持 Temperature State 功能 不支持 Temperature State 功能
puA2500-14uc 不支持 Temperature State 功能 不支持 Temperature State 功能
puA2500-14um 不支持 Temperature State 功能 不支持 Temperature State 功能
r2L2048-29gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-58gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-62cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-62g5c 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-172cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L2048-172g5m 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-14gc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-29gm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-42cc 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-42g5c 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-84cm 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L4096-84g5m 76 °C (168.8 °F) 81 °C (177.8 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L8192-200cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount
r2L16384-120cm 89 °C (192.2 °F) 94 °C (201.2 °F) BslTemperatureMax
BslTemperatureStatusErrorCount

  1. 1 个 CXP(带 PoCXP)/1 个 CXP(通过 AUX 电源供电)或 2 个 CXP

示例代码#

ace 2, boost, dart M/R, and racer 2 Cameras#
// Get the current temperature state
BslTemperatureStatusEnums e = camera.BslTemperatureStatus.GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = camera.BslTemperatureMax.GetValue();
// Determine how often the temperature state changed to Error
int64_t i = camera.BslTemperatureStatusErrorCount.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Get the current temperature state
String_t e = CEnumParameter(nodemap, "BslTemperatureStatus").GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = CFloatParameter(nodemap, "BslTemperatureMax").GetValue();
// Determine how often the temperature state changed to Error
int64_t i = CIntegerParameter(nodemap, "BslTemperatureStatusErrorCount").GetValue();
// Get the current temperature state
string e = camera.Parameters[PLCamera.BslTemperatureStatus].GetValue();
// Get the maximum temperature the camera reached during operation
double temperatureMax = camera.Parameters[PLCamera.BslTemperatureMax].GetValue();
// Determine how often the temperature state changed to Error
Int64 i = camera.Parameters[PLCamera.BslTemperatureStatusErrorCount].GetValue();
size_t len = 0;
char e_str[64] = {0};
double temperatureMax = 0;
int64_t i = 0;
/* Get the current temperature state */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "BslTemperatureStatus", e_str, &len);
CHECK(errRes);
/* Get the maximum temperature the camera reached during operation */
errRes = PylonDeviceGetFloatFeature(hdev, "BslTemperatureMax", &temperatureMax);
CHECK(errRes);
/* Determine how often the temperature state changed to Error */
errRes = PylonDeviceGetIntegerFeature(hdev, "BslTemperatureStatusErrorCount", &i);
CHECK(errRes);
# Get the current temperature state
e = camera.BslTemperatureStatus.Value
# Get the maximum temperature the camera reached during operation
temperatureMax = camera.BslTemperatureMax.Value
# Determine how often the temperature state changed to Error
i = camera.BslTemperatureStatusErrorCount.Value
其他相机#
// Get the current temperature state
TemperatureStateEnums e = camera.TemperatureState.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Get the current temperature state
String_t e = CEnumParameter(nodemap, "TemperatureState").GetValue();
// Get the current temperature state
string e = camera.Parameters[PLCamera.TemperatureState].GetValue();
size_t len = 0;
char e_str[64] = {0};
/* Get the current temperature state */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "TemperatureState", e_str, &len);
CHECK(errRes);
# Get the current temperature state
e = camera.TemperatureState.Value

您也可以使用 pylon Viewer 轻松设置参数。