Rotation matrix and translation vector

A pose can also be defined by a rotation matrix R and a translation vector T.

R = \left(\begin{array}{ccc}
  r_{00} & r_{01} & r_{02} \\
  r_{10} & r_{11} & r_{12} \\
  r_{20} & r_{21} & r_{22}
\end{array}\right), \qquad
T = \left(\begin{array}{c}
  X \\
  Y \\
  Z
\end{array}\right).

The pose transformation can be applied to a point P by

P' = R P + T.

Conversion from rotation matrix to quaternion

The conversion from a rotation matrix (with det(R)=1) to a quaternion q=(\begin{array}{cccc}x & y & z & w\end{array}) can be done as follows.

x &= \text{sign}(r_{21}-r_{12}) \frac{1}{2}\sqrt{\text{max}(0, 1 + r_{00} - r_{11} - r_{22})} \\
y &= \text{sign}(r_{02}-r_{20}) \frac{1}{2}\sqrt{\text{max}(0, 1 - r_{00} + r_{11} - r_{22})} \\
z &= \text{sign}(r_{10}-r_{01}) \frac{1}{2}\sqrt{\text{max}(0, 1 - r_{00} - r_{11} + r_{22})} \\
w &= \frac{1}{2}\sqrt{\text{max}(0, 1 + r_{00} + r_{11} + r_{22})}

即: \text{sign} operator returns -1 if the argument is negative. Otherwise, 1 is returned. It is used to recover the sign for the square root. The \text{max} function ensures that the argument of the square root function is not negative, which can happen in practice due to round-off errors.

Conversion from quaternion to rotation matrix

The conversion from a quaternion q=(\begin{array}{cccc}x & y & z &
w\end{array}) with ||q||=1 to a rotation matrix can be done as follows.

R = 2 \left(\begin{array}{ccc}
  \frac{1}{2} - y^2 - z^2 & x y - z w & x z + y w \\
  x y + z w & \frac{1}{2} - x^2 - z^2 & y z - x w \\
  x z - y w & y z + x w & \frac{1}{2} - x^2 - y^2
\end{array}\right)