General API structure¶
The general entry point to the rc_cube’s API is http://<host>/api/
,
where <host>
is either the device’s IP address or its host name as known
by the respective DHCP server, as explained in
network configuration.
Accessing this entry point with a web browser lets the user explore and test
the full API during run-time using the Swagger UI
.
For actual HTTP requests, the current API version is appended to the entry point
of the API, i.e., http://<host>/api/v2
. All data sent to and
received by the REST-API follows the JavaScript Object Notation (JSON).
The API is designed to let the user create, retrieve, modify, and delete
so-called resources as listed in Available resources and requests using the HTTP requests below.
Request type | 描述 |
---|---|
GET | Access one or more resources and return the result as JSON. |
PUT | Modify a resource and return the modified resource as JSON. |
DELETE | Delete a resource. |
POST | Upload file (e.g., license or firmware image). |
Depending on the type and the specific request itself, arguments to HTTP requests can be transmitted as part of the path (URI) to the resource, as query string, as form data, or in the body of the request. The following examples use the command line tool curl, which is available for various operating systems. See https://curl.haxx.se.
Get a node’s current status; its name is encoded in the path (URI)
curl -X GET 'http://<host>/api/v2/pipelines/0/nodes/rc_stereomatching'
Get values of some of a node’s parameters using a query string
curl -X GET 'http://<host>/api/v2/pipelines/0/nodes/rc_stereomatching/parameters?name=minconf&name=maxdepth'
Set a node’s parameter as JSON-encoded text in the body of the request
curl -X PUT --header 'Content-Type: application/json' -d '[{"name": "mindepth", "value": 0.1}]' 'http://<host>/api/v2/pipelines/0/nodes/rc_stereomatching/parameters'
As for the responses to such requests, some common return codes for the rc_cube’s API are:
Status Code | 描述 |
---|---|
200 OK |
The request was successful; the resource is returned as JSON. |
400 Bad Request |
A required attribute or argument of the API request is missing or invalid. |
404 Not Found |
A resource could not be accessed; e.g., an ID for a resource could not be found. |
403 Forbidden |
Access is (temporarily) forbidden; e.g., some parameters are locked while a GigE Vision application is connected. |
429 Too many requests |
Rate limited due to excessive request frequency. |
The following listing shows a sample response to a successful request that accesses
information about the rc_stereomatching
node’s minconf
parameter:
HTTP/1.1 200 OK
Content-Type: application/json
Content-Length: 157
{
"name": "minconf",
"min": 0,
"default": 0,
"max": 1,
"value": 0,
"type": "float64",
"description": "Minimum confidence"
}
Note
The actual behavior, allowed requests, and specific return codes depend heavily on the specific resource, context, and action. Please refer to the rc_cube’s available resources and to each software module’s parameters and services.
Migration from API version 1¶
API version 1 has become deprecated with the 22.01 firmware release of the rc_cube. The following changes were introduced in API version 2.
- All 3D-camera, detection and configuration modules which were located under
/nodes
in API version 1 are now under/pipelines/<pipeline number>/nodes
to support multiple pipelines running on the rc_cube, e.g./pipelines/1/nodes/rc_camera
.
- Configuring load carriers, grippers and regions of interest is now only possible in the global database modules, which
are located under
/nodes
, e.g./nodes/rc_load_carrier_db
. The corresponding services in the detection modules have been removed or deprecated. - Templates can now be accessed under
/templates
, e.g./templates/rc_silhouettematch
.
Available resources and requests¶
The available REST-API resources are structured into the following parts:
/nodes
- Access the rc_cube’s global Database modules with their run-time status, parameters, and offered services, for storing data used in all camera pipelines and multiple modules, such as load carriers, grippers and regions of interest.
/pipelines
- Access to the status and configuration of the camera pipelines.
/pipelines/<number>/nodes
- Access the rc_cube’s 3D-camera, detection and configuration software modules of the camera pipeline with the specified number, with their run-time status, parameters, and offered services.
/templates
- Access the object templates on the rc_cube.
/system
- Access the system state, set network configuration, configure the camera pipeline types, and manage licenses as well as firmware updates.
/userspace
- Access the UserSpace on the rc_cube.
/logs
- Access the log files on the rc_cube.