Available Patches

The installers listed below include fixes of critical issues that became known after release of Basler runtime software version 5.5.1.

Basler runtime patches are usually distributed in form of complete runtime software installers. The installer file name contains a five-digit number (patch ID) that indicates which patch is included in a specific installer.1

You can always download the latest runtime installer from our website's download section: "Runtime Setup v5.x" (Windows) or "Runtime v5.x ..." (Linux).

 

Patch ID

Fixed Issues

Installer Names with Patch ID

Available since

 68121

  • When an applet designed with VisualApplets 3.0.6 was saved as *.mcf file (via microDisplay or SDK function Fg_saveConfig), this *.mcf file provoked a crash when it was loaded via SDK function Fg_InitConfig. This has been fixed. (7333)
  • Applets created with VisualApplets version 2.0 were not recognized by the applet iterator interface of fglib and due to this also not shown in microDisplay. This has been fixed. Applets created with all VisualApplets versions down to Version 2.0 can be used with the applet iterator interface of fglib and in microDisplay. (7339)

RuntimeSetup_v5.5.1-68121_Win64.exe

11.09.2017

RuntimeSetup_with_Applets_v5.5.1-68121_Win64.exe

11.09.2017

RuntimeSetup_v5.5.1-68121_Win32.exe

11.09.2017

RuntimeSetup_with_Applets_v5.5.1-68121_Win64.exe

11.09.2017

siso-rt5-5.5.1-68121-linux-amd64.tar.bz2

11.09.2017

siso-rt5-5.5.1-68121-linux-ia32.tar.bz2

11.09.2017