Acquisition Start, Stop, and Abort#
信息
- These commands aren't available via the pylon Viewer feature tree. Instead,
AcquisitionStart
andAcquisitionStop
commands are generated automatically when you use the Single Shot, Continuous Shot, and Stop buttons in the toolbar of the pylon Viewer. - pylon C++ API 和 pylon .NET API 提供了自动处理这些命令的相机类。Basler 建议使用这些类。
如需了解详情,请参阅 pylon API 文档中的采集 (C++) 和 采集 (.NET) 代码示例。
该功能的使用#
开始图像采集#
To switch on image acquisition, execute the AcquisitionStart
command.
执行此命令后,相机会等待触发信号。触发信号既可以在相机内部生成(自由运行),也可以从外部应用(触发图像采集)。
信息
To check whether the camera is currently waiting for a trigger signal, monitor the camera's Trigger Wait signals or use the Acquisition Status feature, if available.
停止图像采集#
To switch off image acquisition, execute the AcquisitionStop
command. When the command is executed, the following occurs:
On area scan cameras:
- 如果相机当前未在采集帧,则图像采集功能会立即关闭。
- 如果相机当前正在读出图像数据,则系统会允许读出过程完成。之后,图像采集功能会关闭。
- 如果相机当前正在帧曝光过程中:
- On some camera models, executing an
AcquisitionStop
command aborts exposure. In this case, the camera stops exposing immediately and starts reading out image data. The readout process will be allowed to finish. Afterwards, image acquisition is switched off. - On some camera models, you can configure whether executing an
AcquisitionStop
command aborts exposure or not. To do so, set theAcquisitionStopMode
parameter toAbortExposure
或Complete
.
- On some camera models, executing an
On line scan cameras:
- 即:
AcquisitionStopMode
parameter for line scan cameras is always set toImmediate
. - 如果相机当前未在采集帧,则图像采集功能会立即关闭。
- If the camera is currently exposing a line, the
AcquisitionStop
command leads to the following for all racer 2 line scan cameras:
The exposure of the current line is completed. Acquisition stops immediately. The last acquired line is transmitted to the host computer. - In addtion, for racer 2 S cameras with GigE interface, the following is true:
Only the lines acquired up to the point when the command was executed are delivered to the host computer. This may result in a partial frame being transmitted.
中止图像采集#
To abort image acquisition, execute the AcquisitionAbort
command (如果可用).
On area scan cameras, the following occurs when the command is executed:
- If the camera is not currently acquiring a frame, image acquisition is switched off immediately.
- If the camera is currently exposing a frame, the camera stops exposing immediately. The readout process, if already started, is aborted. The current frame will be incomplete and is not transmitted to the host computer. Afterwards, image acquisition is switched off.
- If the camera is currently reading out image data, the camera stops the readout process immediately. The current frame will be incomplete and is not transmitted to the host computer. Afterwards, image acquisition is switched off.
On line scan cameras, the following occurs when the command is executed:
- If the camera is not currently acquiring a line, image acquisition is switched off immediately.
- If the camera is currently exposing a line, the camera stops exposing immediately. The readout process, if already started, is continued. Only the lines acquired up to the point when the command was executed are delivered to the host computer. For line scan cameras with GigE interface, this may result in a partial frame being transmitted. Afterwards, image acquisition is switched off.
- If the camera is currently reading out image data, the camera continues the readout process until all lines acquired up to the point when the command was executed are delivered to the host computer. For line scan cameras with GigE interface, this means that the current frame may be incomplete (partial frame).
Afterwards, image acquisition is switched off.
详情#
相机型号 | AcquisitionAbort 命令可用 | AcquisitionStop 命令中止曝光 |
---|---|---|
a2A640-240gmSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A640-240umSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1280-80gmSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1280-125umSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-51gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-51gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-51gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-51gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-160ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-160ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-160umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-160umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-165g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A1920-165g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2048-35gmSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2048-110umSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2440-98g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2440-98g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-23gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-23gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-23gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-23gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-75ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-75ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-75umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-75umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-105g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-105g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-120cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-120cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-210cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2448-210cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2560-20gmSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2560-70umSWIR | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-22gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-22gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-22gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-22gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-60ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-60ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-60umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2590-60umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-20gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-20gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-20gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-20gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-64ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-64ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-64umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2600-64umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-14gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-14gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-14gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-14gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-14gmUV | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-48ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-48ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-48umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-48umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-48umUV | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-67g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-67g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-67g5mUV | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-86cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A2840-86cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-9gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-9gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-9gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-9gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-31ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-31ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-31umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-31umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-42g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3536-42g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-13gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-13gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-13gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-13gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-45ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-45ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-45umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A3840-45umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-9gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-9gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-9gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-9gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-30ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-30ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-30umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-30umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-44g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-44g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-67cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4096-67cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-12gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-12gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-12gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-12gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-40ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-40ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-40umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4200-40umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-5gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-5gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-5gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-5gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-18ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-18ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-18umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-18umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-27g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-27g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-42cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4504-42cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-6gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-6gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-6gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-6gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-20ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-20ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-20umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A4508-20umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-4gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-4gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-15ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-15umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-21g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5060-21g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-7gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-7gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-7gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-7gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-23ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-23ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-23umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-23umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-34g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-34g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-52cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5320-52cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-4gcBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-4gcPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-4gmBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-4gmPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-15ucBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-15ucPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-15umBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-15umPRO | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-22g5cBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-22g5mBAS | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-35cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
a2A5328-35cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
acA640-121gm | 无 | 是 |
acA640-300gc | 无 | 是 |
acA640-300gm | 无 | 是 |
acA640-750uc | 无 | 是 |
acA640-750um | 无 | 是 |
acA720-290gc | 无 | 是 |
acA720-290gm | 无 | 是 |
acA720-520uc | 无 | 是 |
acA720-520um | 无 | 是 |
acA800-200gc | 无 | 是 |
acA800-200gm | 无 | 是 |
acA800-510uc | 无 | 是 |
acA800-510um | 无 | 是 |
acA1280-60gc | 无 | 是 |
acA1280-60gm | 无 | 是 |
acA1300-60gc | 无 | 是 |
acA1300-60gm | 无 | 是 |
acA1300-60gmNIR | 无 | 是 |
acA1300-75gc | 无 | 是 |
acA1300-75gm | 无 | 是 |
acA1300-200uc | 无 | 是 |
acA1300-200um | 无 | 是 |
acA1440-73gc | 无 | 是 |
acA1440-73gm | 无 | 是 |
acA1440-220uc | 无 | 是 |
acA1440-220um | 无 | 是 |
acA1600-20gc | 无 | 是 |
acA1600-20uc | 无 | 是 |
acA1600-60gc | 无 | 是 |
acA1600-60gm | 无 | 是 |
acA1920-25gc | 无 | 是 |
acA1920-25gm | 无 | 是 |
acA1920-25uc | 无 | 是 |
acA1920-25um | 无 | 是 |
acA1920-40gc | 无 | 是 |
acA1920-40gm | 无 | 是 |
acA1920-40uc | 无 | 是 |
acA1920-40ucMED | 无 | 是 |
acA1920-40um | 无 | 是 |
acA1920-40umMED | 无 | 是 |
acA1920-48gc | 无 | 是 |
acA1920-48gm | 无 | 是 |
acA1920-50gc | 无 | 是 |
acA1920-50gm | 无 | 是 |
acA1920-150uc | 无 | 是 |
acA1920-150um | 无 | 是 |
acA1920-155uc | 无 | 是 |
acA1920-155ucMED | 无 | 是 |
acA1920-155um | 无 | 是 |
acA1920-155umMED | 无 | 是 |
acA2000-50gc | 无 | 是 |
acA2000-50gm | 无 | 是 |
acA2000-165uc | 无 | 是 |
acA2000-165um | 无 | 是 |
acA2040-25gc | 无 | 是 |
acA2040-25gm | 无 | 是 |
acA2040-25gmNIR | 无 | 是 |
acA2040-35gc | 无 | 是 |
acA2040-35gm | 无 | 是 |
acA2040-55uc | 无 | 是 |
acA2040-55um | 无 | 是 |
acA2040-90uc | 无 | 是 |
acA2040-90um | 无 | 是 |
acA2040-90umNIR | 无 | 是 |
acA2040-120uc | 无 | 是 |
acA2040-120um | 无 | 是 |
acA2440-20gc | 无 | 是 |
acA2440-20gm | 无 | 是 |
acA2440-35uc | 无 | 是 |
acA2440-35ucMED | 无 | 是 |
acA2440-35um | 无 | 是 |
acA2440-35umMED | 无 | 是 |
acA2440-75uc | 无 | 是 |
acA2440-75ucMED | 无 | 是 |
acA2440-75um | 无 | 是 |
acA2440-75umMED | 无 | 是 |
acA2500-14gc | 无 | 是 |
acA2500-14gm | 无 | 是 |
acA2500-14uc | 无 | 是 |
acA2500-14um | 无 | 是 |
acA2500-20gc | 无 | 是 |
acA2500-20gcMED | 无 | 是 |
acA2500-20gm | 无 | 是 |
acA2500-20gmMED | 无 | 是 |
acA2500-60uc | 无 | 是 |
acA2500-60um | 无 | 是 |
acA3088-16gc | 无 | 是 |
acA3088-16gm | 无 | 是 |
acA3088-57uc | 无 | 是 |
acA3088-57ucMED | 无 | 是 |
acA3088-57um | 无 | 是 |
acA3088-57umMED | 无 | 是 |
acA3800-10gc | 无 | 是 |
acA3800-10gm | 无 | 是 |
acA3800-14uc | 无 | 是 |
acA3800-14um | 无 | 是 |
acA4024-8gc | 无 | 是 |
acA4024-8gm | 无 | 是 |
acA4024-29uc | 无 | 是 |
acA4024-29um | 无 | 是 |
acA4096-11gc | 无 | 是 |
acA4096-11gm | 无 | 是 |
acA4096-30uc | 无 | 是 |
acA4096-30ucMED | 无 | 是 |
acA4096-30um | 无 | 是 |
acA4096-30umMED | 无 | 是 |
acA4096-40uc | 无 | 是 |
acA4096-40ucMED | 无 | 是 |
acA4096-40um | 无 | 是 |
acA4096-40umMED | 无 | 是 |
acA4112-8gc | 无 | 是 |
acA4112-8gm | 无 | 是 |
acA4112-20uc | 无 | 是 |
acA4112-20ucMED | 无 | 是 |
acA4112-20um | 无 | 是 |
acA4112-20umMED | 无 | 是 |
acA4112-30uc | 无 | 是 |
acA4112-30ucMED | 无 | 是 |
acA4112-30um | 无 | 是 |
acA4112-30umMED | 无 | 是 |
acA5472-5gc | 无 | 是 |
acA5472-5gm | 无 | 是 |
acA5472-17uc | 无 | 是 |
acA5472-17ucMED | 无 | 是 |
acA5472-17um | 无 | 是 |
acA5472-17umMED | 无 | 是 |
boA1936-400cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA1936-400cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA2448-250cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
bo2448-250cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA2832-190cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
bo2832-190cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4096-93cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4096-93cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4096-180cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
bo4096-180cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4112-68cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4112-68cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4500-45cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4500-45cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4504-100cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA4504-100cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA5120-150cc | 无 | 是 |
boA5120-150cm | 无 | 是 |
boA5120-230cc | 无 | 是 |
boA5120-230cm | 无 | 是 |
boA5320-150cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA5320-150cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA5328-100cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA5328-100cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA6500-36cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA6500-36cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA8100-16cc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA8100-16cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
boA9344-30cc | 无 | 是 |
boA9344-30cm | 无 | 是 |
boA9344-70cc | 无 | 是 |
boA9344-70cm | 无 | 是 |
boA13440-17cm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA720-520uc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA720-520um | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA1280-54uc | 无 | 是 |
daA1280-54um | 无 | 是 |
daA1440-220uc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA1440-220um | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA1600-60uc | 无 | 是 |
daA1600-60um | 无 | 是 |
daA1920-15um | 无 | 是 |
daA1920-30uc | 无 | 是 |
daA1920-30um | 无 | 是 |
daA1920-160uc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA1920-160um | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA2448-70uc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA2448-70um | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA2500-14uc | 无 | 是 |
daA2500-14um | 无 | 是 |
daA3840-45uc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
daA3840-45um | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA720-290gc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA720-290gm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA1440-73gc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA1440-73gm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA1920-51gc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA1920-51gm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA3536-9gc | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
dmA3536-9gm | 是 | 可通过 BslAcquisitionStopMode 参数进行配置 |
puA1280-54uc | 无 | 是 |
puA1280-54um | 无 | 是 |
puA1600-60uc | 无 | 是 |
puA1600-60um | 无 | 是 |
puA1920-30uc | 无 | 是 |
puA1920-30um | 无 | 是 |
puA2500-14uc | 无 | 是 |
puA2500-14um | 无 | 是 |
r2L2048-29gc | 是 | 无 |
r2L2048-58gm | 是 | 无 |
r2L2048-62cc | 是 | 无 |
r2L2048-62g5c | 是 | 无 |
r2L2048-172cm | 是 | 无 |
r2L2048-172g5m | 是 | 无 |
r2L4096-14gc | 是 | 无 |
r2L4096-29gm | 是 | 无 |
r2L4096-42cc | 是 | 无 |
r2L4096-42g5c | 是 | 无 |
r2L4096-84cm | 是 | 无 |
r2L4096-84g5m | 是 | 无 |
r2L8192-200cm | 是 | 无 |
r2L16384-120cm | 是 | 无 |
示例代码#
// Configure continuous image acquisition on the cameras
camera.AcquisitionMode.SetValue(AcquisitionMode_Continuous);
// Switch on image acquisition
camera.AcquisitionStart.Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
camera.AcquisitionStop.Execute();
// Switch image acquisition back on
camera.AcquisitionStart.Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
camera.AcquisitionAbort.Execute();
INodeMap& nodemap = camera.GetNodeMap();
// Configure continuous image acquisition on the cameras
CEnumParameter(nodemap, "AcquisitionMode").SetValue("Continuous");
// Switch on image acquisition
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
CCommandParameter(nodemap, "AcquisitionStop").Execute();
// Switch image acquisition back on
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
CCommandParameter(nodemap, "AcquisitionAbort").Execute();
// Configure continuous image acquisition on the cameras
camera.Parameters[PLCamera.AcquisitionMode].SetValue(PLCamera.AcquisitionMode.Continuous);
// Switch on image acquisition
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for trigger signals
// (...)
// Switch off image acquisition
camera.Parameters[PLCamera.AcquisitionStop].Execute();
// Switch image acquisition back on
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for trigger signals
// (...)
// Abort image acquisition
camera.Parameters[PLCamera.AcquisitionAbort].Execute();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Configure continuous image acquisition on the cameras */
errRes = PylonDeviceFeatureFromString(hdev, "AcquisitionMode", "Continuous");
CHECK(errRes);
/* Switch on image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for trigger signals */
/* (...) */
/* Switch off image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStop");
CHECK(errRes);
/* Switch image acquisition back on */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for trigger signals */
/* (...) */
/* Abort image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionAbort");
CHECK(errRes);
# Configure continuous image acquisition on the cameras
camera.AcquisitionMode.Value = "Continuous"
# Switch on image acquisition
camera.AcquisitionStart.Execute()
# The camera waits for trigger signals
# (...)
# Switch off image acquisition
camera.AcquisitionStop.Execute()
# Switch image acquisition back on
camera.AcquisitionStart.Execute()
# The camera waits for trigger signals
# (...)
# Abort image acquisition
camera.AcquisitionAbort.Execute()
您也可以使用 pylon Viewer 轻松设置参数。