Exposure Time#
要自动设置曝光时间,请使用 Exposure Auto 功能。
该功能的使用#
确定曝光时间#
确定当前的曝光时间(以微秒为单位):
- On ace 2, boost R, and dart R/M cameras, get the value of the
BslEffectiveExposureTime
parameter. This parameter is read-only. It takes factors like internal offsets or clock speed requirements into account that may cause the exposure time to differ from the exposure time set. - 在其他相机上,获取
ExposureTime
参数的值。请注意,根据传感器类型及其特定特性,此值可能与有效曝光时间稍有不同。
确定曝光时间可能是有用的,例如,如果自动功能 Exposure Auto
已启用,且您想检索自动调节的曝光时间。
曝光时间模式#
On some camera models, the ExposureTimeMode
parameter is available. It allows you to choose between exposure time modes that provide different exposure time ranges. Depending on your camera model, you can also set individual exposure times for different regions on the sensor, e.g., for two sensor lines or for red and green pixels.
您可以将 ExposureTimeMode
参数设置为以下值:
Common
orStandard
: Enables the Common or Standard exposure time mode. This is the default setting.Individual
: Allows you to specify different exposure times for individual regions on the image sensor. This can be useful, if you want to define different exposure times, e.g., for two sensor lines.Short
: Allows you to set a short exposure time within the value range available.UltraShort
: Allows you to set an ultra short exposure time within the value range available.
信息
- 根据曝光时间模式,曝光开始延迟会发生改变。
- If the Short or Ultra Short exposure time mode is enabled, the Sequencer feature is not available.
- If the exposure time mode is set to
Individual
, the GainAuto and ExposureAuto features are disabled.
Exposure Time Selector#
On some camera models, the ExposureTimeSelector
parameter is available. It allows you to expose either the entire image sensor for the exposure time specified or individual regions on the image sensor.
You can set the ExposureTimeSelector
parameter to one of the following values:
Common
: The entire image sensor is exposed for the exposure time specified.Stage 1
: Stage 1 is exposed for the exposure time specified. Stage 1 is a predefined region on the image sensor.Stage 2
: Stage 2 is exposed for the exposure time specified. Stage 2 is a predefined region on the image sensor.
Interleaved HDR#
Basler ace 2 R mono cameras with the sensors GMAX2505, GMAX2509, and GMAX2518 support interleaved HDR (iHDR). The iHDR feature allows you to set different exposure times for even and odd pixel lines of the sensor to increase the dynamic range of the final image.
To set the exposure time for iHDR:
- Set the
ExposureTimeMode
parameter toIndividual
. - Set the
ExposureTimeSelector
parameter toStage 1
. - Specify the exposure time for stage 1.
The value specified for stage 1 applies to the even pixel lines of the sensor. - Set the
ExposureTimeSelector
parameter toStage 2
. - Specify the exposure time for stage 2.
The value specified for stage 2 applies to the odd pixel lines of the sensor.
For example, you can specify a long exposure time for lines 1, 3, 5, etc. and a reduced exposure time for lines 2, 4, 6, etc. The long and short exposures start simultaneously. This creates a "striped" image with bright and dark lines.
Use an external post-processing program to combine the bright and dark lines to generate a high dynamic range image.
设置曝光时间#
要设置曝光时间:
- 将
ExposureMode
参数设置为Timed
。 - 如果可用,请将
ExposureAuto
参数设置为Off
。 - Set the
ExposureTimeMode
parameter (if available) to the desired exposure time mode. -
Set the
ExposureTimeSelector
parameter (if available) to the sensor region that should be exposed.信息
To be able to specify exposure times for different regions, the
ExposureTimeMode
parameter must be set toIndividual
. -
将
ExposureTime
参数设置为所需的曝光时间(以微秒为单位)。 - If necessary, repeat steps 4 and 5 for every region for which you want to specify individual exposure times.
最短和最长曝光时间因相机型号而异。
详情#
信息
在部分相机机型上,您可以使用 Remove Parameter Limits 功能提高曝光时间参数的上限。
相机型号 | 最短曝光时间 [µs] | 最长曝光时间 [µs] | 可用的 Exposure Time 模式 | Available ExposureTimeSelector Parameter Values |
---|---|---|---|---|
a2A640-240gmSWIR | Common exposure time mode: 16 Ultra Short exposure time mode: 2 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Common Ultra Short | 常规 |
a2A640-240umSWIR | Common exposure time mode: 16 Ultra Short exposure time mode: 2 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Common Ultra Short | 常规 |
a2A1280-80gmSWIR | Common exposure time mode: 16 Ultra Short exposure time mode: 2 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Common Ultra Short | 常规 |
a2A1280-125umSWIR | Common exposure time mode: 16 Ultra Short exposure time mode: 2 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 7 | Common Ultra Short | 常规 |
a2A1920-51gcBAS | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-51gcPRO | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-51gmBAS | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-51gmPRO | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-160ucBAS | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-160ucPRO | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-160umBAS | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-160umPRO | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-165g5cBAS | Common exposure time mode: 21 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A1920-165g5mBAS | Common exposure time mode: 21 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
a2A2048-35gmSWIR | Common exposure time mode: 27 Ultra Short exposure time mode: 7 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 13 | Common Ultra Short | 常规 |
a2A2048-37gcBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-37gcPRO | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-37gmBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-37gmPRO | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-110umSWIR | Common exposure time mode: 27 Ultra Short exposure time mode: 7 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 13 | Common Ultra Short | 常规 |
a2A2048-114g5cBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-114g5mBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-114ucBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-114ucPRO | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-114umBAS | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2048-114umPRO | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2440-98g5cBAS | 20 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2440-98g5mBAS | 20 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-23gcBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-23gcPRO | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-23gmBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-23gmPRO | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-75ucBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-75ucPRO | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-75umBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-75umPRO | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-105g5cBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-105g5mBAS | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-120cc | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-120cm | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-210cc | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2448-210cm | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2560-20gmSWIR | Common exposure time mode: 29 Ultra Short exposure time mode: 7 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 13 | Common Ultra Short | 常规 |
a2A2560-70umSWIR | Common exposure time mode: 29 Ultra Short exposure time mode: 7 | Common exposure time mode: 1000000 Ultra Short exposure time mode: 13 | Common Ultra Short | 常规 |
a2A2590-22gcBAS | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-22gcPRO | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-22gmBAS | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-22gmPRO | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-60ucBAS | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-60ucPRO | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-60umBAS | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2590-60umPRO | 10 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-20gcBAS | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-20gcPRO | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-20gmBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A2600-20gmPRO | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-64ucBAS | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-64ucPRO | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2600-64umBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A2600-64umPRO | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A2840-14gcBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-14gcPRO | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-14gmBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-14gmPRO | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-14gmUV | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-48ucBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-48ucPRO | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-48umBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-48umPRO | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-48umUV | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-67g5cBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-67g5mBAS | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-67g5mUV | 8 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-86cc | 8/9i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A2840-86cm | 8/9i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3536-9gcBAS | 12 | 10000000 | 常规 | 常规 |
a2A3536-9gcPRO | 12 | 10000000 | 常规 | 常规 |
a2A3536-9gmBAS | 12 | 10000000 | 常规 | 常规 |
a2A3536-9gmPRO | 12 | 10000000 | 常规 | 常规 |
a2A3536-31ucBAS | 12 | 10000000 | 常规 | 常规 |
a2A3536-31ucPRO | 12 | 10000000 | 常规 | 常规 |
a2A3536-31umBAS | 12 | 10000000 | 常规 | 常规 |
a2A3536-31umPRO | 12 | 10000000 | 常规 | 常规 |
a2A3536-42g5cBAS | 12 | 10000000 | 常规 | 常规 |
a2A3536-42g5mBAS | 12 | 10000000 | 常规 | 常规 |
a2A3840-13gcBAS | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-13gcPRO | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-13gmBAS | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-13gmPRO | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-45ucBAS | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-45ucPRO | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-45umBAS | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A3840-45umPRO | 12 | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-9gcBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-9gcPRO | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-9gmBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-9gmPRO | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-30ucBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-30ucPRO | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-30umBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-30umPRO | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-44g5cBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-44g5mBAS | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-67cc | 8/9i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4096-67cm | 8/9i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4200-12gcBAS | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4200-12gcPRO | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4200-12gmBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4200-12gmPRO | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4200-40ucBAS | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4200-40ucPRO | 2 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4200-40umBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4200-40umPRO | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4504-5gcBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-5gcPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-5gmBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-5gmPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-18ucBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-18ucPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-18umBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-18umPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-27g5cBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-27g5mBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-42cc | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4504-42cm | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4508-6gcBAS | 8 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4508-6gcPRO | 8 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4508-6gmBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4508-6gmPRO | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4508-20ucBAS | 8 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4508-20ucPRO | 8 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A4508-20umBAS | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A4508-20umPRO | Common exposure time mode: 2 Individual exposure time mode: Stage 1: 3 Stage 2: 2 | Common exposure time mode: 10000000 Individual exposure time mode: Stage 1: 10000000 Stage 2: 9999999m | Common Individual | Common Stage1 Stage2 |
a2A5060-4gcBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5060-4gmBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5060-15ucBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5060-15umBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5060-21g5cBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5060-21g5mBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-7gcBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-7gcPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-7gmBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-7gmPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-23ucBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-23ucPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-23umBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-23umPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-34g5cBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-34g5mBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-52cc | 11/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5320-52cm | 11/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-4gcBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-4gcPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-4gmBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-4gmPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-15ucBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-15ucPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-15umBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-15umPRO | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-22g5cBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-22g5mBAS | 16 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-35cc | 11/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
a2A5328-35cm | 11/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA640-121gm | 标准曝光时间模式:22/23b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA640-300gc | 80 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA640-300gm | 80 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA640-750uc | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA640-750um | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA720-290gc | Standard exposure time mode: 22/20b Ultra Short exposure time mode: 1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA720-290gm | Standard exposure time mode: 22/20b Ultra Short exposure time mode: 1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA720-520uc | 标准曝光时间模式:30/24b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA720-520um | 标准曝光时间模式:30/24b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA800-200gc | 80 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA800-200gm | 80 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA800-510uc | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA800-510um | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1280-60gc | 15 | 896000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1280-60gm | 15 | 896000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-60gc | 10 / 15a | 916000 / 896000a | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-60gm | 10 / 15a | 916000 / 896000a | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-60gmNIR | 10 / 15a | 916000 / 896000a | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-75gc | 80 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-75gm | 80 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-200uc | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1300-200um | 59 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1440-73gc | 标准曝光时间模式:22/23b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA1440-73gm | 标准曝光时间模式:22/23b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA1440-220uc | 标准曝光时间模式:21/20b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA1440-220um | 标准曝光时间模式:21/20b 超短曝光时间模式:1 | 标准曝光时间模式:10000000 超短曝光时间模式:13 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA1600-20gc | 25 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1600-20uc | 25 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1600-60gc | 10/35a | 840000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1600-60gm | 10/35a | 840000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-25gc | 35 | 999985 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-25gm | 35 | 999985 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-25uc | 35 | 9999990 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-25um | 35 | 9999990 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40gc | 34/40b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40gm | 34/40b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40uc | 34/40b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40ucMED | 34/40b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40um | 34/40 乙 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-40umMED | 34/40b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-48gc | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-48gm | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-50gc | 24/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-50gm | 24/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-150uc | 105 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-150um | 105 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-155uc | 20/21b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-155ucMED | 20/21b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-155um | 20/21b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA1920-155umMED | 20/21b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2000-50gc | 24 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2000-50gm | 24 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2000-165uc | 28c | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2000-165um | 28c | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-25gc | 24 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-25gm | 24 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-25gmNIR | 24 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-35gc | Standard 曝光时间模式:26 Ultra Short 曝光时间模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2040-35gm | Standard 曝光时间模式:26 Ultra Short 曝光时间模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2040-55uc | Standard Exposure Time 模式:27 Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2040-55um | Standard Exposure Time 模式:27 Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2040-90uc | 28c | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-90um | 28c | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-90umNIR | 28c | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2040-120uc | Standard Exposure Time 模式:21/20b Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2040-120um | Standard Exposure Time 模式:21/20b Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-20gc | Standard 曝光时间模式:28 Ultra Short 曝光时间模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-20gm | Standard 曝光时间模式:28 Ultra Short 曝光时间模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-35uc | Standard Exposure Time 模式:29 Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-35ucMED | 29 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2440-35um | Standard Exposure Time 模式:29 Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-35umMED | 29 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2440-75uc | Standard Exposure Time 模式:21/20b Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-75ucMED | 21/22b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2440-75um | Standard Exposure Time 模式:21/20b Ultra Short Exposure Time 模式:2 | 标准曝光时间模式:10000000 超短曝光时间模式:14 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA2440-75umMED | 21/22b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-14gc | 35 | 999985 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-14gm | 35 | 999985 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-14uc | 35 | 9999990 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-14um | 35 | 9999990 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-20gc | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-20gcMED | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-20gm | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-20gmMED | 137 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-60uc | 81 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA2500-60um | 81 | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-16gc | 滚动快门模式:25 全局重置释放快门模式:625 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-16gm | 滚动快门模式:25 全局重置释放快门模式:625 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-57uc | 滚动快门模式:8 全局重置释放快门模式:200 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-57ucMED | 滚动快门模式:8 全局重置释放快门模式:200 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-57um | 滚动快门模式:8 全局重置释放快门模式:200 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3088-57umMED | 滚动快门模式:8 全局重置释放快门模式:200 | 滚动快门模式:10000000 全局重置释放快门模式:10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3800-10gc | 35f | 1600000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3800-10gm | 35f | 1600000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3800-14uc | 35f | 1600000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA3800-14um | 35f | 1600000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4024-8gc | 滚动快门模式:35 全局重置释放快门模式:1260 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4024-8gm | 滚动快门模式:35 全局重置释放快门模式:1260 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4024-29uc | 滚动快门模式:10/12b 全局重置释放快门模式:360/432b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4024-29um | 滚动快门模式:10/12b 全局重置释放快门模式:360/432b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4096-11gc | 标准曝光时间模式:38 Ultra Short 曝光时间模式:2j | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-11gm | 标准曝光时间模式:38 Ultra Short 曝光时间模式:2j | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-30uc | Standard Exposure Time 模式:30 Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-30ucMED | 30 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4096-30um | Standard Exposure Time 模式:30 Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-30umMED | 30 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4096-40uc | Standard Exposure Time 模式:26/27b Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-40ucMED | 26/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4096-40um | Standard Exposure Time 模式:26/27b Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4096-40umMED | 26/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4112-8gc | Standard 曝光时间模式:38 Ultra Short 曝光时间模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-8gm | Standard 曝光时间模式:38 Ultra Short 曝光时间模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-20uc | Standard Exposure Time 模式:30 Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-20ucMED | 30 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4112-20um | Standard Exposure Time 模式:30 Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-20umMED | 30 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4112-30uc | Standard Exposure Time 模式:26/27b Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-30ucMED | 26/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA4112-30um | Standard Exposure Time 模式:26/27b Ultra Short Exposure Time 模式:2 | Standard Exposure Time 模式:10000000 Ultra Short Exposure Time 模式:16 | 标准 Ultra Short | ExposureTimeSelector parameter not available |
acA4112-30umMED | 26/27b | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-5gc | 滚动快门模式:52/55b 全局重置释放快门模式:1872/1980b | 10000016/10000045b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-5gm | 滚动快门模式:52/55b 全局重置释放快门模式:1872/1980b | 10000016/10000045b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-17uc | 滚动快门模式:13/16b 全局重置释放快门模式:468/576b | 10000003/10000000b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-17ucMED | 滚动快门模式:13/16b 全局重置释放快门模式:468/576b | 10000003/10000000b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-17um | 滚动快门模式:13/16b 全局重置释放快门模式:468/576b | 10000003/10000000b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
acA5472-17umMED | 滚动快门模式:13/16b 全局重置释放快门模式:468/576b | 10000003/10000000b | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA1936-400cc | Common exposure time mode: 7/7/8g Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 4 | Common Ultra Short | 常规 |
boA1936-400cm | Common exposure time mode: 7/7/8g Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 4 | Common Ultra Short | 常规 |
boA2448-250cc | Common exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
bo2448-250cm | Common exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA2832-190cc | Common exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
bo2832-190cm | Common exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA4096-93cc | Common exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Common exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Common Ultra Short | 常规 |
boA4096-93cm | Common exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Common exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Common Ultra Short | 常规 |
boA4096-180cc | Common exposure time mode: 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
bo4096-180cm | Common exposure time mode (sensor binning disabled): 5 / 5 / 6 / 10 / 10 / 14k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA4112-68cc | Common exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Common exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Common Ultra Short | 常规 |
boA4112-68cm | Common exposure time mode: 21/21/23g Ultra Short exposure time mode: 2/2/2g | Common exposure time mode: 8000000/8000000/8000000g Ultra Short exposure time mode: 16/16/16g | Common Ultra Short | 常规 |
boA4500-45cc | Common exposure time mode: 100 Short exposure time mode: 20 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA4500-45cm | Common exposure time mode: 100 Short exposure time mode: 20 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA4504-100cc | Common exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA4504-100cm | Common exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA5120-150cc | Common exposure time mode: 8 Ultra Short exposure time mode: 2 | Common exposure time mode: 1 / frame rate Ultra Short exposure time mode: 7 | Common Ultra Short | ExposureTimeSelector parameter not available |
boA5120-150cm | Common exposure time mode: 8 Ultra Short exposure time mode: 2 | Common exposure time mode: 1 / frame rate Ultra Short exposure time mode: 7 | Common Ultra Short | ExposureTimeSelector parameter not available |
boA5120-230cc | 4 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA5120-230cm | 4 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA5320-150cc | Common exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA5320-150cm | Common exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA5328-100cc | Common exposure time mode: 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA5328-100cm | Common exposure time mode (sensor binning disabled): 5 / 6 / 6 / 11 / 12 / 15k Ultra Short exposure time mode: 1l | Common exposure time mode: 8000000 Ultra Short exposure time mode: 2 | Common Ultra Short | 常规 |
boA6500-36cc | Common exposure time mode: 100 Short exposure time mode: 20 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA6500-36cm | Common exposure time mode: 100 Short exposure time mode: 20 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA8100-16cc | Common exposure time mode: 100 Short exposure time mode: 45 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA8100-16cm | Common exposure time mode: 100 Short exposure time mode: 45 | Common exposure time mode: 8000000 Short exposure time mode: 100 | Common Short | 常规 |
boA9344-30cc | 12 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA9344-30cm | 12 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA9344-70cc | 12 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA9344-70cm | 12 | 1 / 帧速率 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
boA13440-17cm | 8-bit sensor bit depth: 551 | 8000000 | 常规 | 常规 |
daA720-520uc | 18/18/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA720-520um | 18/18/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1280-54uc | 10de | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1280-54um | 10de | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1440-220uc | 18/18/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1440-220um | 18/18/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1600-60uc | 10d | 850000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1600-60um | 10d | 850000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1920-15um | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1920-30uc | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1920-30um | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1920-160uc | 19/19/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA1920-160um | 19/19/20g | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA2448-70uc | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA2448-70um | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA2500-14uc | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA2500-14um | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA3840-45uc | 26dh | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
daA3840-45um | 26dh | 999999 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA720-290gc | Common exposure time mode: 18 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA720-290gm | Common exposure time mode: 18 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA1440-73gc | Common exposure time mode: 18 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA1440-73gm | Common exposure time mode: 18 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA1920-51gc | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA1920-51gm | Common exposure time mode: 19 Ultra Short exposure time mode: 1 | Common exposure time mode: 10000000 Ultra Short exposure time mode: 14 | Common Ultra Short | 常规 |
dmA2048-37gc | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA2048-37gm | 9 | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA2448-23gc | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA2448-23gm | 10/11i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA2840-14gc | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA2840-14gm | 10/12i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA3536-9gc | 12 | 10000000 | 常规 | 常规 |
dmA3536-9gm | 12 | 10000000 | 常规 | 常规 |
dmA4096-9gc | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
dmA4096-9gm | 13/15i | 10000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1280-54uc | 10de | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1280-54um | 10de | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1600-60uc | 10d | 850000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1600-60um | 10d | 850000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1920-30uc | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA1920-30um | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA2500-14uc | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
puA2500-14um | 10d | 1000000 | ExposureTimeMode 参数不可用 | ExposureTimeSelector parameter not available |
r2L2048-29gc | 3.15 | 1000000 | 常规 | 常规 |
r2L2048-58gm | 1.57 | 1000000 | 常规 | 常规 |
r2L2048-62cc | 3.15 | 1000000 | 常规 | 常规 |
r2L2048-62g5c | 3.15 | 1000000 | 常规 | 常规 |
r2L2048-172cm | 1.57 | 1000000 | 常规 | 常规 |
r2L2048-172g5m | 1.57 | 1000000 | 常规 | 常规 |
r2L4096-14gc | 3.15 | 1000000 | 常规 | 常规 |
r2L4096-29gm | 2.1 | 1000000 | 常规 | 常规 |
r2L4096-42cc | 3.15 | 1000000 | 常规 | 常规 |
r2L4096-42g5c | 3.15 | 1000000 | 常规 | 常规 |
r2L4096-84cm | 2.1 | 1000000 | 常规 | 常规 |
r2L4096-84g5m | 2.1 | 1000000 | 常规 | 常规 |
r2L8192-200cm | Common exposure time mode: 3.07 Individual exposure time mode: Stage 1: 3.07 Stage 2: 3.07 | Common exposure time mode: 1000000 Individual exposure time mode: Stage 1: 1000000 Stage 2: 1000000 | Common Individual | Common Stage1 Stage2 |
r2L16384-120cm | Common exposure time mode: 2.56 Individual exposure time mode: Stage 1: 2.56 Stage 2: 2.56 | Common exposure time mode: 1000000 Individual exposure time mode: Stage 1: 1000000 Stage 2: 1000000 | Common Individual | Common Stage1 Stage2 |
-
全局快门模式/滚动快门模式
-
8 位像素格式/12 位像素格式
-
pixel format 设置为 12 位格式时有效。对于 8 位格式,该值取决于可用的 USB 3.0 带宽。请参见下面的表 1。
-
根据相机的传感器和帧速率,有效 exposure time 可能会与设置的 exposure time 有所不同。该变化通常在数微秒之间,但是如果设置了很短的 exposure time,则应考虑到这一点。
-
由于传感器的特定特性,在曝光时间低于 ≈70 µs 时,增量可能会有所变化,并且可能会高于 1 µs。因此,并非所有曝光时间值都能实现。此行为还取决于 Image ROI 设置和重叠模式。
-
8 位传感器位深度/10 位传感器位深度/12 位传感器位深度
-
在默认设置下有效。值取决于可用的 USB 3.0 带宽(
DeviceLinkThroughputLimit
参数设置)。 -
10 位传感器位深度 / 12位传感器位深度
-
在 Ultra Short 曝光时间模式下设置 2 µs 或 3 µs 的曝光时间时,有效曝光时间可能会比指定的时间稍长。差值不到一微秒。
-
2x CXP(AUX 电源或 PoCXP)或 1x CXP(AUX 电源)(8 位传感器位深)/2x CXP(AUX 电源或 PoCXP)或 1x CXP(AUX 电源)(10 位传感器位深)/2x CXP(AUX 电源或 PoCXP)或 1x CXP(AUX 电源)(12 位传感器位深)/1x CXP (PoCXP)(8 位传感器位深)/1x CXP (PoCXP)(10 位传感器位深)/1x CXP (PoCXP)(12 位传感器位深)
-
将 Ultra Short 曝光时间模式下的曝光时间设置为 1 µs 或 2 µs 时,产生的图像亮度可能高于预期。
-
The exposure time value set for stage 1 limits the maximum possible exposure time value for stage 2, which is additionally reduced by 1 µs. For example, if you set the exposure time for stage 1 to 100 µs, the maximum exposure time for stage 2 is limited to 99 µs.
有关 ace Classic 相机的其他信息#
表 1#
下表适用于使用 8 位 pixel format 的 acA2040-90uc/um/umNIR 和 acA2000-165uc/um/umNIR 相机。
可用 USB 带宽 (设备链路吞吐量) | 最小 Exposure time 和 Exposure time 偏移量 (8 位 pixel format) |
---|---|
≤ 108000 | 42 |
108001–140000 | 32 |
140001–160020 | 28 |
160021–180000 | 25 |
180001–192112 | 24 |
192113–216000 | 42 |
216001–280000 | 32 |
280001–320040 | 28 |
320041–360000 | 25 |
360001–384224 | 24 |
表 2#
下表适用于在全局重置释放 shutter mode 下操作的指定相机型号。
相机型号 | 额外 Exposure time(单位为 GRR [µs]) |
---|---|
acA3800-10gm/gc | 5218 |
acA3800-14um/uc | 4077 |
Example: Assume you are operating an acA3800-10gm camera in Global Reset Release shutter mode. You set the exposure time to 1000 µs. The effective exposure time is 1000 + 5218 = 6218 µs.
示例代码#
ace Classic/U/L GigE 相机#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTimeAbs", &d);
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTimeAbs", 3500.0);
CHECK(errRes);
ace 2, boost, and dart M/R Cameras#
// Determine the current exposure time using Exposure Time
double d = camera.ExposureTime.GetValue();
// Determine the current exposure time using Effective Exposure Time
double d = camera.BslEffectiveExposureTime.GetValue();
// Set the exposure time mode to Common
camera.ExposureTimeMode.SetValue(ExposureTimeMode_Common);
// Set the exposure time to 3500 microseconds
camera.ExposureTime.SetValue(3500.0);
INodeMap& nodemap = camera.GetNodeMap();
// Determine the current exposure time using Exposure Time
double d = CFloatParameter(nodemap, "ExposureTime").GetValue();
// Determine the current exposure time using Effective Exposure Time
d = CFloatParameter(nodemap, "BslEffectiveExposureTime").GetValue();
// Set the exposure time mode to Common
CEnumParameter(nodemap, "ExposureTimeMode").SetValue("Common");
// Set the exposure time to 3500 microseconds
CFloatParameter(nodemap, "ExposureTime").SetValue(3500.0);
// Determine the current exposure time using Exposure Time
double d = camera.Parameters[PLCamera.ExposureTime].GetValue();
// Determine the current exposure time using Effective Exposure Time
d = camera.Parameters[PLCamera.BslEffectiveExposureTime].GetValue();
// Set the exposure time mode to Common
camera.Parameters[PLCamera.ExposureTimeMode].SetValue(PLCamera.ExposureTimeMode.Common);
// Set the exposure time to 3500 microseconds
camera.Parameters[PLCamera.ExposureTime].SetValue(3500.0);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time using Exposure Time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTime", &d);
CHECK(errRes);
/* Determine the current exposure time using Effective Exposure Time */
errRes = PylonDeviceGetFloatFeature(hdev, "BslEffectiveExposureTime", &d);
CHECK(errRes);
/* Set the exposure time mode to Common */
errRes = PylonDeviceFeatureFromString(hdev, "ExposureTimeMode", "Common");
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 3500.0);
CHECK(errRes);
# Determine the current exposure time using Exposure Time
d = camera.ExposureTime.Value
# Determine the current exposure time using Effective Exposure Time
d = camera.BslEffectiveExposureTime.Value
# Set the exposure time mode to Common
camera.ExposureTimeMode.Value = "Common"
# Set the exposure time to 3500 microseconds
camera.ExposureTime.Value = 3500.0
其他相机#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Determine the current exposure time */
errRes = PylonDeviceGetFloatFeature(hdev, "ExposureTime", &d);
CHECK(errRes);
/* Set the exposure time to 3500 microseconds */
errRes = PylonDeviceSetFloatFeature(hdev, "ExposureTime", 3500.0);
CHECK(errRes);
您也可以使用 pylon Viewer 轻松设置参数。