跳转到内容

Gain#

相机的 Gain 功能可让您增加相机输出图像的亮度。

Increasing the gain increases all pixel values of the images.

要自动调整增益值,请使用 Gain Auto 功能。

该功能的使用#

模拟和数字增益#

The gain is an amplification factor applied to all pixel values of the acquired images. There are different types of gains:

  • Analog gain is applied before the signal from the camera sensor is converted into digital values.
  • Digital gain is applied after the conversion, i.e., it is basically a multiplication of the digitized values.

Depending on your camera model, the mechanisms to control the gain can vary:

  • 对于部分相机,增益控制为模拟式,并且达到一定阈值。高于阈值时,增益控制为数字式。
  • For some cameras, gain control is entirely digital or analog.
  • For some cameras, you can use the GainSelector parameter to manually switch between analog and digital gain.

Choosing the Gain Type#

On some camera models, the GainSelector parameter is available. This parameter allows you to apply a universal gain, which can be analog, digital, or both, depending on your camera model and the sensor used. The GainSelector parameter also allows you to manually switch between analog and digital gain (if available).

racer 2 L cameras, the GainSelector parameter can be used to apply the gain to a specific sensor line if the camera is operated in Dual Line sensor acquisition mode.

You can set the GainSelector parameter to one of the following values, if available:

  • All: A universal gain is applied.
  • AnalogAll: An analog gain is applied.
  • DigitalAll: A digital gain is applied.
  • Line1: A digital gain is applied to line 1.
  • Line2: A digital gain is applied to line 2.

信息

For racer 2 L cameras, consider the following:

  • The gain value specified for line 2 only becomes effective if the Dual Line sensor acquisition mode is enabled.
  • The gain value finally applied to line 1 and line 2 is the sum of the gain value specified for All plus the gain value specified for Line1Line2 respectively.

Conversion Gain Mode#

On a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras, the BslConversionGainMode parameter is available. It allows you to select one of the following conversion gain modes:

  • High: Enables the High Conversion Gain (HCG) mode.
    HCG helps to improve image quality in low light conditions. The sensitivity is increased and the readout noise reduced, which results in an improved signal-to-noise ratio, but a lower dynamic range.
  • Low: Enables the Low Conversion Gain (LCG) mode.
    LCG is recommended for normal to bright light conditions. The saturation capacity is increased and the dynamic range is higher.

“原始”和绝对增益值#

部分相机机型上,必须以整数比例将增益输入为“原始”值。相机需要其内部处理机制的原始值。但是,原始值与实际增益值不同,实际增益值以分贝 (dB) 表示。

在特定于相机的 Gain Properties 表中,您可以找到一个公式,可以根据原始增益值计算绝对增益(以 dB 为单位)。

附加参数#

On boA13440-17cm cameras, the BslGainTopLeft, BslGainTopRight, BslGainBottomLeft, and BslGainBottomRight parameters are available. You can use these parameters to increase the brightness individually in each of the four quadrants of the image. This can be useful to compensate for differences in the image brightness.

The brightness in each quadrant can be increased linearly by up to 5 % (digital gain).

Setting the Gain#

  1. 设置 GainAuto parameter to Off.
  2. 如果可用,请设置 GainSelector parameter to the desired gain type, e.g., All.
  3. 如果可用,请设置 BslConversionGain parameter to the desired conversion gain mode, e.g., High.
  4. 设置 Gain parameter to the desired value.
    The minimum and maximum parameter values vary depending on the camera model, the pixel format chosen, and the Binning settings.

详情#

增益属性#

显示所有相机型号

相机型号 增益控制机制 阈值 增益必须以如下形式输入 根据原始增益值计算增益的公式
a2A640-240gmSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A640-240umSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1280-80gmSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1280-125umSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-51gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-51gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-51gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-51gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-160ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-160ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-160umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-160umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-165g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A1920-165g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2048-35gmSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2048-110umSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2440-98g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2440-98g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-23gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-23gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-23gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-23gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-75ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-75ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-75umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-75umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-105g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-105g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-120cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-120cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-210cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2448-210cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2560-20gmSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2560-70umSWIR 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2590-22gcBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-22gcPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-22gmBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-22gmPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-60ucBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-60ucPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-60umBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2590-60umPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A2600-20gcBAS 仅数字增益 0 dB 不适用
a2A2600-20gcPRO 仅数字增益 0 dB 不适用
a2A2600-20gmBAS 仅数字增益 0 dB 不适用
a2A2600-20gmPRO 仅数字增益 0 dB 不适用
a2A2600-64ucBAS 仅数字增益 0 dB 不适用
a2A2600-64ucPRO 仅数字增益 0 dB 不适用
a2A2600-64umBAS 仅数字增益 0 dB 不适用
a2A2600-64umPRO 仅数字增益 0 dB 不适用
a2A2840-14gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-14gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-14gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-14gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-14gmUV 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-48ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-48ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-48umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-48umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-48umUV 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-67g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-67g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-67g5mUV 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-86cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A2840-86cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A3536-9gcBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-9gcPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-9gmBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-9gmPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-31ucBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-31ucPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-31umBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-31umPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-42g5cBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3536-42g5mBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-13gcBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-13gcPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-13gmBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-13gmPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-45ucBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-45ucPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-45umBAS 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A3840-45umPRO 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
a2A4096-9gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-9gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-9gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-9gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-30ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-30ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-30umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-30umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-44g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-44g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-67cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4096-67cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4200-12gcBAS 仅数字增益 0 dB 不适用
a2A4200-12gcPRO 仅数字增益 0 dB 不适用
a2A4200-12gmBAS 仅数字增益 0 dB 不适用
a2A4200-12gmPRO 仅数字增益 0 dB 不适用
a2A4200-40ucBAS 仅数字增益 0 dB 不适用
a2A4200-40ucPRO 仅数字增益 0 dB 不适用
a2A4200-40umBAS 仅数字增益 0 dB 不适用
a2A4200-40umPRO 仅数字增益 0 dB 不适用
a2A4504-5gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-5gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-5gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-5gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-18ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-18ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-18umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-18umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-27g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-27g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-42cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4504-42cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A4508-6gcBAS 仅数字增益 0 dB 不适用
a2A4508-6gcPRO 仅数字增益 0 dB 不适用
a2A4508-6gmBAS 仅数字增益 0 dB 不适用
a2A4508-6gmPRO 仅数字增益 0 dB 不适用
a2A4508-20ucBAS 仅数字增益 0 dB 不适用
a2A4508-20ucPRO 仅数字增益 0 dB 不适用
a2A4508-20umBAS 仅数字增益 0 dB 不适用
a2A4508-20umPRO 仅数字增益 0 dB 不适用
a2A5060-4gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5060-4gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5060-15ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5060-15umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5060-21g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5060-21g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-7gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-7gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-7gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-7gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-23ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-23ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-23umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-23umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-34g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-34g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-52cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5320-52cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-4gcBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-4gcPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-4gmBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-4gmPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-15ucBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-15ucPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-15umBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-15umPRO 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-22g5cBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-22g5mBAS 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-35cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
a2A5328-35cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA640-121gm 高于阈值时,模拟增益自动切换为数字增益 不适用 原始 Gain = 0.0359 * Gain原始(Sony ICX618 替换件ace)
acA640-300gc 仅限数字控制 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA640-300gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA640-750uc 仅数字增益 - dB 不适用
acA640-750um 仅数字增益 - dB 不适用
acA720-290gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA720-290gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA720-520uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA720-520um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA800-200gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA800-200gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA800-510uc 仅数字增益 - dB 不适用
acA800-510um 仅数字增益 - dB 不适用
acA1280-60gc 可通过 GainSelector 参数设置增益控制。 - 原始 Analog Gain: - Gain is 0 when GainRaw is set to 0
- Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1280-60gm 可通过 GainSelector 参数设置增益控制。 - 原始 Analog Gain: - Gain is 0 when GainRaw is set to 0
- Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1300-60gc 可通过 GainSelector 参数设置增益控制。 - 原始 Analog Gain: - Gain is 0 when GainRaw is set to 0
- Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1300-60gm 可通过 GainSelector 参数设置增益控制。 - 原始 Analog Gain: - Gain is 0 when GainRaw is set to 0
- Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1300-60gmNIR 可通过 GainSelector 参数设置增益控制。 - 原始 Analog Gain: - Gain is 0 when GainRaw is set to 0
- Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1300-75gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA1300-75gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA1300-200uc 仅数字增益 - dB 不适用
acA1300-200um 仅数字增益 - dB 不适用
acA1440-73gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1440-73gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1440-220uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1440-220um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1600-20gc 高于阈值时,模拟增益自动切换为数字增益 511 原始 增益 = 0.0359 * GainRaw
acA1600-20uc 高于阈值时,模拟增益自动切换为数字增益 10.1 dB 不适用
acA1600-60gc 可通过 GainSelector 参数设置增益控制 - 原始 Analog Gain: - Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1600-60gm 可通过 GainSelector 参数设置增益控制 - 原始 Analog Gain: - Gain is 3.5 when GainRaw is set to 1
- Gain is 6 when GainRaw is set to 2
- Gain is 9.5 when GainRaw is set to 3
Digital Gain: - Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw < 32
- Gain = 20 * log10 (1 + ((GainRaw * 2) / 64)) for all GainRaw ≥ 32
acA1920-25gc 高于阈值时,模拟增益自动切换为数字增益 19 原始 请参见此图以获取近似值。
acA1920-25gm 高于阈值时,模拟增益自动切换为数字增益 19 原始 请参见此图以获取近似值。
acA1920-25uc 仅数字增益 - dB 不适用
acA1920-25um 仅数字增益 - dB 不适用
acA1920-40gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1920-40gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1920-40uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-40ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-40um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-40umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-48gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA1920-48gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA1920-50gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1920-50gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA1920-150uc 仅数字增益 - dB 不适用
acA1920-150um 仅数字增益 - dB 不适用
acA1920-155uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-155ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-155um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA1920-155umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2000-50gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA2000-50gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA2000-165uc 仅数字增益 - dB 不适用
acA2000-165um 仅数字增益 - dB 不适用
acA2040-25gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA2040-25gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA2040-25gmNIR 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA2040-35gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA2040-35gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA2040-55uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2040-55um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2040-90uc 仅数字增益 - dB 不适用
acA2040-90um 仅数字增益 - dB 不适用
acA2040-90umNIR 仅数字增益 - dB 不适用
acA2040-120uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2040-120um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-20gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA2440-20gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA2440-35uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-35ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-35um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-35umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-75uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-75ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-75um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2440-75umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA2500-14gc 高于阈值时,模拟增益自动切换为数字增益 19 原始 请参见此图以获取近似值。
acA2500-14gm 高于阈值时,模拟增益自动切换为数字增益 19 原始 请参见此图以获取近似值。
acA2500-14uc 仅数字增益 - dB 不适用
acA2500-14um 仅数字增益 - dB 不适用
acA2500-20gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA2500-20gcMED 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA2500-20gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA2500-20gmMED 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 136)
acA2500-60uc 仅数字增益 - dB 不适用
acA2500-60um 仅数字增益 - dB 不适用
acA3088-16gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA3088-16gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA3088-57uc 仅模拟增益 - dB 不适用
acA3088-57ucMED 仅模拟增益 - dB 不适用
acA3088-57um 仅模拟增益 - dB 不适用
acA3088-57umMED 仅模拟增益 - dB 不适用
acA3800-10gc 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA3800-10gm 仅数字增益 - 原始 增益 = 20 * log10 (GainRaw / 32)
acA3800-14uc 仅数字增益 - dB 不适用
acA3800-14um 仅数字增益 - dB 不适用
acA4024-8gc 仅模拟增益 - 原始 Gain = -20 * log10 ((2048-GainRaw) / 2048)
acA4024-8gm 仅模拟增益 - 原始 Gain = -20 * log10 ((2048-GainRaw) / 2048)
acA4024-29uc 仅模拟增益 - dB 不适用
acA4024-29um 仅模拟增益 - dB 不适用
acA4096-11gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA4096-11gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA4096-30uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-30ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-30um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-30umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-40uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-40ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-40um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4096-40umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-8gc 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA4112-8gm 高于阈值时,模拟增益自动切换为数字增益 240 原始 增益 = 0.1 * GainRaw
acA4112-20uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-20ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-20um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-20umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-30uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-30ucMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-30um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA4112-30umMED 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
acA5472-5gc 仅模拟增益 - 原始 Gain = -20 * log10 ((2048-GainRaw) / 2048)
acA5472-5gm 仅模拟增益 - 原始 Gain = -20 * log10 ((2048-GainRaw) / 2048)
acA5472-17uc 仅模拟增益 - dB 不适用
acA5472-17ucMED 仅模拟增益 - dB 不适用
acA5472-17um 仅模拟增益 - dB 不适用
acA5472-17umMED 仅模拟增益 - dB 不适用
boA1936-400cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA1936-400cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA2448-250cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
bo2448-250cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA2832-190cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
bo2832-190cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4096-93cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4096-93cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4096-180cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
bo4096-180cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4112-68cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4112-68cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4500-45cc 模拟和数字增益的组合 - dB 不适用
boA4500-45cm 模拟和数字增益的组合 - dB 不适用
boA4504-100cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA4504-100cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA5120-150cc 仅数字增益 - dB 不适用
boA5120-150cm 仅数字增益 - dB 不适用
boA5120-230cc 仅数字增益 - dB 不适用
boA5120-230cm 仅数字增益 - dB 不适用
boA5320-150cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA5320-150cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA5328-100cc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA5328-100cm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
boA6500-36cc 模拟和数字增益的组合 - dB 不适用
boA6500-36cm 模拟和数字增益的组合 - dB 不适用
boA8100-16cc 模拟和数字增益的组合 - dB 不适用
boA8100-16cm 模拟和数字增益的组合 - dB 不适用
boA9344-30cc 仅数字增益 - dB 不适用
boA9344-30cm 仅数字增益 - dB 不适用
boA9344-70cc 仅数字增益 - dB 不适用
boA9344-70cm 仅数字增益 - dB 不适用
boA13440-17cm 仅模拟增益 - dB 不适用
daA720-520uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA720-520um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA1280-54uc 仅数字增益 - dB 不适用
daA1280-54um 仅数字增益 - dB 不适用
daA1440-220uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA1440-220um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA1600-60uc 仅数字增益 - dB 不适用
daA1600-60um 仅数字增益 - dB 不适用
daA1920-15um 仅数字增益 - dB 不适用
daA1920-30uc 仅数字增益 - dB 不适用
daA1920-30um 仅数字增益 - dB 不适用
daA1920-160uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA1920-160um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA2448-70uc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA2448-70um 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
daA2500-14uc 仅数字增益 - dB 不适用
daA2500-14um 仅数字增益 - dB 不适用
daA3840-45uc 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
daA3840-45um 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
dmA720-290gc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA720-290gm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA1440-73gc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA1440-73gm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA1920-51gc 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA1920-51gm 高于阈值时,模拟增益自动切换为数字增益 24 dB 不适用
dmA3536-9gc 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
dmA3536-9gm 高于阈值时,模拟增益自动切换为数字增益 30 dB 不适用
puA1280-54uc 仅数字增益 - dB 不适用
puA1280-54um 仅数字增益 - dB 不适用
puA1600-60uc 仅数字增益 - dB 不适用
puA1600-60um 仅数字增益 - dB 不适用
puA1920-30uc 仅数字增益 - dB 不适用
puA1920-30um 仅数字增益 - dB 不适用
puA2500-14uc 仅数字增益 - dB 不适用
puA2500-14um 仅数字增益 - dB 不适用
r2L2048-29gc 仅数字增益 - dB 不适用
r2L2048-58gm 仅数字增益 - dB 不适用
r2L2048-62cc 仅数字增益 - dB 不适用
r2L2048-62g5c 仅数字增益 - dB 不适用
r2L2048-172cm 仅数字增益 - dB 不适用
r2L2048-172g5m 仅数字增益 - dB 不适用
r2L4096-14gc 仅数字增益 - dB 不适用
r2L4096-29gm 仅数字增益 - dB 不适用
r2L4096-42cc 仅数字增益 - dB 不适用
r2L4096-42g5c 仅数字增益 - dB 不适用
r2L4096-84cm 仅数字增益 - dB 不适用
r2L4096-84g5m 仅数字增益 - dB 不适用
r2L8192-200cm 仅数字增益 - dB 不适用
r2L16384-120cm 仅数字增益 - dB 不适用

增益值#

信息

在部分相机机型上,可以使用 Remove Parameter Limits 功能提高增益参数的上限。

显示所有相机型号

相机型号 最小增益设置 启用垂直像素合并的最小增益设置 最大增益设置(8 位像素格式) 最大增益设置(10 位像素格式) 最大增益设置(12 位像素格式)
a2A640-240gmSWIR 0 0 42 42 42
a2A640-240umSWIR 0 0 42 42 42
a2A1280-80gmSWIR 0 0 42 42 42
a2A1280-125umSWIR 0 0 42 42 42
a2A1920-51gcBAS 0 - 48 48 48
a2A1920-51gcPRO 0 - 48 48 48
a2A1920-51gmBAS 0 0 48 48 48
a2A1920-51gmPRO 0 0 48 48 48
a2A1920-160ucBAS 0 - 48 48 48
a2A1920-160ucPRO 0 - 48 48 48
a2A1920-160umBAS 0 0 48 48 48
a2A1920-160umPRO 0 0 48 48 48
a2A1920-165g5cBAS 0 - 48 48 48
a2A1920-165g5mBAS 0 0 48 48 48
a2A2048-35gmSWIR 0 0 42 42 42
a2A2048-110umSWIR 0 0 42 42 42
a2A2440-98g5cBAS 0 - 48 48 48
a2A2440-98g5mBAS 0 0 48 48 48
a2A2448-23gcBAS 0 - - 48 48
a2A2448-23gcPRO 0 - - 48 48
a2A2448-23gmBAS 0 0 48 - 48
a2A2448-23gmPRO 0 0 48 - 48
a2A2448-75ucBAS 0 - - 48 48
a2A2448-75ucPRO 0 - - 48 48
a2A2448-75umBAS 0 0 48 - 48
a2A2448-75umPRO 0 0 48 - 48
a2A2448-105g5cBAS 0 - - 48 48
a2A2448-105g5mBAS 0 0 48 - 48
a2A2448-120cc 0 - 48 48 48
a2A2448-120cm 0 0 48 48 48
a2A2448-210cc 0 - 48 48 48
a2A2448-210cm 0 0 48 48 48
a2A2560-20gmSWIR 0 0 42 42 42
a2A2560-70umSWIR 0 0 42 42 42
a2A2590-22gcBAS 0 - 48 48 48
a2A2590-22gcPRO 0 - 48 48 48
a2A2590-22gmBAS 0 0 48 48 48
a2A2590-22gmPRO 0 0 48 48 48
a2A2590-60ucBAS 0 - 48 48 48
a2A2590-60ucPRO 0 - 48 48 48
a2A2590-60umBAS 0 0 48 48 48
a2A2590-60umPRO 0 0 48 48 48
a2A2600-20gcBAS 0 - 36 36 36
a2A2600-20gcPRO 0 - 36 36 36
a2A2600-20gmBAS 0 0 36 36 36
a2A2600-20gmPRO 0 0 36 36 36
a2A2600-64ucBAS 0 - 36 36 36
a2A2600-64ucPRO 0 - 36 36 36
a2A2600-64umBAS 0 0 36 36 36
a2A2600-64umPRO 0 0 36 36 36
a2A2840-14gcBAS 0 - - 48 48
a2A2840-14gcPRO 0 - - 48 48
a2A2840-14gmBAS 0 0 48 - 48
a2A2840-14gmPRO 0 0 48 - 48
a2A2840-14gmUV 0 0 48 48 48
a2A2840-48ucBAS 0 - - 48 48
a2A2840-48ucPRO 0 - - 48 48
a2A2840-48umBAS 0 0 48 - 48
a2A2840-48umPRO 0 0 48 - 48
a2A2840-48umUV 0 0 48 48 48
a2A2840-67g5cBAS 0 - - 48 48
a2A2840-67g5mBAS 0 0 48 - 48
a2A2840-67g5mUV 0 0 48 48 48
a2A2840-86cc 0 - 48 48 48
a2A2840-86cm 0 0 48 - 48
a2A3536-9gcBAS 0 - 48 48 48
a2A3536-9gcPRO 0 - 48 48 48
a2A3536-9gmBAS 0 0 48 48 48
a2A3536-9gmPRO 0 0 48 48 48
a2A3536-31ucBAS 0 - 48 48 48
a2A3536-31ucPRO 0 - 48 48 48
a2A3536-31umBAS 0 0 48 48 48
a2A3536-31umPRO 0 0 48 48 48
a2A3536-42g5cBAS 0 - 48 48 48
a2A3536-42g5mBAS 0 0 48 48 48
a2A3840-13gcBAS 0 - 48 48 48
a2A3840-13gcPRO 0 - 48 48 48
a2A3840-13gmBAS 0 0 48 48 48
a2A3840-13gmPRO 0 0 48 48 48
a2A3840-45ucBAS 0 - 48 48 48
a2A3840-45ucPRO 0 - 48 48 48
a2A3840-45umBAS 0 0 48 48 48
a2A3840-45umPRO 0 0 48 48 48
a2A4096-9gcBAS 0 - - 48 48
a2A4096-9gcPRO 0 - - 48 48
a2A4096-9gmBAS 0 0 48 - 48
a2A4096-9gmPRO 0 0 48 - 48
a2A4096-30ucBAS 0 - - 48 48
a2A4096-30ucPRO 0 - - 48 48
a2A4096-30umBAS 0 0 48 - 48
a2A4096-30umPRO 0 0 48 - 48
a2A4096-44g5cBAS 0 - - 48 48
a2A4096-44g5mBAS 0 0 48 - 48
a2A4096-67cc 0 - 48 48 48
a2A4096-67cm 0 0 48 48 48
a2A4200-12gcBAS 0 - 36 36 36
a2A4200-12gcPRO 0 - 36 36 36
a2A4200-12gmBAS 0 0 36 36 36
a2A4200-12gmPRO 0 0 36 36 36
a2A4200-40ucBAS 0 - 36 36 36
a2A4200-40ucPRO 0 - 36 36 36
a2A4200-40umBAS 0 0 36 36 36
a2A4200-40umPRO 0 0 36 36 36
a2A4504-5gcBAS 0 - - 48 48
a2A4504-5gcPRO 0 - - 48 48
a2A4504-5gmBAS 0 0 48 - 48
a2A4504-5gmPRO 0 0 48 - 48
a2A4504-18ucBAS 0 - - 48 48
a2A4504-18ucPRO 0 - - 48 48
a2A4504-18umBAS 0 0 48 - 48
a2A4504-18umPRO 0 0 48 - 48
a2A4504-27g5cBAS 0 - - 48 48
a2A4504-27g5mBAS 0 0 48 - 48
a2A4504-42cc 0 - 48 48 48
a2A4504-42cm 0 0 48 48 48
a2A4508-6gcBAS 0 - 36 36 36
a2A4508-6gcPRO 0 - 36 36 36
a2A4508-6gmBAS 0 0 36 36 36
a2A4508-6gmPRO 0 0 36 36 36
a2A4508-20ucBAS 0 - 36 36 36
a2A4508-20ucPRO 0 - 36 36 36
a2A4508-20umBAS 0 0 36 36 36
a2A4508-20umPRO 0 0 36 36 36
a2A5060-4gcBAS 0 - - 48 48
a2A5060-4gmBAS 0 0 48 - 48
a2A5060-15ucBAS 0 - - 48 48
a2A5060-15umBAS 0 0 48 - 48
a2A5060-21g5cBAS 0 - - 48 48
a2A5060-21g5mBAS 0 0 48 - 48
a2A5320-7gcBAS 0 - - 48 48
a2A5320-7gcPRO 0 - - 48 48
a2A5320-7gmBAS 0 0 48 - 48
a2A5320-7gmPRO 0 0 48 - 48
a2A5320-23ucBAS 0 - - 48 48
a2A5320-23ucPRO 0 - - 48 48
a2A5320-23umBAS 0 0 48 - 48
a2A5320-23umPRO 0 0 48 - 48
a2A5320-34g5cBAS 0 - - 48 48
a2A5320-34g5mBAS 0 0 48 - 48
a2A5320-52cc 0 - 48 48 48
a2A5320-52cm 0 0 48 48 48
a2A5328-4gcBAS 0 - - 48 48
a2A5328-4gcPRO 0 - - 48 48
a2A5328-4gmBAS 0 0 48 - 48
a2A5328-4gmPRO 0 0 48 - 48
a2A5328-15ucBAS 0 - - 48 48
a2A5328-15ucPRO 0 - - 48 48
a2A5328-15umBAS 0 0 48 - 48
a2A5328-15umPRO 0 0 48 - 48
a2A5328-22g5cBAS 0 - - 48 48
a2A5328-22g5mBAS 0 0 48 - 48
a2A5328-35cc 0 - 48 48 48
a2A5328-35cm 0 0 48 48 48
acA640-121gm 0 0 1023 - 600
acA640-300gc 136 - 542 542 -
acA640-300gm 136 136 542 542 -
acA640-750uc 0 - 12 12 -
acA640-750um 0 0 12 12 -
acA720-290gc 0 - 360 - 240
acA720-290gm 0 0 360 - 240
acA720-520uc 0 - 36 - 24
acA720-520um 0 0 36 - 24
acA800-200gc 136 - 542 542 -
acA800-200gm 136 136 542 542 -
acA800-510uc 0 - 12 12 -
acA800-510um 0 0 12 12 -
acA1280-60gc 0 - - - 3/95a
acA1280-60gm 0 0 - - 3/95a
acA1300-60gc 0 - - - 3/95a
acA1300-60gm 0 0 - - 3/95a
acA1300-60gmNIR 0 0 - - 3/95a
acA1300-75gc 136 - 542 542 -
acA1300-75gm 136 136 542 542 -
acA1300-200uc 0 - 12 12 -
acA1300-200um 0 0 12 12 -
acA1440-73gc 0 - 360 - 240
acA1440-73gm 0 0 360 - 240
acA1440-220uc 0 - 36 - 24
acA1440-220um 0 0 36 - 24
acA1600-20gc 230 - 850 - 400
acA1600-20uc 0 - 22.25800 - 6.10300
acA1600-60gc 1/0a - - - 3/95a
acA1600-60gm 1/0a 1/0a - - 3/95a
acA1920-25gc 0 - 63 - 63
acA1920-25gm 0 0 63 - 63
acA1920-25uc 0 - 23.79814 - 23.79814
acA1920-25um 0 0 23.79814 - 23.79814
acA1920-40gc 0 0 360 - 240
acA1920-40gm 0 0 360 - 240
acA1920-40uc 0 - 36 - 24
acA1920-40ucMED 0 0 36 - 24
acA1920-40um 0 0 36 24
acA1920-40umMED 0 0 36 - 24
acA1920-48gc 136 - 542 542 -
acA1920-48gm 136 136 542 542 -
acA1920-50gc 0 - 360 - 240
acA1920-50gm 0 0 360 - 240
acA1920-150uc 0 - 12 12 -
acA1920-150um 0 0 12 12 -
acA1920-155uc 0 - 36 - 24
acA1920-155ucMED 0 - 36 - 24
acA1920-155um 0 0 36 - 24
acA1920-155umMED 0 0 36 - 24
acA2000-50gc 36 - 512 - 512
acA2000-50gm 36 33 512 - 512
acA2000-165uc 0 - 23.59350 - 23.59350
acA2000-165um 0 0 23.59350 - 23.59350
acA2040-25gc 36 - 512 - 512
acA2040-25gm 36 33 512 - 512
acA2040-25gmNIR 36 33 512 - 512
acA2040-35gc 0 - 360 - 240
acA2040-35gm 0 0 360 - 240
acA2040-55uc 0 - 36 - 24
acA2040-55um 0 0 36 - 24
acA2040-90uc 0 - 23.59350 - 23.59350
acA2040-90um 0 0 23.59350 - 23.59350
acA2040-90umNIR 0 0 23.59350 - 23.59350
acA2040-120uc 0 - 36 - 24
acA2040-120um 0 0 36 - 24
acA2440-20gc 0 - 360 - 240
acA2440-20gm 0 0 360 - 240
acA2440-35uc 0 - 36 - 24
acA2440-35ucMED 0 - 36 - 24
acA2440-35um 0 0 36 - 24
acA2440-35umMED 0 0 36 - 24
acA2440-75uc 0 - 36 - 24
acA2440-75ucMED 0 0 36 - 24
acA2440-75um 0 0 36 - 24
acA2440-75umMED 0 - 36 - 24
acA2500-14gc 0 - 63 - 63
acA2500-14gm 0 0 63 - 63
acA2500-14uc 0 - 23.79814 - 23.79814
acA2500-14um 0 0 23.79814 - 23.79814
acA2500-20gc 136 136 542 542 -
acA2500-20gcMED 136 - 542 542 -
acA2500-20gm 136 136 542 542 -
acA2500-20gmMED 136 136 542 542 -
acA2500-60uc 0 - 12 12 -
acA2500-60um 0 0 12 12 -
acA3088-16gc 0 - 360 - 240
acA3088-16gm 0 0 360 - 240
acA3088-57uc 0 - 36 - 24
acA3088-57ucMED 0 - 36 - 24
acA3088-57um 0 0 36 - 24
acA3088-57umMED 0 0 36 - 24
acA3800-10gc 33 - 255 - 255
acA3800-10gm 33 33 255 - 255
acA3800-14uc 0 - 16.67569 - 16.67569
acA3800-14um 0 0 16.67569 - 16.67569
acA4024-8gc 0 - 1957 - 1957
acA4024-8gm 0 0 1957 - 1957
acA4024-29uc 0 - 27 - 27
acA4024-29um 0 0 27 - 27
acA4096-11gc 0 0 36 - 24
acA4096-11gm 0 0 36 - 24
acA4096-30uc 0 - 36 - 24
acA4096-30ucMED 0 - 36 - 24
acA4096-30um 0 0 36 - 24
acA4096-30umMED 0 0 36 - 24
acA4096-40uc 0 - 36 - 24
acA4096-40ucMED 0 - 36 - 24
acA4096-40um 0 0 36 - 24
acA4096-40umMED 0 0 36 - 24
acA4112-8gc 0 0 36 - 24
acA4112-8gm 0 0 36 - 24
acA4112-20uc 0 - 36 - 24
acA4112-20ucMED 0 - 36 - 24
acA4112-20um 0 0 36 - 24
acA4112-20umMED 0 0 36 - 24
acA4112-30uc 0 - 36 - 24
acA4112-30ucMED 0 - 36 - 24
acA4112-30um 0 0 36 - 24
acA4112-30umMED 0 0 36 - 24
acA5472-5gc 0 - 1957 - 1957
acA5472-5gm 0 0 1957 - 1957
acA5472-17uc 0 - 27.04000 - 27.04000
acA5472-17ucMED 0 - 27.04000 - 27.04000
acA5472-17um 0 0 27.04000 - 27.04000
acA5472-17umMED 0 0 27.04000 - 27.04000
boA1936-400cc 0 - 48 48 48
boA1936-400cm 0 - 48 48 48
boA2448-250cc 0 - 48 48 48
bo2448-250cm 0 - 48 48 48
boA2832-190cc 0 - 48 48 48
bo2832-190cm 0 - 48 48 48
boA4096-93cc 0 - 48 - 48
boA4096-93cm 0 - 48 - 48
boA4096-180cc 0 - 48 48 48
bo4096-180cm 0 - 48 48 48
boA4112-68cc 0 - 48 - 48
boA4112-68cm 0 - 48 - 48
boA4500-45cc 0 - 18.06200 18.062 18.06200
boA4500-45cm 0 - 18.06200 18.062 18.06200
boA4504-100cc 0 - 48 48 48
boA4504-100cm 0 - 48 48 48
boA5120-150cc 0 - 24 24 -
boA5120-150cm 0 - 24 24 -
boA5120-230cc 0 - 24 24 -
boA5120-230cm 0 - 24 24 -
boA5320-150cc 0 - 48 48 48
boA5320-150cm 0 - 48 48 48
boA5328-100cc 0 - 48 48 48
boA5328-100cm 0 - 48 48 48
boA6500-36cc 0 - 18.06200 18.062 18.06200
boA6500-36cm 0 - 18.06200 18.062 18.06200
boA8100-16cc 0 - 18.06200 18.062 18.06200
boA8100-16cm 0 - 18.06200 18.062 18.06200
boA9344-30cc 0 - 24 24 -
boA9344-30cm 0 - 24 24 -
boA9344-70cc 0 - 24 24 -
boA9344-70cm 0 - 24 24 -
boA13440-17cm 0 - 36 36 36b
daA720-520uc 0 - 48 - 48
daA720-520um 0 0 48 - 48
daA1280-54uc 0 0 18 - 18
daA1280-54um 0 0 18 - 18
daA1440-220uc 0 - 48 - 48
daA1440-220um 0 0 48 - 48
daA1600-60uc 0 0 24 - 24
daA1600-60um 0 0 24 - 24
daA1920-15um 0 0 24 - 24
daA1920-30uc 0 0 24 - 24
daA1920-30um 0 0 24 - 24
daA1920-160uc 0 - 48 - 48
daA1920-160um 0 0 48 - 48
daA2448-70uc 0 - 48 - 48
daA2448-70um 0 0 48 - 48
daA2500-14uc 0 0 24 - 24
daA2500-14um 0 0 24 - 24
daA3840-45uc 0 - 48 - 48
daA3840-45um 0 0 48 - 48
dmA720-290gc 0 - 48 48 48
dmA720-290gm 0 0 48 48 48
dmA1440-73gc 0 - 48 48 48
dmA1440-73gm 0 0 48 48 48
dmA1920-51gc 0 - 48 48 48
dmA1920-51gm 0 0 48 48 48
dmA3536-9gc 0 - 48 48 48
dmA3536-9gm 0 0 48 48 48
puA1280-54uc 0 0 18 - 18
puA1280-54um 0 0 18 - 18
puA1600-60uc 0 0 24 - 24
puA1600-60um 0 0 24 - 24
puA1920-30uc 0 0 24 - 24
puA1920-30um 0 0 24 - 24
puA2500-14uc 0 0 24 - 24
puA2500-14um 0 0 24 - 24
r2L2048-29gc 0 - 36 36 36
r2L2048-58gm 0 - 36 36 36
r2L2048-62cc 0 - 36 36 36
r2L2048-62g5c 0 - 36 36 36
r2L2048-172cm 0 - 36 36 36
r2L2048-172g5m 0 - 36 36 36
r2L4096-14gc 0 - 36 36 36
r2L4096-29gm 0 - 36 36 36
r2L4096-42cc 0 - 36 36 36
r2L4096-42g5c 0 - 36 36 36
r2L4096-84cm 0 - 36 36 36
r2L4096-84g5m 0 - 36 36 36
r2L8192-200cm 0 - - - 36
r2L16384-120cm 0 - - 36 -

  1. 模拟增益/数字增益。

  2. Also valid when the pixel format is set to a 14-bit format.

示例代码#

ace Classic/U/L GigE 相机#
// Set the "raw" gain value to 400
// If you want to know the resulting gain in dB, use the formula given in this topic
camera.GainRaw.SetValue(400);
INodeMap& nodemap = camera.GetNodeMap();
// Set the "raw" gain value to 400
// If you want to know the resulting gain in dB, use the formula given in this topic
CIntegerParameter(nodemap, "GainRaw").SetValue(400);
// Set the "raw" gain value to 400
// If you want to know the resulting gain in dB, use the formula given in this topic
camera.Parameters[PLCamera.GainRaw].SetValue(400);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Set the "raw" gain value to 400 */
/* If you want to know the resulting gain in dB, use the formula given in this topic */
errRes = PylonDeviceSetIntegerFeature(hdev, "GainRaw", 400);
CHECK(errRes);
# Set the "raw" gain value to 400
# If you want to know the resulting gain in dB, use the formula given in this topic
camera.GainRaw.Value = 400
其他相机#
// Select the type of gain
camera.GainSelector.SetValue(GainSelector_All);
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.BslConversionGainMode.SetValue(BslConversionGainMode_High);
// Set the gain to 4.2 dB
camera.Gain.SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
camera.BslGainTopLeft.SetValue(1.03);
INodeMap& nodemap = camera.GetNodeMap();
// Select the type of gain
CEnumParameter(nodemap, "GainSelector").SetValue("All");
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
CEnumParameter(nodemap, "BslConversionGainMode").SetValue("High");
// Set the gain to 4.2 dB
CFloatParameter(nodemap, "Gain").SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
CFloatParameter(nodemap, "BslGainTopLeft").SetValue(1.03);
// Select the type of gain
camera.Parameters[PLCamera.GainSelector].SetValue(PLCamera.GainSelector.All);
// Set the conversion gain mode to High
// Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.Parameters[PLCamera.BslConversionGainMode].SetValue(PLCamera.BslConversionGainMode.High);
// Set the gain to 4.2 dB
camera.Parameters[PLCamera.Gain].SetValue(4.2);
// Increase the gain in the top-left quadrant of the image by 3 %
// Note: Available on boA13440-17cm cameras only
camera.Parameters[PLCamera.BslGainTopLeft].SetValue(1.03);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Select the type of gain */
errRes = PylonDeviceFeatureFromString(hdev, "GainSelector", "All");
CHECK(errRes);
/* Set the conversion gain mode to High */
/* Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only */
errRes = PylonDeviceFeatureFromString(hdev, "BslConversionGainMode", "High");
CHECK(errRes);
/* Set the gain to 4.2 dB */
errRes = PylonDeviceSetFloatFeature(hdev, "Gain", 4.2);
CHECK(errRes);
/* Increase the gain in the top-left quadrant of the image by 3 % */
/* Note: Available on boA13440-17cm cameras only */
errRes = PylonDeviceSetFloatFeature(hdev, "BslGainTopLeft", 1.03);
CHECK(errRes);
# Select the type of gain
camera.GainSelector.Value = "All"
# Set the conversion gain mode to High
# Note: Available on a2A2048-35gmSWIR, a2A2048-110umSWIR, a2A2560-20gmSWIR, and a2A2560-70umSWIR cameras only
camera.BslConversionGainMode.Value = "High"
# Set the gain to 4.2 dB
camera.Gain.Value = 4.2
# Increase the gain in the top-left quadrant of the image by 3 %
# Note: Available on boA13440-17cm cameras only
camera.BslGainTopLeft.Value = 1.03

您也可以使用 pylon Viewer 轻松设置参数。