跳转到内容

Line Connection#

The Line Connection camera feature allows you to set or determine the connection signal of the currently selected general purpose I/O line (GPIO line).

Connection signals are used to control certain camera features. For example, the "TWI SDA" and "TWI SCL" signals are used for Two-Wire Interface communication.

该功能的使用#

设置 Line Connection#

设置线路连接:

  1. Set the LineSelector parameter to the desired GPIO line.
  2. 设置 BslLineConnection 参数设置为以下值:
    • ConnectionOff: No connection signal is set for the currently selected line.
    • TwiSda: The TWI SDA signal is set for the currently selected line.
    • TwiScl: The TWI SCL signal is set for the currently selected line.
    • LightControl: The light control signal is set for the currently selected line.
  3. Make sure the LineMode parameter is set to InOut. This allows you to use the GPIO line as an input-output line. If the parameter isn't automatically set to InOut, set it manually.

确定 Line Connection#

确定线路连接:

  1. Set the LineSelector parameter to the desired I/O line.
  2. Get the value of the BslLineConnection parameter to determine the current line connection of the I/O line.

示例代码#

// Select Line 2
camera.LineSelector.SetValue(LineSelector_Line2);
// Set the line connection to TWI SDA
camera.BslLineConnection.SetValue(BslLineConnection_TwiSda);
// Get the current line connection
BslLineConnectionEnums e = camera.BslLineConnection.GetValue();
INodeMap& nodemap = camera.GetNodeMap();
// Select Line 2
CEnumParameter(nodemap, "LineSelector").SetValue("Line2");
// Set the line connection to TWI SDA
CEnumParameter(nodemap, "BslLineConnection").SetValue("TwiSda");
// Get the current line connection
String_t e = CEnumParameter(nodemap, "BslLineConnection").GetValue();
// Select Line 2
camera.Parameters[PLCamera.LineSelector].SetValue(PLCamera.LineSelector.Line2);
// Set the line connection to TWI SDA
camera.Parameters[PLCamera.BslLineConnection].SetValue(PLCamera.BslLineConnection.TwiSda);
// Get the current line connection
string e = camera.Parameters[PLCamera.BslLineConnection].GetValue();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
size_t len = 0;
char e_str[64] = {0};
/* Select Line 2 */
errRes = PylonDeviceFeatureFromString(hdev, "LineSelector", "Line2");
CHECK(errRes);
/* Set the line connection to TWI SDA */
errRes = PylonDeviceFeatureFromString(hdev, "BslLineConnection", "TwiSda");
CHECK(errRes);
/* Get the current line connection */
len = sizeof(e_str);
errRes = PylonDeviceFeatureToString(hdev, "BslLineConnection", e_str, &len);
CHECK(errRes);
# Select Line 2
camera.LineSelector.Value = "Line2"
# Set the line connection to TWI SDA
camera.BslLineConnection.Value = "TwiSda"
# Get the current line connection
e = camera.BslLineConnection.Value

您也可以使用 pylon Viewer 轻松设置参数。