跳转到内容
STAGING SERVER
DEVELOPMENT SERVER

Acquisition Mode#

相机的 Acquisition Mode 功能允许您选择单帧采集或连续图像采集。

信息

  • 无法通过 pylon Viewer 功能树使用此功能。在使用 pylon Viewer 工具栏中的单拍和连拍按钮时,可以自动设定 acquisition mode。
  • pylon C++ API 和 pylon .NET API 提供了配置事件处理程序,用于设置 AcquisitionMode 参数。Basler 建议使用这些事件处理程序。

如需了解详情,请参阅 pylon API 文档中的采集 (C++) 和采集 (.NET) 代码示例。

该功能的使用#

指定 Acquisition Mode#

要指定采集模式,请将 AcquisitionMode 参数设置为以下值:

可用 Acquisition Mode#

单帧 Acquisition Mode#

在单帧采集模式下,相机将仅采集一张图像。

执行采集开始命令后,相机会等待触发信号。触发信号既可以在相机内部生成(自由运行),也可以通过外部施加(触发图像采集)。

信息

要检查相机是否在等待触发信号,请监控相机的 Trigger Wait 信号,或者使用 Acquisition Status 功能(如果可用)。

当收到 Frame Start trigger signal 或 Line Start trigger signal 并且已采集一幅图像后,相机会关闭图像采集。若要采集另一幅图像,必须再次执行 Acquisition Start 命令。

连续 Acquisition Mode#

在连续采集模式下,相机将连续采集并传输图像,直到关闭采集功能为止。

执行采集开始命令后,相机会等待触发信号。触发信号既可以在相机内部生成(自由运行图像采集),也可以通过外部应用(触发图像采集)。相机将持续采集图像,直至执行了采集停止命令。

示例代码#

// Configure single frame acquisition on the camera
camera.AcquisitionMode.SetValue(AcquisitionMode_SingleFrame);
// Switch on image acquisition
camera.AcquisitionStart.Execute();
// The camera waits for a trigger signal.
// When a Frame Start trigger signal has been received,
// the camera executes an Acquisition Stop command internally.
// Configure continuous image acquisition on the camera
camera.AcquisitionMode.SetValue(AcquisitionMode_Continuous);
// Switch on image acquisition
camera.AcquisitionStart.Execute();
// The camera waits for trigger signals.
// (...)
// Switch off image acquisition
camera.AcquisitionStop.Execute();
INodeMap& nodemap = camera.GetNodeMap();
// Configure single frame acquisition on the camera
CEnumParameter(nodemap, "AcquisitionMode").SetValue("SingleFrame");
// Switch on image acquisition
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for a trigger signal.
// When a Frame Start trigger signal has been received,
// the camera executes an Acquisition Stop command internally.
// Configure continuous image acquisition on the camera
CEnumParameter(nodemap, "AcquisitionMode").SetValue("Continuous");
// Switch on image acquisition
CCommandParameter(nodemap, "AcquisitionStart").Execute();
// The camera waits for trigger signals.
// (...)
// Switch off image acquisition
CCommandParameter(nodemap, "AcquisitionStop").Execute();
// Configure single frame acquisition on the camera
camera.Parameters[PLCamera.AcquisitionMode].SetValue(PLCamera.AcquisitionMode.SingleFrame);
// Switch on image acquisition
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for a trigger signal.
// When a Frame Start trigger signal has been received,
// the camera executes an Acquisition Stop command internally.
// Configure continuous image acquisition on the camera
camera.Parameters[PLCamera.AcquisitionMode].SetValue(PLCamera.AcquisitionMode.Continuous);
// Switch on image acquisition
camera.Parameters[PLCamera.AcquisitionStart].Execute();
// The camera waits for trigger signals.
// (...)
// Switch off image acquisition
camera.Parameters[PLCamera.AcquisitionStop].Execute();
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK;  /* Return value of pylon methods */
/* Configure single frame acquisition on the camera */
errRes = PylonDeviceFeatureFromString(hdev, "AcquisitionMode", "SingleFrame");
CHECK(errRes);
/* Switch on image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for a trigger signal. */
/* When a Frame Start trigger signal has been received, */
/* the camera executes an Acquisition Stop command internally. */
/* Configure continuous image acquisition on the camera */
errRes = PylonDeviceFeatureFromString(hdev, "AcquisitionMode", "Continuous");
CHECK(errRes);
/* Switch on image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStart");
CHECK(errRes);
/* The camera waits for trigger signals. */
/* (...) */
/* Switch off image acquisition */
errRes = PylonDeviceExecuteCommandFeature(hdev, "AcquisitionStop");
CHECK(errRes);
# Configure single frame acquisition on the camera
camera.AcquisitionMode.Value = "SingleFrame"
# Switch on image acquisition
camera.AcquisitionStart.Execute()
# The camera waits for a trigger signal.
# When a Frame Start trigger signal has been received,
# the camera executes an Acquisition Stop command internally.
# Configure continuous image acquisition on the camera
camera.AcquisitionMode.Value = "Continuous"
# Switch on image acquisition
camera.AcquisitionStart.Execute()
# The camera waits for trigger signals.
# (...)
# Switch off image acquisition
camera.AcquisitionStop.Execute()

您也可以使用 pylon Viewer 轻松设置参数。