Light Source Preset (dart E)#
根据其特定的色温,用于图像采集的光源会导致图像中的色彩偏移。您可以通过选择相关的光源预设来纠正这些色彩偏移。
该功能的使用#
选择一种 Light Source Preset#
To select a light source preset, set the LightSourcePreset parameter.
Which presets are available depends on the BalanceWhiteAuto parameter setting.
- If the
BalanceWhiteAutoparameter is set toContinuous, theLightSourcePresetparameter is set toAuto, and the light source preset is determined automatically. -
If the
BalanceWhiteAutoparameter is set toOff, the following presets are available:CoolWhiteFluorescent4250K: The camera corrects color shifts caused by fluorescent lighting that has a color temperature of about 4 250 K.Daylight5000K: The camera corrects color shifts caused by daylight lighting that has a color temperature of about 5 000 K.Daylight6500K: The camera corrects color shifts caused by daylight lighting that has a color temperature of about 6 500 K.Daylight7500K: The camera corrects color shifts caused by daylight lighting that has a color temperature of about 7 500 K.Horizon2500K: The camera corrects color shifts caused by horizon lighting that has a color temperature of about 2 500 K.Manual: The color temperature can be set manually.Tungsten2800K: The camera corrects color shifts caused by tungsten lighting that has a color temperature of about 2 500 to 3 000 K.
获取或设置色温#
即: BslLightSourceColorTemperature parameter indicates the color temperature of the currently selected light source preset.
Also, if the light source preset is set to Manual, the parameter allows you to manually set the color temperature.
外部链接#
示例代码#
// Set the light source preset to Daylight5000K
camera.LightSourcePreset.SetValue(LightSourcePreset_Daylight5000K);
// Get the color temperature of the currently selected light source preset
int64_t i = camera.BslLightSourceColorTemperature.GetValue();
// Set the light source preset to Manual
camera.LightSourcePreset.SetValue(LightSourcePreset_Manual);
// Manually set the color temperature
camera.BslLightSourceColorTemperature.SetValue(7334);
INodeMap& nodemap = camera.GetNodeMap();
// Set the light source preset to Daylight5000K
CEnumParameter(nodemap, "LightSourcePreset").SetValue("Daylight5000K");
// Get the color temperature of the currently selected light source preset
int64_t i = CIntegerParameter(nodemap, "BslLightSourceColorTemperature").GetValue();
// Set the light source preset to Manual
CEnumParameter(nodemap, "LightSourcePreset").SetValue("Manual");
// Manually set the color temperature
CIntegerParameter(nodemap, "BslLightSourceColorTemperature").SetValue(7334);
// Set the light source preset to Daylight5000K
camera.Parameters[PLCamera.LightSourcePreset].SetValue(PLCamera.LightSourcePreset.Daylight5000K);
// Get the color temperature of the currently selected light source preset
Int64 i = camera.Parameters[PLCamera.BslLightSourceColorTemperature].GetValue();
// Set the light source preset to Manual
camera.Parameters[PLCamera.LightSourcePreset].SetValue(PLCamera.LightSourcePreset.Manual);
// Manually set the color temperature
camera.Parameters[PLCamera.BslLightSourceColorTemperature].SetValue(7334);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
int64_t i = 0;
/* Set the light source preset to Daylight5000K */
errRes = PylonDeviceFeatureFromString(hdev, "LightSourcePreset", "Daylight5000K");
CHECK(errRes);
/* Get the color temperature of the currently selected light source preset */
errRes = PylonDeviceGetIntegerFeature(hdev, "BslLightSourceColorTemperature", &i);
CHECK(errRes);
/* Set the light source preset to Manual */
errRes = PylonDeviceFeatureFromString(hdev, "LightSourcePreset", "Manual");
CHECK(errRes);
/* Manually set the color temperature */
errRes = PylonDeviceSetIntegerFeature(hdev, "BslLightSourceColorTemperature", 7334);
CHECK(errRes);
# Set the light source preset to Daylight5000K
camera.LightSourcePreset.Value = "Daylight5000K"
# Get the color temperature of the currently selected light source preset
i = camera.BslLightSourceColorTemperature.Value
# Set the light source preset to Manual
camera.LightSourcePreset.Value = "Manual"
# Manually set the color temperature
camera.BslLightSourceColorTemperature.Value = 7334
You can also use the pylon Viewer to easily set the parameters.