Line Selector#
该功能的使用#
选择一条线路#
To select a line, set the LineSelector parameter to the desired I/O line, e.g., Line1 or LinkSignal1.
Depending on the camera model, the total number of I/O lines, the format of the lines (opto-coupled or GPIO), and the pin assignment may vary. For some camera models, you can also configure I/O link signals (i.e., virtual I/O signals). To find out what your camera model offers, check the "General Specifiations" table and "Physical Interface" section in your camera topic. You can find your camera topic in the Area and Line Scan Cameras section.
可能的任务取决于 I/O 线路用作输入还是输出。
选择一条线路后,可以执行以下操作:
| 任务 | 功能 |
|---|---|
| Configuring input filtering for an input line | Input Filter (if available) |
| 为输入线路配置消抖 | Line Debouncer (if available) |
| 选择输出线路的源信号 | Line Source |
| 设置输出线路的最小脉宽 | Line Minimum Output Pulse Width |
| 设置用户可设置输出线路的线路状态 | User Output Value |
| 设置 GPIO 线路的线路模式 | Line Mode |
| 启用反转功能 | Line Inverter |
| 检查单条 I/O 线路的状态 | Line Status |
示例代码#
您也可以使用 pylon Viewer 轻松设置参数。