Classes#
- PylonAviCompressionOptions_t
Wraps the AVI compression options of the Video for Window API. File PylonAviCompressionOptions.h has to be included. - PylonCompressionInfo_t
The struct containing information about a grab buffer/result. - PylonDeviceInfo_t
Device info struct. - PylonEventResult_t
Result data struct for PylonEventGrabberRetrieveEvent(). - PylonGigEActionCommandResult_t
Optional result structure of PylonGigEIssueActionCommand() and PylonGigEIssueScheduledActionCommand(). - PylonGrabResult_t
Result data struct for PylonStreamGrabberRetrieveResult(). This data describes grab results (typically image data) retrieved from the device. Some items are optional (marked as "optional") and are only filled in if they are supported by the device. - PylonImagePersistenceOptions_t
Holds the image persistence options. - PylonInterfaceInfo_t
Interface info struct.