GenICam Base Module Exceptions#
Defines#
Name |
---|
GENERIC_EXCEPTION Fires a generic exception, e.g. throw GENERIC_EXCEPTION("%ld too large", Value);. |
BAD_ALLOC_EXCEPTION Fires a bad alloc exception, e.g. throw BAD_ALLOC_EXCEPTION();. |
INVALID_ARGUMENT_EXCEPTION Fires an invalid argument exception, e.g. throw INVALID_ARGUMENT_EXCEPTION("%ld too large", Value);. |
OUT_OF_RANGE_EXCEPTION Fires an out of range exception, e.g. throw OUT_OF_RANGE_EXCEPTION("%ld too large", Value);. |
PROPERTY_EXCEPTION Fires an property exception, e.g. throw PROPERTY_EXCEPTION("%ld too large", Value);. |
RUNTIME_EXCEPTION Fires a runtime exception, e.g. throw RUNTIME_EXCEPTION("buh!") |
LOGICAL_ERROR_EXCEPTION Fires a logical error exception, e.g. throw LOGICAL_ERROR_EXCEPTION("Should never reach this point") |
ACCESS_EXCEPTION Fires a access exception, e.g. throw ACCESS_EXCEPTION("Not everybody") |
TIMEOUT_EXCEPTION Fires a timeout error exception, e.g. throw TIMEOUT_EXCEPTION("Not everybody") |
DYNAMICCAST_EXCEPTION Fires a dynamic cast exception, e.g. throw DYNAMICCAST_EXCEPTION("Not everybody") |
CHECK_RANGE_I64(_Value, _Min, _Max, _Inc) Range check for int64. |
CHECK_RANGE_FLT(_Value, _Min, _Max) Range check for float. |
CHECK_DYNAMIC_CAST_POINTER(_Pointer) Checks if a dynamic_cast is possible. |
Macros Documentation#
define GENERIC_EXCEPTION#
#define GENERIC_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::GenericException>(__FILE__, __LINE__).Report
Fires a generic exception, e.g. throw GENERIC_EXCEPTION("%ld too large", Value);.
define BAD_ALLOC_EXCEPTION#
#define BAD_ALLOC_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::BadAllocException>(__FILE__, __LINE__, "BadAllocException" ).Report
Fires a bad alloc exception, e.g. throw BAD_ALLOC_EXCEPTION();.
define INVALID_ARGUMENT_EXCEPTION#
#define INVALID_ARGUMENT_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::InvalidArgumentException>(__FILE__, __LINE__, "InvalidArgumentException" ).Report
Fires an invalid argument exception, e.g. throw INVALID_ARGUMENT_EXCEPTION("%ld too large", Value);.
define OUT_OF_RANGE_EXCEPTION#
#define OUT_OF_RANGE_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::OutOfRangeException>(__FILE__, __LINE__, "OutOfRangeException" ).Report
Fires an out of range exception, e.g. throw OUT_OF_RANGE_EXCEPTION("%ld too large", Value);.
define PROPERTY_EXCEPTION#
#define PROPERTY_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::PropertyException>(__FILE__, __LINE__, "PropertyException" ).Report
Fires an property exception, e.g. throw PROPERTY_EXCEPTION("%ld too large", Value);.
define RUNTIME_EXCEPTION#
#define RUNTIME_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::RuntimeException>(__FILE__, __LINE__, "RuntimeException" ).Report
Fires a runtime exception, e.g. throw RUNTIME_EXCEPTION("buh!")
define LOGICAL_ERROR_EXCEPTION#
#define LOGICAL_ERROR_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::LogicalErrorException>(__FILE__, __LINE__, "LogicalErrorException" ).Report
Fires a logical error exception, e.g. throw LOGICAL_ERROR_EXCEPTION("Should never reach this point")
define ACCESS_EXCEPTION#
#define ACCESS_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::AccessException>(__FILE__, __LINE__, "AccessException" ).Report
Fires a access exception, e.g. throw ACCESS_EXCEPTION("Not everybody")
define TIMEOUT_EXCEPTION#
#define TIMEOUT_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::TimeoutException>(__FILE__, __LINE__,"TimeoutException" ).Report
Fires a timeout error exception, e.g. throw TIMEOUT_EXCEPTION("Not everybody")
define DYNAMICCAST_EXCEPTION#
#define DYNAMICCAST_EXCEPTION GENICAM_NAMESPACE::ExceptionReporter<GENICAM_NAMESPACE::DynamicCastException>(__FILE__, __LINE__, "DynamicCastException" ).Report
Fires a dynamic cast exception, e.g. throw DYNAMICCAST_EXCEPTION("Not everybody")
define CHECK_RANGE_I64#
#define CHECK_RANGE_I64(
_Value,
_Min,
_Max,
_Inc
)
if((int64_t)(_Value) < (int64_t)(_Min)) \
throw OUT_OF_RANGE_EXCEPTION("Value = %" FMT_I64 "d must be equal or greater than Min = %" FMT_I64 "d", (int64_t)(_Value), (int64_t)(_Min)); \
else if((int64_t)(_Value) > (int64_t)(_Max)) \
throw OUT_OF_RANGE_EXCEPTION("Value = %" FMT_I64 "d must be equal or smaller than Max = %" FMT_I64 "d", (int64_t)(_Value), (int64_t)(_Max)); \
else if ( 0 == _Inc ) \
throw LOGICAL_ERROR_EXCEPTION("Increment must not equal 0!"); \
else if( ((int64_t)(_Value) - (int64_t)(_Min)) % (int64_t)(_Inc) != 0) \
throw OUT_OF_RANGE_EXCEPTION("The difference between Value = %" FMT_I64 "d and Min = %" FMT_I64 "d must be dividable without rest by Inc = %" FMT_I64 "d", (int64_t)(_Value), (int64_t)(_Min), (int64_t)(_Inc));
Range check for int64.
define CHECK_RANGE_FLT#
#define CHECK_RANGE_FLT(
_Value,
_Min,
_Max
)
if ((_Value) < (_Min)) \
throw OUT_OF_RANGE_EXCEPTION( "Value %f must be greater than or equal %f", (_Value), (_Min) ); \
else if ((_Value) > (_Max)) \
throw OUT_OF_RANGE_EXCEPTION( "Value %f must be smaller than or equal %f", (_Value), (_Max) );
Range check for float.
define CHECK_DYNAMIC_CAST_POINTER#
#define CHECK_DYNAMIC_CAST_POINTER(
_Pointer
)
assert( (_Pointer) != NULL ); \
if (NULL == (_Pointer)) throw LOGICAL_ERROR_EXCEPTION( "Unexpected type in dynamic cast" )
Checks if a dynamic_cast is possible.