PLCamera.ChunkLineSelectorEnum Class#
Applies to: Stereo ace
Visibility: Expert
Selecting Parameters: ChunkBslLineRatio, ChunkLineSource, ChunkLineStatus
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ChunkLineSelectorEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.ChunkLineSelectorEnum | Initializes a new instance of the PLCamera.ChunkLineSelectorEnum class |
Properties#
Name | Description | |
---|---|---|
In1 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
In2 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
In3 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
In4 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
Name | The full name of ChunkLineSelector (Overrides ParameterListEnum.Name.) | |
Out1 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
Out2 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
Out3 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace | |
Out4 | Index of the physical line and associated I/O control block to use. Applies to: Stereo ace |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of ChunkLineSelector (Overrides Object.ToString()()()().) |
PLCamera.ChunkLineSelectorEnum.ToString Method#
The full name of ChunkLineSelector
Return Value#
Type: String
Returns the full name of ChunkLineSelector
PLCamera.ChunkLineSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ChunkLineSelectorEnum class
PLCamera.ChunkLineSelectorEnum.In1 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.In2 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.In3 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.In4 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.Name Property#
The full name of ChunkLineSelector
PLCamera.ChunkLineSelectorEnum.Out1 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.Out2 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.Out3 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace
PLCamera.ChunkLineSelectorEnum.Out4 Property#
Index of the physical line and associated I/O control block to use.
Applies to: Stereo ace