PLCamera.EncoderSourceBEnum Class#
Applies to: racer 2 CXP
Visibility: Expert
Selected by: EncoderSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.EncoderSourceBEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.EncoderSourceBEnum | Initializes a new instance of the PLCamera.EncoderSourceBEnum class |
Properties#
Name | Description | |
---|---|---|
Line1 | The source signal for the B input of the encoder control is set to Line 1. Applies to: racer 2 CXP | |
Line2 | The source signal for the B input of the encoder control is set to Line 2. Applies to: racer 2 CXP | |
Line3 | The source signal for the B input of the encoder control is set to Line 3. Applies to: racer 2 CXP | |
Name | The full name of EncoderSourceB (Overrides ParameterListEnum.Name.) | |
Off | No source signal is set for the B input of the encoder control. Applies to: racer 2 CXP |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of EncoderSourceB (Overrides Object.ToString()()()().) |
PLCamera.EncoderSourceBEnum.ToString Method#
The full name of EncoderSourceB
Return Value#
Type: String
Returns the full name of EncoderSourceB
PLCamera.EncoderSourceBEnum Constructor#
Initializes a new instance of the PLCamera.EncoderSourceBEnum class
PLCamera.EncoderSourceBEnum.Line1 Property#
The source signal for the B input of the encoder control is set to Line 1.
Applies to: racer 2 CXP
PLCamera.EncoderSourceBEnum.Line2 Property#
The source signal for the B input of the encoder control is set to Line 2.
Applies to: racer 2 CXP
PLCamera.EncoderSourceBEnum.Line3 Property#
The source signal for the B input of the encoder control is set to Line 3.
Applies to: racer 2 CXP
PLCamera.EncoderSourceBEnum.Name Property#
The full name of EncoderSourceB
PLCamera.EncoderSourceBEnum.Off Property#
No source signal is set for the B input of the encoder control.
Applies to: racer 2 CXP