Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLTransportLayer.AreaTriggerModeEnum Class#

Sets the trigger mode of the area trigger signal.

Applies to: CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLTransportLayer.AreaTriggerModeEnum

Constructors#

 NameDescription
Public methodPLTransportLayer.AreaTriggerModeEnum Initializes a new instance of the PLTransportLayer.AreaTriggerModeEnum class
 

Properties#

 NameDescription
Public propertyExternal

The trigger mode is set to External.

Applies to: CoaXPress

Public propertyGenerator

The trigger mode is set to Generator.

Applies to: CoaXPress

Public propertyName The full name of AreaTriggerMode (Overrides ParameterListEnum.Name.)
Public propertySoftware

The trigger mode is set to Software.

Applies to: CoaXPress

Public propertySynchronized

The trigger mode is set to Synchronized.

Applies to: CoaXPress

 

Methods#

 NameDescription
Public methodToString The full name of AreaTriggerMode (Overrides Object.ToString()()()().)
 

PLTransportLayer.AreaTriggerModeEnum.ToString Method#

The full name of AreaTriggerMode

Return Value#

Type: String
Returns the full name of AreaTriggerMode

PLTransportLayer.AreaTriggerModeEnum Constructor#

Initializes a new instance of the PLTransportLayer.AreaTriggerModeEnum class

PLTransportLayer.AreaTriggerModeEnum.External Property#

The trigger mode is set to External.

Applies to: CoaXPress

PLTransportLayer.AreaTriggerModeEnum.Generator Property#

The trigger mode is set to Generator.

Applies to: CoaXPress

PLTransportLayer.AreaTriggerModeEnum.Name Property#

The full name of AreaTriggerMode

PLTransportLayer.AreaTriggerModeEnum.Software Property#

The trigger mode is set to Software.

Applies to: CoaXPress

PLTransportLayer.AreaTriggerModeEnum.Synchronized Property#

The trigger mode is set to Synchronized.

Applies to: CoaXPress