Skip to content
STAGING SERVER

PLCamera.BslUSBSpeedModeEnum Class#

Indicates the speed mode of the USB port.

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

Visibility: Beginner

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslUSBSpeedModeEnum

Constructors#

 NameDescription
Public methodPLCamera.BslUSBSpeedModeEnum Initializes a new instance of the PLCamera.BslUSBSpeedModeEnum class
 

Properties#

 NameDescription
Public propertyFullSpeed

The USB port is operating at Full Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

Public propertyHighSpeed

The USB port is operating at High Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

Public propertyLowSpeed

The USB port is operating at Low Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

Public propertyName The full name of BslUSBSpeedMode (Overrides ParameterListEnum.Name.)
Public propertySuperSpeed

The USB port is operating at SuperSpeed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

 

Methods#

 NameDescription
Public methodToString The full name of BslUSBSpeedMode (Overrides Object.ToString()()()().)
 

PLCamera.BslUSBSpeedModeEnum.ToString Method#

The full name of BslUSBSpeedMode

Return Value#

Type: String
Returns the full name of BslUSBSpeedMode

PLCamera.BslUSBSpeedModeEnum Constructor#

Initializes a new instance of the PLCamera.BslUSBSpeedModeEnum class

PLCamera.BslUSBSpeedModeEnum.FullSpeed Property#

The USB port is operating at Full Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

PLCamera.BslUSBSpeedModeEnum.HighSpeed Property#

The USB port is operating at High Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

PLCamera.BslUSBSpeedModeEnum.LowSpeed Property#

The USB port is operating at Low Speed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB

PLCamera.BslUSBSpeedModeEnum.Name Property#

The full name of BslUSBSpeedMode

PLCamera.BslUSBSpeedModeEnum.SuperSpeed Property#

The USB port is operating at SuperSpeed (as specified in the USB standard).

Applies to: ace 2 USB, ace USB, dart USB and pulse USB