PLCamera.LineLogicEnum Class#
Applies to: CameraLink, ace GigE and ace USB
Visibility: Beginner
Selected by: LineSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.LineLogicEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.LineLogicEnum | Initializes a new instance of the PLCamera.LineLogicEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of LineLogic (Overrides ParameterListEnum.Name.) |
![]() | Negative | The line logic of the currently selected line is negative. Applies to: CameraLink, ace GigE and ace USB |
![]() | Positive | The line logic of the currently selected line is positive. Applies to: CameraLink, ace GigE and ace USB |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of LineLogic (Overrides Object.ToString()()()().) |
PLCamera.LineLogicEnum.ToString Method#
The full name of LineLogic
Return Value#
Type: String
Returns the full name of LineLogic
PLCamera.LineLogicEnum Constructor#
Initializes a new instance of the PLCamera.LineLogicEnum class
PLCamera.LineLogicEnum.Name Property#
The full name of LineLogic
PLCamera.LineLogicEnum.Negative Property#
The line logic of the currently selected line is negative.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.LineLogicEnum.Positive Property#
The line logic of the currently selected line is positive.
Applies to: CameraLink, ace GigE and ace USB