Skip to content
STAGING SERVER
DEVELOPMENT SERVER

CommandName Structure#

Defines a command parameter name by combining the parameter name string and the parameter type information.

Syntax#

C#

public struct CommandName

VB

Public Structure CommandName

The CommandName type exposes the following members.

Constructors#

NameDescription
Public methodCommandName Create a command parameter name.
 

Properties#

NameDescription
Public propertyName Returns the command parameter name as string.
 

Methods#

NameDescription
Public methodToString Returns the command parameter name as string. (Overrides ValueType.ToString().)
 

Operators#

NameDescription
Public operatorStatic memberExplicit(String to CommandName) A cast can be used to create a command parameter name from a string.
 

CommandName Explicit Conversion (String to CommandName)#

A cast can be used to create a command parameter name from a string.

Syntax#

C#

public static explicit operator CommandName (
    string name
)

VB

Public Shared Narrowing Operator CType ( 
    name As String
) As CommandName

Parameters#

 

name
Type: System.String
The name of the parameter as string. The name can include path information.

Return Value#

Type: CommandName
Returns the command parameter name.

CommandName.ToString Method#

Returns the command parameter name as string.

Syntax#

C#

public override sealed string ToString()

VB

Public Overrides NotOverridable Function ToString As String

Return Value#

Type: String
Returns the command parameter name as string. The name can include path information.

CommandName Constructor#

Create a command parameter name.

Syntax#

C#

public CommandName(
    string name
)

VB

Public Sub New ( 
    name As String
)

Parameters#

 

name
Type: System.String
The name of the parameter as string. The name can include path information.

CommandName.Name Property#

Returns the command parameter name as string.

Syntax#

C#

public string Name { get; }

VB

Public ReadOnly Property Name As String
    Get

Property Value#

Type: String

CommandName Type Conversions#

The CommandName type exposes the following members.

Operators#

NameDescription
Public operatorStatic memberExplicit(String to CommandName) A cast can be used to create a command parameter name from a string.