Skip to content
STAGING SERVER

PLCamera.BLCSerialPortBaudRateEnum Class#

Reports the baud rate of the serial communication module.

Applies to: ace GigE and ace USB

Visibility: Guru

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BLCSerialPortBaudRateEnum

Constructors#

 NameDescription
Public methodPLCamera.BLCSerialPortBaudRateEnum Initializes a new instance of the PLCamera.BLCSerialPortBaudRateEnum class
 

Properties#

 NameDescription
Public propertyBaud115200

The baud rate is 115200 Bd.

Applies to: ace GigE and ace USB

Public propertyName The full name of BLCSerialPortBaudRate (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of BLCSerialPortBaudRate (Overrides Object.ToString()()()().)
 

PLCamera.BLCSerialPortBaudRateEnum.ToString Method#

The full name of BLCSerialPortBaudRate

Return Value#

Type: String
Returns the full name of BLCSerialPortBaudRate

PLCamera.BLCSerialPortBaudRateEnum Constructor#

Initializes a new instance of the PLCamera.BLCSerialPortBaudRateEnum class

PLCamera.BLCSerialPortBaudRateEnum.Baud115200 Property#

The baud rate is 115200 Bd.

Applies to: ace GigE and ace USB

PLCamera.BLCSerialPortBaudRateEnum.Name Property#

The full name of BLCSerialPortBaudRate