Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.ColorOverexposureCompensationAOISelectorEnum Class#

Selcts the area of interest where color overexposure compensation will be performed.

Applies to: CameraLink and ace GigE

Visibility: Guru

Selecting Parameters: ColorOverexposureCompensationAOIEnable, ColorOverexposureCompensationAOIFactor, ColorOverexposureCompensationAOIFactorRaw, ColorOverexposureCompensationAOIHeight, ColorOverexposureCompensationAOIOffsetX, ColorOverexposureCompensationAOIOffsetY, ColorOverexposureCompensationAOIWidth

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.ColorOverexposureCompensationAOISelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.ColorOverexposureCompensationAOISelectorEnum Initializes a new instance of the PLCamera.ColorOverexposureCompensationAOISelectorEnum class
 

Properties#

 NameDescription
Public propertyAOI1

Selects Color Overexposure Compensation AOI 1.

Applies to: CameraLink and ace GigE

Public propertyName The full name of ColorOverexposureCompensationAOISelector (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of ColorOverexposureCompensationAOISelector (Overrides Object.ToString()()()().)
 

PLCamera.ColorOverexposureCompensationAOISelectorEnum.ToString Method#

The full name of ColorOverexposureCompensationAOISelector

Return Value#

Type: String
Returns the full name of ColorOverexposureCompensationAOISelector

PLCamera.ColorOverexposureCompensationAOISelectorEnum Constructor#

Initializes a new instance of the PLCamera.ColorOverexposureCompensationAOISelectorEnum class

PLCamera.ColorOverexposureCompensationAOISelectorEnum.AOI1 Property#

Selects Color Overexposure Compensation AOI 1.

Applies to: CameraLink and ace GigE

PLCamera.ColorOverexposureCompensationAOISelectorEnum.Name Property#

The full name of ColorOverexposureCompensationAOISelector