Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLTransportLayer.TriggerQueueModeEnum Class#

Enables/disable the trigger queue mode. The maximum output frequency is specified by the Trigger Output Frequency parameter.

Applies to: CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLTransportLayer.TriggerQueueModeEnum

Constructors#

 NameDescription
Public methodPLTransportLayer.TriggerQueueModeEnum Initializes a new instance of the PLTransportLayer.TriggerQueueModeEnum class
 

Properties#

 NameDescription
Public propertyName The full name of TriggerQueueMode (Overrides ParameterListEnum.Name.)
Public propertyOff

The trigger queue mode is disabled.

Applies to: CoaXPress

Public propertyOn

The trigger queue mode is enabled.

Applies to: CoaXPress

 

Methods#

 NameDescription
Public methodToString The full name of TriggerQueueMode (Overrides Object.ToString()()()().)
 

PLTransportLayer.TriggerQueueModeEnum.ToString Method#

The full name of TriggerQueueMode

Return Value#

Type: String
Returns the full name of TriggerQueueMode

PLTransportLayer.TriggerQueueModeEnum Constructor#

Initializes a new instance of the PLTransportLayer.TriggerQueueModeEnum class

PLTransportLayer.TriggerQueueModeEnum.Name Property#

The full name of TriggerQueueMode

PLTransportLayer.TriggerQueueModeEnum.Off Property#

The trigger queue mode is disabled.

Applies to: CoaXPress

PLTransportLayer.TriggerQueueModeEnum.On Property#

The trigger queue mode is enabled.

Applies to: CoaXPress