PLCamera.BslAcquisitionAlternateFilterEnum Class#
Applies to: Stereo ace
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslAcquisitionAlternateFilterEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.BslAcquisitionAlternateFilterEnum | Initializes a new instance of the PLCamera.BslAcquisitionAlternateFilterEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of BslAcquisitionAlternateFilter (Overrides ParameterListEnum.Name.) |
![]() | Off | The filter is turned off, i.e. all images are sent irrespective of the LineSource of Out1 and Out2. Applies to: Stereo ace |
![]() | OnlyHigh | Only send images if LineSource of Out1 or Out2 is ExposureAlternateActive and output currently high. Applies to: Stereo ace |
![]() | OnlyLow | Only send images if LineSource of Out1 or Out2 is ExposureAlternateActive and output currently low. Applies to: Stereo ace |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of BslAcquisitionAlternateFilter (Overrides Object.ToString()()()().) |
PLCamera.BslAcquisitionAlternateFilterEnum.ToString Method#
The full name of BslAcquisitionAlternateFilter
Return Value#
Type: String
Returns the full name of BslAcquisitionAlternateFilter
PLCamera.BslAcquisitionAlternateFilterEnum Constructor#
Initializes a new instance of the PLCamera.BslAcquisitionAlternateFilterEnum class
PLCamera.BslAcquisitionAlternateFilterEnum.Name Property#
The full name of BslAcquisitionAlternateFilter
PLCamera.BslAcquisitionAlternateFilterEnum.Off Property#
The filter is turned off, i.e. all images are sent irrespective of the LineSource of Out1 and Out2.
Applies to: Stereo ace
PLCamera.BslAcquisitionAlternateFilterEnum.OnlyHigh Property#
Only send images if LineSource of Out1 or Out2 is ExposureAlternateActive and output currently high.
Applies to: Stereo ace
PLCamera.BslAcquisitionAlternateFilterEnum.OnlyLow Property#
Only send images if LineSource of Out1 or Out2 is ExposureAlternateActive and output currently low.
Applies to: Stereo ace