PLCamera.TimerSequenceTimerSelectorEnum Class#
Visibility: Guru
Selected by: TimerSequenceEntrySelector
Selecting Parameters: TimerSequenceTimerDelayRaw, TimerSequenceTimerDurationRaw, TimerSequenceTimerEnable, TimerSequenceTimerInverter
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.TimerSequenceTimerSelectorEnum
Constructors#
| Name | Description | |
|---|---|---|
|  | PLCamera.TimerSequenceTimerSelectorEnum | Initializes a new instance of the PLCamera.TimerSequenceTimerSelectorEnum class | 
Properties#
| Name | Description | |
|---|---|---|
|  | Name | The full name of TimerSequenceTimerSelector (Overrides ParameterListEnum.Name.) | 
|  | Timer1 | |
|  | Timer2 | |
|  | Timer3 | |
|  | Timer4 | 
Methods#
| Name | Description | |
|---|---|---|
|  | ToString | The full name of TimerSequenceTimerSelector (Overrides Object.ToString()()()().) | 
PLCamera.TimerSequenceTimerSelectorEnum.ToString Method#
The full name of TimerSequenceTimerSelector
Return Value#
Type: String
Returns the full name of TimerSequenceTimerSelector
PLCamera.TimerSequenceTimerSelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSequenceTimerSelectorEnum class
PLCamera.TimerSequenceTimerSelectorEnum.Name Property#
The full name of TimerSequenceTimerSelector