PLTransportLayer.ShaftEncoderCompensationEnableEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.ShaftEncoderCompensationEnableEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLTransportLayer.ShaftEncoderCompensationEnableEnum | Initializes a new instance of the PLTransportLayer.ShaftEncoderCompensationEnableEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of ShaftEncoderCompensationEnable (Overrides ParameterListEnum.Name.) |
![]() | Off | The trigger queue mode is disabled. Applies to: CoaXPress |
![]() | On | The trigger queue mode is enabled. Applies to: CoaXPress |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of ShaftEncoderCompensationEnable (Overrides Object.ToString()()()().) |
PLTransportLayer.ShaftEncoderCompensationEnableEnum.ToString Method#
The full name of ShaftEncoderCompensationEnable
Return Value#
Type: String
Returns the full name of ShaftEncoderCompensationEnable
PLTransportLayer.ShaftEncoderCompensationEnableEnum Constructor#
Initializes a new instance of the PLTransportLayer.ShaftEncoderCompensationEnableEnum class
PLTransportLayer.ShaftEncoderCompensationEnableEnum.Name Property#
The full name of ShaftEncoderCompensationEnable
PLTransportLayer.ShaftEncoderCompensationEnableEnum.Off Property#
The trigger queue mode is disabled.
Applies to: CoaXPress
PLTransportLayer.ShaftEncoderCompensationEnableEnum.On Property#
The trigger queue mode is enabled.
Applies to: CoaXPress