Skip to content
STAGING SERVER

PLCamera.BslChunkAutoBrightnessStatusEnum Class#

Indicates the status of the target brightness adjustments performed by the Exposure Auto and Gain Auto auto functions.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslChunkAutoBrightnessStatusEnum

Constructors#

 NameDescription
Public methodPLCamera.BslChunkAutoBrightnessStatusEnum Initializes a new instance of the PLCamera.BslChunkAutoBrightnessStatusEnum class
 

Properties#

 NameDescription
Public propertyDisabled

Target brightness adjustments are disabled, i.e., Gain Auto and Exposure Auto are set to Off.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

Public propertyName The full name of BslChunkAutoBrightnessStatus (Overrides ParameterListEnum.Name.)
Public propertyTargetNotReached

Target brightness adjustments are enabled, but the target brightness value has not been reached.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

Public propertyTargetReached

Target brightness adjustments are enabled, and the target brightness value has been reached.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

 

Methods#

 NameDescription
Public methodToString The full name of BslChunkAutoBrightnessStatus (Overrides Object.ToString()()()().)
 

PLCamera.BslChunkAutoBrightnessStatusEnum.ToString Method#

The full name of BslChunkAutoBrightnessStatus

Return Value#

Type: String
Returns the full name of BslChunkAutoBrightnessStatus

PLCamera.BslChunkAutoBrightnessStatusEnum Constructor#

Initializes a new instance of the PLCamera.BslChunkAutoBrightnessStatusEnum class

PLCamera.BslChunkAutoBrightnessStatusEnum.Disabled Property#

Target brightness adjustments are disabled, i.e., Gain Auto and Exposure Auto are set to Off.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

PLCamera.BslChunkAutoBrightnessStatusEnum.Name Property#

The full name of BslChunkAutoBrightnessStatus

PLCamera.BslChunkAutoBrightnessStatusEnum.TargetNotReached Property#

Target brightness adjustments are enabled, but the target brightness value has not been reached.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB

PLCamera.BslChunkAutoBrightnessStatusEnum.TargetReached Property#

Target brightness adjustments are enabled, and the target brightness value has been reached.

Applies to: ace 2 GigE, ace 2 USB, dart GigE and dart USB