PLCamera.OperatingModeEnum Class#
Applies to: blaze
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.OperatingModeEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.OperatingModeEnum | Initializes a new instance of the PLCamera.OperatingModeEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | LongRange | The operating mode is set to Long Range. The Minimum Working Range and Maximum Working Range parameters change accordingly and camera settings are optimized for capturing images at long distances. Applies to: blaze |
![]() | Name | The full name of OperatingMode (Overrides ParameterListEnum.Name.) |
![]() | ShortRange | The operating mode is set to Short Range. The Minimum Working Range and Maximum Working Range parameters change accordingly and camera settings are optimized for capturing images at short distances. Applies to: blaze |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of OperatingMode (Overrides Object.ToString()()()().) |
PLCamera.OperatingModeEnum.ToString Method#
The full name of OperatingMode
Return Value#
Type: String
Returns the full name of OperatingMode
PLCamera.OperatingModeEnum Constructor#
Initializes a new instance of the PLCamera.OperatingModeEnum class
PLCamera.OperatingModeEnum.LongRange Property#
The operating mode is set to Long Range. The Minimum Working Range and Maximum Working Range parameters change accordingly and camera settings are optimized for capturing images at long distances.
Applies to: blaze
PLCamera.OperatingModeEnum.Name Property#
The full name of OperatingMode
PLCamera.OperatingModeEnum.ShortRange Property#
The operating mode is set to Short Range. The Minimum Working Range and Maximum Working Range parameters change accordingly and camera settings are optimized for capturing images at short distances.
Applies to: blaze