Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Basler_UniversalStreamParams#

Classes#

Name
class Basler_UniversalStreamParams::CUniversalStreamParams_Params
A parameter class containing all parameters as members that are available for pylon stream grabbers.
class Basler_UniversalStreamParams::CUniversalStreamParams_Params_v12_0_0
A parameter class containing all parameters as members that are available for pylon stream grabbers.

Types#

Name
enum AccessModeEnums { AccessMode_Control, AccessMode_Exclusive, AccessMode_Monitor, AccessMode_NotInitialized}
Valid values for AccessMode.
enum StatusEnums { Status_Closed, Status_Locked, Status_NotInitialized, Status_Open}
Valid values for Status.
enum StreamBufferHandlingModeEnums { StreamBufferHandlingMode_NewestOnly, StreamBufferHandlingMode_OldestFirst, StreamBufferHandlingMode_OldestFirstOverwrite}
Valid values for StreamBufferHandlingMode.
enum StreamTypeEnums { StreamType_CL, StreamType_CLHS, StreamType_CXP, StreamType_CameraLink, StreamType_CameraLinkHS, StreamType_CoaXPress, StreamType_Custom, StreamType_GEV, StreamType_GigEVision, StreamType_Mixed, StreamType_U3V, StreamType_USB3Vision}
Valid values for StreamType.
enum TransmissionTypeEnums { TransmissionType_LimitedBroadcast, TransmissionType_Multicast, TransmissionType_SubnetDirectedBroadcast, TransmissionType_Unicast, TransmissionType_UseCameraConfig}
Valid values for TransmissionType.
enum TypeEnums { Type_GigEAccelerator, Type_NoDriverAvailable, Type_SocketDriver, Type_WindowsFilterDriver, Type_WindowsIntelPerformanceDriver}
Valid values for Type.

Types Documentation#

enum AccessModeEnums#

Enumerator Value Description
AccessMode_Control The application has control access to the device - Applies to: GigE and blaze.
AccessMode_Exclusive The application has exclusive access to the device - Applies to: GigE and blaze.
AccessMode_Monitor The application has monitoring, i e , read-only, access to the device - Applies to: GigE and blaze.
AccessMode_NotInitialized Access to the device has not been initialized - Applies to: GigE and blaze.

Valid values for AccessMode.

enum StatusEnums#

Enumerator Value Description
Status_Closed The stream grabber is closed - Applies to: GigE.
Status_Locked The stream grabber is locked - Applies to: GigE.
Status_NotInitialized The stream grabber is not initialized - Applies to: GigE.
Status_Open The stream grabber is open - Applies to: GigE.

Valid values for Status.

enum StreamBufferHandlingModeEnums#

Enumerator Value Description
StreamBufferHandlingMode_NewestOnly The application always gets the latest completed buffer (i e , the newest) - Applies to: CoaXPress and blaze.
StreamBufferHandlingMode_OldestFirst The application always gets the buffer from the head of the output buffer queue (i e , the oldest available) - Applies to: CoaXPress and blaze.
StreamBufferHandlingMode_OldestFirstOverwrite The application always gets the buffer from the head of the output buffer queue (i e , the oldest available) - Applies to: CoaXPress and blaze.

Valid values for StreamBufferHandlingMode.

enum StreamTypeEnums#

Enumerator Value Description
StreamType_CL The data stream uses the Camera Link transport layer - Applies to: CoaXPress.
StreamType_CLHS The data stream uses the Camera Link HS transport layer - Applies to: CoaXPress.
StreamType_CXP The data stream uses the CoaXPress transport layer - Applies to: CoaXPress.
StreamType_CameraLink Camera Link - Applies to: CoaXPress.
StreamType_CameraLinkHS Camera Link High Speed - Applies to: CoaXPress.
StreamType_CoaXPress CoaXPress - Applies to: CoaXPress.
StreamType_Custom The data stream uses a custom transport layer - Applies to: CoaXPress.
StreamType_GEV The data stream uses the GigE Vision transport layer - Applies to: CoaXPress.
StreamType_GigEVision GigE Vision - Applies to: CoaXPress.
StreamType_Mixed Different interface modules of the GenTL Producer are of different types - Applies to: CoaXPress.
StreamType_U3V The data stream uses the USB3 Vision transport layer - Applies to: CoaXPress.
StreamType_USB3Vision USB3 Vision - Applies to: CoaXPress.

Valid values for StreamType.

enum TransmissionTypeEnums#

Enumerator Value Description
TransmissionType_LimitedBroadcast The stream data is sent to all devices in the local area network (255 255 255 255) - Applies to: GigE.
TransmissionType_Multicast The stream data is sent to selected devices in the local network - Applies to: GigE.
TransmissionType_SubnetDirectedBroadcast The stream data is sent to all devices in the same subnet as the camera - Applies to: GigE.
TransmissionType_Unicast The stream data is sent to a single device in the local network - Applies to: GigE and blaze.
TransmissionType_UseCameraConfig The stream transmission configuration is read from the camera - Applies to: GigE and blaze.

Valid values for TransmissionType.

enum TypeEnums#

Enumerator Value Description
Type_GigEAccelerator The GigE Accelerator - Applies to: GigE.
Type_NoDriverAvailable No suitable driver is installed - Applies to: GigE and blaze.
Type_SocketDriver The socket driver is used - Applies to: GigE and blaze.
Type_WindowsFilterDriver The pylon GigE Vision Filter Driver is used - Applies to: GigE and blaze.
Type_WindowsIntelPerformanceDriver The pylon GigE Vision Performance Driver is used - Applies to: GigE and blaze.

Valid values for Type.