Low Level API#
Classes#
| Name | |
|---|---|
| class | Pylon::CChunkParser Low Level API: Base class for chunk parsers returned by camera objects. | 
| class | Pylon::GrabResult Low Level API: A grab result that combines the used image buffer and status information. | 
| class | Pylon::EventResult Low Level API: An event result. | 
| class | Pylon::CGrabResultImageT Low Level API: Adapts grab result to Pylon::IImage. | 
| class | Pylon::CSharedByteBuffer Byte buffer with smart pointer semantics. Not thread safe. | 
| class | Pylon::CStreamGrabberProxyT Low Level API: The stream grabber class with parameter access methods. | 
| interface | Pylon::IChunkParser Low Level API: The interface for chunk parsers analyzing a data stream consisting of chunks. | 
| interface | Pylon::ISelfReliantChunkParser Low Level API: Interface for chunk parsers with an own chunk data node map attached. | 
| interface | Pylon::IDevice Low Level API: The interface implemented by all device objects. | 
| interface | Pylon::IPylonDevice Low Level API: Interface for camera objects. | 
| interface | Pylon::IEventAdapter Low Level API: IEventAdapter delivers event messages to ports. | 
| interface | Pylon::IEventGrabber Low Level API: Interface of an object receiving asynchronous events. | 
| interface | Pylon::IStreamGrabber Low Level API: Interface to an (input) data stream. | 
| interface | Pylon::IPylonGigEDevice Low Level API: The interface for Basler GigE camera devices. | 
Types#
| Name | |
|---|---|
| enum | EGrabStatus { GrabStatus_Undefined = -1, _UndefinedGrabStatus = GrabStatus_Undefined, GrabStatus_Idle, Idle = GrabStatus_Idle, GrabStatus_Queued, Queued = GrabStatus_Queued, GrabStatus_Grabbed, Grabbed = GrabStatus_Grabbed, GrabStatus_Canceled, Canceled = GrabStatus_Canceled, GrabStatus_Failed, Failed = GrabStatus_Failed} Low Level API: Possible grab status values. | 
| typedef CGrabResultImageT< GrabResult > | CGrabResultImage Low Level API: Adapts a copy of a grab result to pylon image. | 
Functions#
| Name | |
|---|---|
| template <class Function > DeviceCallbackHandle | RegisterRemovalCallback(IPylonDevice * pDevice, Function f) Low Level API: Register a C-function as a removal callback. | 
| template <class Client ,class Member > DeviceCallbackHandle | RegisterRemovalCallback(IPylonDevice * pDevice, Client & c, Member m) Low Level API: Register a C++-member function as removal callback. | 
| CSharedByteBuffer() default constructer for shared buffer | |
| CSharedByteBuffer(size_t nBytes) constructer for shared buffer form buffer size | |
| CSharedByteBuffer(const CSharedByteBuffer & other) copy constructor | |
| ~CSharedByteBuffer() destructor | |
| CSharedByteBuffer & | operator=(const CSharedByteBuffer & rhs) copy assignment operator | 
| operator bool() const pointer like test if nullptr | |
| void | Release() release the referenz on buffer and memory if last referenzing object. | 
| size_t | GetSize() const return size of buffer in bytes | 
| uint8_t * | GetBuffer() get pointer to buffer memory | 
| const uint8_t * | GetBuffer() const get pointer to buffer memory | 
| bool | IsNull() const test if buffer references memory | 
Types Documentation#
enum EGrabStatus#
| Enumerator | Value | Description | 
|---|---|---|
| GrabStatus_Undefined | -1 | |
| _UndefinedGrabStatus | GrabStatus_Undefined | |
| GrabStatus_Idle | Currently not used. | |
| Idle | GrabStatus_Idle | Currently not used. For backward compatibility only. | 
| GrabStatus_Queued | Grab request is in the input queue. | |
| Queued | GrabStatus_Queued | Grab request is in the input queue. For backward compatibility only. Consider using GrabStatus_Queued instead. | 
| GrabStatus_Grabbed | Grab request terminated successfully. Buffer is filled with data. | |
| Grabbed | GrabStatus_Grabbed | Grab request terminated successfully. Buffer is filled with data. For backward compatibility only. Consider using GrabStatus_Grabbed instead. | 
| GrabStatus_Canceled | Grab request was canceled. Buffer doesn't contain valid data. | |
| Canceled | GrabStatus_Canceled | Grab request was canceled. Buffer doesn't contain valid data. For backward compatibility only. Consider using GrabStatus_Canceled instead. | 
| GrabStatus_Failed | Grab request failed. Buffer doesn't contain valid data. | |
| Failed | GrabStatus_Failed | Grab request failed. Buffer doesn't contain valid data. For backward compatibility only. Consider using GrabStatus_Queued instead. | 
Low Level API: Possible grab status values.
typedef CGrabResultImage#
Low Level API: Adapts a copy of a grab result to pylon image.
Attention: The referenced grab result must not be destroyed and the result's buffer must not be queued for grabbing again during the lifetime of this object.
Functions Documentation#
function RegisterRemovalCallback#
template <class Function >
DeviceCallbackHandle RegisterRemovalCallback(
    IPylonDevice * pDevice,
    Function f
)
Low Level API: Register a C-function as a removal callback.
Parameters:
- pDevice Pointer to the device that generates callbacks
- f The function to be called
See: Pylon::IPylonDevice::RegisterRemovalCallback()
function RegisterRemovalCallback#
template <class Client ,
class Member >
DeviceCallbackHandle RegisterRemovalCallback(
    IPylonDevice * pDevice,
    Client & c,
    Member m
)
Low Level API: Register a C++-member function as removal callback.
Parameters:
- pDevice Pointer to the device that generates callbacks
- c The client object
- m The member function to be called
See: Pylon::IPylonDevice::RegisterRemovalCallback()
function CSharedByteBuffer#
default constructer for shared buffer
function CSharedByteBuffer#
constructer for shared buffer form buffer size
function CSharedByteBuffer#
copy constructor
function ~CSharedByteBuffer#
destructor
function operator=#
copy assignment operator
function operator bool#
pointer like test if nullptr
function Release#
release the referenz on buffer and memory if last referenzing object.
function GetSize#
return size of buffer in bytes
function GetBuffer#
get pointer to buffer memory
Return: nullptr if buffer references no memory
function GetBuffer#
get pointer to buffer memory
Return: nullptr if buffer references no memory
function IsNull#
test if buffer references memory