PLCamera.TimerSelectorEnum Class#
Applies to: CameraLink, ace 2 CXP, ace 2 GigE, ace 2 USB, ace GigE, ace USB, boost CoaXPress, dart GigE, dart USB, racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE
Visibility: Beginner
Selecting Parameters: TimerDelay, TimerDelayAbs, TimerDelayRaw, TimerDuration, TimerDurationAbs, TimerDurationRaw, TimerReset, TimerStatus, TimerTriggerActivation, TimerTriggerArmDelay, TimerTriggerSource
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TimerSelectorEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.TimerSelectorEnum | Initializes a new instance of the PLCamera.TimerSelectorEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of TimerSelector (Overrides ParameterListEnum.Name.) |
![]() | Timer1 | Timer 1 can be configured. Applies to: CameraLink, ace 2 CXP, ace 2 GigE, ace 2 USB, ace GigE, ace USB, boost CoaXPress, dart GigE, dart USB, racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE |
![]() | Timer2 | Timer 2 can be configured. Applies to: CameraLink, ace 2 CXP, ace 2 GigE, ace 2 USB, ace GigE, boost CoaXPress, dart GigE, dart USB, racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE |
![]() | Timer3 | Timer 3 can be configured. Applies to: CameraLink and ace GigE |
![]() | Timer4 | Timer 4 can be configured. Applies to: CameraLink and ace GigE |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of TimerSelector (Overrides Object.ToString()()()().) |
PLCamera.TimerSelectorEnum.ToString Method#
The full name of TimerSelector
Return Value#
Type: String
Returns the full name of TimerSelector
PLCamera.TimerSelectorEnum Constructor#
Initializes a new instance of the PLCamera.TimerSelectorEnum class
PLCamera.TimerSelectorEnum.Name Property#
The full name of TimerSelector
PLCamera.TimerSelectorEnum.Timer1 Property#
Timer 1 can be configured.
Applies to: CameraLink, ace 2 CXP, ace 2 GigE, ace 2 USB, ace GigE, ace USB, boost CoaXPress, dart GigE, dart USB, racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE
PLCamera.TimerSelectorEnum.Timer2 Property#
Timer 2 can be configured.
Applies to: CameraLink, ace 2 CXP, ace 2 GigE, ace 2 USB, ace GigE, boost CoaXPress, dart GigE, dart USB, racer 2 CXP, racer 2S 5GigE, racer 2S CXP and racer 2S GigE
PLCamera.TimerSelectorEnum.Timer3 Property#
Timer 3 can be configured.
Applies to: CameraLink and ace GigE
PLCamera.TimerSelectorEnum.Timer4 Property#
Timer 4 can be configured.
Applies to: CameraLink and ace GigE