Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.EventSelectorEnum Class#

Sets the event notification to be enabled. The notification can be enabled using the Event Notification parameter.

Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Visibility: Beginner

Selecting Parameters: EventNotification

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.EventSelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.EventSelectorEnum Initializes a new instance of the PLCamera.EventSelectorEnum class
 

Properties#

 NameDescription
Public propertyAcquisitionStart

Event notifications for the Acquisition Start event can be enabled. An Acquisition Start event is raised whenever the Acquisition Start trigger is activated. It is not associated with the Acquisition Start command.

Applies to: ace GigE

Public propertyAcquisitionStartOvertrigger

Event notifications for the Acquisition Start Overtrigger event can be enabled.

Applies to: ace GigE

Public propertyAcquisitionStartWait

Event notifications for the Acquisition Start Wait event can be enabled.

Applies to: ace GigE

Public propertyAcquisitionWait

Event notifications for the Acquisition Wait event can be enabled.

Applies to: ace GigE

Public propertyActionLate

Event notifications for the Action Late event can be enabled.

Applies to: ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE

Public propertyCriticalTemperature

Event notifications for the Critical Temperature event can be enabled.

Applies to: ace GigE and ace USB

Public propertyEventOverrun

Event notifications for the Event Overrun event can be enabled.

Applies to: ace GigE

Public propertyExposureEnd

Event notifications for the Exposure End event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE and dart USB

Public propertyFrameBufferOverrun

Event notifications for the Frame Buffer Overrun event can be enabled.

Applies to: ace 2 GigE, ace 2 USB and dart GigE

Public propertyFrameBurstStart

Event notifications for the Frame Burst Start event can be enabled.

Applies to: ace USB

Public propertyFrameBurstStartOvertrigger

Event notifications for the Frame Burst Start Overtrigger event can be enabled.

Applies to: ace USB

Public propertyFrameBurstStartWait

Event notifications for the Frame Burst Start Wait event can be enabled.

Applies to: ace USB

Public propertyFrameStart

Event notifications for the Frame Start event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Public propertyFrameStartOvertrigger

Event notifications for the Frame Start Overtrigger event can be enabled.

Applies to: ace GigE and ace USB

Public propertyFrameStartWait

Event notifications for the Frame Start Wait event can be enabled.

Applies to: ace GigE and ace USB

Public propertyFrameTimeout

Event notifications for the Frame Timeout event can be enabled.

Applies to: ace GigE

Public propertyFrameTriggerMissed

Event notifications for the Frame Trigger Missed event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Public propertyFrameWait

Event notifications for the Frame Wait event can be enabled.

Applies to: ace GigE

Public propertyLine1RisingEdge

The event will be generated when a Rising Edge is detected on the Line 1

Applies to: ace GigE

Public propertyLine2RisingEdge

The event will be generated when a Rising Edge is detected on the Line 2

Applies to: ace GigE

Public propertyLine3RisingEdge

The event will be generated when a Rising Edge is detected on the Line 3

Applies to: ace GigE

Public propertyLine4RisingEdge

The event will be generated when a Rising Edge is detected on the Line 4

Applies to: ace GigE

Public propertyLineStartOvertrigger

Event notifications for the Line Start Overtrigger event can be enabled.

Applies to: ace GigE

Public propertyLineTimeout

Enables event notifications for the Line Timeout event.

Applies to: racer 2S 5GigE and racer 2S GigE

Public propertyLineTriggerMissed

Event notifications for the Line Trigger Missed event can be enabled.

Applies to: racer 2S 5GigE and racer 2S GigE

Public propertyName The full name of EventSelector (Overrides ParameterListEnum.Name.)
Public propertyOverrun

Event notifications for the Overrun event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Public propertyOverTemperature

Event notifications for the Over Temperature event can be enabled.

Applies to: ace GigE and ace USB

Public propertyTemperatureStatusChanged

Event notifications for the Temperature Status Changed event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Public propertyTest

Event notifications for the Test event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

Public propertyVirtualLine1RisingEdge

The event will be generated when a Rising Edge is detected on the Virtual Line 1

Applies to: ace GigE

Public propertyVirtualLine2RisingEdge

The event will be generated when a Rising Edge is detected on the Virtual Line 2

Applies to: ace GigE

Public propertyVirtualLine3RisingEdge

The event will be generated when a Rising Edge is detected on the Virtual Line 3

Applies to: ace GigE

Public propertyVirtualLine4RisingEdge

The event will be generated when a Rising Edge is detected on the Virtual Line 4

Applies to: ace GigE

 

Methods#

 NameDescription
Public methodToString The full name of EventSelector (Overrides Object.ToString()()()().)
 

PLCamera.EventSelectorEnum.ToString Method#

The full name of EventSelector

Return Value#

Type: String
Returns the full name of EventSelector

PLCamera.EventSelectorEnum Constructor#

Initializes a new instance of the PLCamera.EventSelectorEnum class

PLCamera.EventSelectorEnum.AcquisitionStart Property#

Event notifications for the Acquisition Start event can be enabled. An Acquisition Start event is raised whenever the Acquisition Start trigger is activated. It is not associated with the Acquisition Start command.

Applies to: ace GigE

PLCamera.EventSelectorEnum.AcquisitionStartOvertrigger Property#

Event notifications for the Acquisition Start Overtrigger event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.AcquisitionStartWait Property#

Event notifications for the Acquisition Start Wait event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.AcquisitionWait Property#

Event notifications for the Acquisition Wait event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.ActionLate Property#

Event notifications for the Action Late event can be enabled.

Applies to: ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.CriticalTemperature Property#

Event notifications for the Critical Temperature event can be enabled.

Applies to: ace GigE and ace USB

PLCamera.EventSelectorEnum.EventOverrun Property#

Event notifications for the Event Overrun event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.ExposureEnd Property#

Event notifications for the Exposure End event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE and dart USB

PLCamera.EventSelectorEnum.FrameBufferOverrun Property#

Event notifications for the Frame Buffer Overrun event can be enabled.

Applies to: ace 2 GigE, ace 2 USB and dart GigE

PLCamera.EventSelectorEnum.FrameBurstStart Property#

Event notifications for the Frame Burst Start event can be enabled.

Applies to: ace USB

PLCamera.EventSelectorEnum.FrameBurstStartOvertrigger Property#

Event notifications for the Frame Burst Start Overtrigger event can be enabled.

Applies to: ace USB

PLCamera.EventSelectorEnum.FrameBurstStartWait Property#

Event notifications for the Frame Burst Start Wait event can be enabled.

Applies to: ace USB

PLCamera.EventSelectorEnum.FrameStart Property#

Event notifications for the Frame Start event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.FrameStartOvertrigger Property#

Event notifications for the Frame Start Overtrigger event can be enabled.

Applies to: ace GigE and ace USB

PLCamera.EventSelectorEnum.FrameStartWait Property#

Event notifications for the Frame Start Wait event can be enabled.

Applies to: ace GigE and ace USB

PLCamera.EventSelectorEnum.FrameTimeout Property#

Event notifications for the Frame Timeout event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.FrameTriggerMissed Property#

Event notifications for the Frame Trigger Missed event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.FrameWait Property#

Event notifications for the Frame Wait event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.Line1RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Line 1

Applies to: ace GigE

PLCamera.EventSelectorEnum.Line2RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Line 2

Applies to: ace GigE

PLCamera.EventSelectorEnum.Line3RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Line 3

Applies to: ace GigE

PLCamera.EventSelectorEnum.Line4RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Line 4

Applies to: ace GigE

PLCamera.EventSelectorEnum.LineStartOvertrigger Property#

Event notifications for the Line Start Overtrigger event can be enabled.

Applies to: ace GigE

PLCamera.EventSelectorEnum.LineTimeout Property#

Enables event notifications for the Line Timeout event.

Applies to: racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.LineTriggerMissed Property#

Event notifications for the Line Trigger Missed event can be enabled.

Applies to: racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.Name Property#

The full name of EventSelector

PLCamera.EventSelectorEnum.Overrun Property#

Event notifications for the Overrun event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.OverTemperature Property#

Event notifications for the Over Temperature event can be enabled.

Applies to: ace GigE and ace USB

PLCamera.EventSelectorEnum.TemperatureStatusChanged Property#

Event notifications for the Temperature Status Changed event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.Test Property#

Event notifications for the Test event can be enabled.

Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE

PLCamera.EventSelectorEnum.VirtualLine1RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Virtual Line 1

Applies to: ace GigE

PLCamera.EventSelectorEnum.VirtualLine2RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Virtual Line 2

Applies to: ace GigE

PLCamera.EventSelectorEnum.VirtualLine3RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Virtual Line 3

Applies to: ace GigE

PLCamera.EventSelectorEnum.VirtualLine4RisingEdge Property#

The event will be generated when a Rising Edge is detected on the Virtual Line 4

Applies to: ace GigE