Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.BslSpatialCorrectionDirectionReversalEnum Class#

Sets the signal source to be used to trigger a reversal of the defined spatial correction direction. A high signal level triggers a reversal of the direction.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslSpatialCorrectionDirectionReversalEnum

Constructors#

 NameDescription
Public methodPLCamera.BslSpatialCorrectionDirectionReversalEnum Initializes a new instance of the PLCamera.BslSpatialCorrectionDirectionReversalEnum class
 

Properties#

 NameDescription
Public propertyEncoderReverse1

The Encoder Reverse 1 signal level determines the spatial correction direction. If the Encoder Reverse 1 signal is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

Public propertyLine1

The signal level of line 1 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

Public propertyLine2

The signal level of line 2 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

Public propertyLine3

The signal level of line 3 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

Public propertyName The full name of BslSpatialCorrectionDirectionReversal (Overrides ParameterListEnum.Name.)
Public propertyOff

Direction reversal is disabled.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

 

Methods#

 NameDescription
Public methodToString The full name of BslSpatialCorrectionDirectionReversal (Overrides Object.ToString()()()().)
 

PLCamera.BslSpatialCorrectionDirectionReversalEnum.ToString Method#

The full name of BslSpatialCorrectionDirectionReversal

Return Value#

Type: String
Returns the full name of BslSpatialCorrectionDirectionReversal

PLCamera.BslSpatialCorrectionDirectionReversalEnum Constructor#

Initializes a new instance of the PLCamera.BslSpatialCorrectionDirectionReversalEnum class

PLCamera.BslSpatialCorrectionDirectionReversalEnum.EncoderReverse1 Property#

The Encoder Reverse 1 signal level determines the spatial correction direction. If the Encoder Reverse 1 signal is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

PLCamera.BslSpatialCorrectionDirectionReversalEnum.Line1 Property#

The signal level of line 1 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

PLCamera.BslSpatialCorrectionDirectionReversalEnum.Line2 Property#

The signal level of line 2 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

PLCamera.BslSpatialCorrectionDirectionReversalEnum.Line3 Property#

The signal level of line 3 determines the spatial correction direction. If the signal level is high, the spatial correction direction is reversed.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE

PLCamera.BslSpatialCorrectionDirectionReversalEnum.Name Property#

The full name of BslSpatialCorrectionDirectionReversal

PLCamera.BslSpatialCorrectionDirectionReversalEnum.Off Property#

Direction reversal is disabled.

Applies to: racer 2S 5GigE, racer 2S CXP and racer 2S GigE