IFloatParameter Interface#
Syntax#
C#
VB
The IFloatParameter type exposes the following members.
Properties#
Name | Description | |
---|---|---|
Advanced | The advanced parameter settings, if available. (Inherited from IParameter.) | |
FullName | The full name of the parameter including path information. (Inherited from IParameter.) | |
IsEmpty | Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable. (Inherited from IParameter.) | |
IsReadable | Indicates if the parameter is readable. (Inherited from IParameter.) | |
IsWritable | Indicates if the parameter is writable. (Inherited from IParameter.) | |
Name | The name of the parameter without path information. (Inherited from IParameter.) |
Methods#
Name | Description | |
---|---|---|
GetIncrement | Gets the increment value of the current parameter. Returns null if the parameter does not have an increment. | |
GetMaximum | Gets the maximum value of the current parameter. | |
GetMinimum | Gets the minimum value of the current parameter. | |
GetValue | Gets the current parameter value. | |
ParseAndSetValue | Parses the value as string and sets the value. (Inherited from IParameter.) | |
SetValue | Sets the provided value. | |
ToString | The parameter value as a string. (Inherited from IParameter.) |
Events#
Name | Description | |
---|---|---|
ParameterChanged | This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed. (Inherited from IParameter.) | |
ParameterValueChanged | This event fires after the parameter value has changed. (Inherited from IParameter.) |
Extension Methods#
Name | Description | |
---|---|---|
GetValueOrDefault | Gets the parameter value if the parameter is readable. Otherwise, returns the default value. (Defined by IFloatParameterExtensions.) | |
GetValuePercentOfRange | Returns the current value in percent of minimum/maximum range. (Defined by IFloatParameterExtensions.) | |
SetToMaximum | Sets the parameter value to the maximum possible value. (Defined by IFloatParameterExtensions.) | |
SetToMinimum | Sets the parameter value to the minimum possible value. (Defined by IFloatParameterExtensions.) | |
SetValue | Sets the provided value. The value is automatically corrected if needed. (Defined by IFloatParameterExtensions.) | |
SetValuePercentOfRange | Sets the provided value to a value within the range, using this formula (simplified): ((max - min) * (percentOfRange / 100.0)) + min. (Defined by IFloatParameterExtensions.) | |
TrySetToMaximum | Sets the parameter value to the maximum possible value if the parameter is readable and writable. (Defined by IFloatParameterExtensions.) | |
TrySetToMinimum | Sets the parameter value to the minimum possible value if the parameter is readable and writable. (Defined by IFloatParameterExtensions.) | |
TrySetValue(Double) | Overloaded. Sets the value passed if the parameter is writable. The value must be in the valid range and the increment must be correct. (Defined by IFloatParameterExtensions.) | |
TrySetValue(Double, FloatValueCorrection) | Overloaded. Sets the provided value if the parameter is writable and readable. The value is automatically corrected if needed. (Defined by IFloatParameterExtensions.) | |
TrySetValuePercentOfRange | If the parameter is writable and readable, sets the value passed to a value within the range, using this formula (simplified): ((max - min) * (percentOfRange / 100.0)) + min (Defined by IFloatParameterExtensions.) |
IFloatParameter.GetIncrement Method#
Gets the increment value of the current parameter. Returns null if the parameter does not have an increment.
Syntax#
C#
VB
Return Value#
Type: Nullable(Double)
Returns the increment value of the current parameter. Returns null if the parameter does not have an increment.
Remarks#
Preconditions: The parameter must be readable.
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.
IFloatParameter.GetMaximum Method#
Gets the maximum value of the current parameter.
Syntax#
C#
VB
Return Value#
Type: Double
Returns the maximum value of the current parameter.
Remarks#
Preconditions: The parameter must be readable.
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.
IFloatParameter.GetMinimum Method#
Gets the minimum value of the current parameter.
Syntax#
C#
VB
Return Value#
Type: Double
Returns the minimum value of the current parameter.
Remarks#
Preconditions: The parameter must be readable.
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.
IFloatParameter.GetValue Method#
Gets the current parameter value.
Syntax#
C#
VB
Return Value#
Type: Double
Returns the current parameter value.
Remarks#
Preconditions: The parameter must be readable.
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.
IFloatParameter.SetValue Method#
Sets the provided value.
Syntax#
C#
VB
Parameters#
- value
- Type: System.Double
The value to set.
Remarks#
If the float parameter has an increment, the increment is automatically corrected.
Preconditions:
- The parameter must be writable.
- The value passed must be >= GetMinimum().
- The value passed must be <= GetMaximum().
Error Safety: Can throw exceptions if writing the value fails, if the value is out of bounds, if the alignment is not correct, or if the parameter is not writable.