PLCamera.SequencerTriggerSourceEnum Class#
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
Visibility: Expert
Selected by: SequencerPathSelector, SequencerSetSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.SequencerTriggerSourceEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.SequencerTriggerSourceEnum | Initializes a new instance of the PLCamera.SequencerTriggerSourceEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | AcquisitionActive | Acquisition Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Action1 | Action 1 signals can be used to advance to the next sequence set. Applies to: ace 2 GigE |
![]() | Action2 | Action 2 signals can be used to advance to the next sequence set. Applies to: ace 2 GigE |
![]() | Counter1Active | Counter 1 Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Counter1End | Counter 1 End signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Counter1Start | Counter 1 Start signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Counter2Active | Counter 2 Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Counter2End | Counter 2 End signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Counter2Start | Counter 2 Start signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Counter3End | Counter 3 End signals can be used to advance to the next sequence set. Applies to: ace USB |
![]() | CxpTrigger0 | CXP Trigger 0 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP and boost CoaXPress |
![]() | CxpTrigger1 | CXP Trigger 1 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP and boost CoaXPress |
![]() | ExposureActive | Exposure Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | ExposureStart | Exposure Start signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | ExposureTriggerWait | Exposure Trigger Wait signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | FlashWindow | Flash Window signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | FrameBurstActive | Frame Burst Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | FrameBurstTriggerWait | Frame Burst Trigger Wait signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | FrameEnd | Frame End is selected as the trigger source for sequencer set advance. Applies to: ace USB |
![]() | FrameStart | Frame Start signals can be used to advance to the next sequence set. Applies to: ace USB |
![]() | FrameTriggerWait | Frame Trigger Wait signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Line1 | Line 1 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Line2 | Line 2 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Line3 | Line 3 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Line4 | Line 4 signals can be used to advance to the next sequence set. Applies to: ace USB |
![]() | Name | The full name of SequencerTriggerSource (Overrides ParameterListEnum.Name.) |
![]() | Off | The sequencer can't be triggered. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | PeriodicSignal1 | Periodic Signal 1 signals can be used to advance to the next sequence set. Applies to: ace 2 GigE |
![]() | SoftwareSignal1 | Software Signal 1 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | SoftwareSignal2 | Software Signal 2 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | SoftwareSignal3 | Software Signal 3 signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress |
![]() | Timer1Active | Timer 1 Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Timer1End | Timer 1 End signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Timer2Active | Timer 2 Active signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
![]() | Timer2End | Timer 2 End signals can be used to advance to the next sequence set. Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of SequencerTriggerSource (Overrides Object.ToString()()()().) |
PLCamera.SequencerTriggerSourceEnum.ToString Method#
The full name of SequencerTriggerSource
Return Value#
Type: String
Returns the full name of SequencerTriggerSource
PLCamera.SequencerTriggerSourceEnum Constructor#
Initializes a new instance of the PLCamera.SequencerTriggerSourceEnum class
PLCamera.SequencerTriggerSourceEnum.AcquisitionActive Property#
Acquisition Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Action1 Property#
Action 1 signals can be used to advance to the next sequence set.
Applies to: ace 2 GigE
PLCamera.SequencerTriggerSourceEnum.Action2 Property#
Action 2 signals can be used to advance to the next sequence set.
Applies to: ace 2 GigE
PLCamera.SequencerTriggerSourceEnum.Counter1Active Property#
Counter 1 Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter1End Property#
Counter 1 End signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter1Start Property#
Counter 1 Start signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter2Active Property#
Counter 2 Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter2End Property#
Counter 2 End signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter2Start Property#
Counter 2 Start signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Counter3End Property#
Counter 3 End signals can be used to advance to the next sequence set.
Applies to: ace USB
PLCamera.SequencerTriggerSourceEnum.CxpTrigger0 Property#
CXP Trigger 0 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.CxpTrigger1 Property#
CXP Trigger 1 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.ExposureActive Property#
Exposure Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.ExposureStart Property#
Exposure Start signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.ExposureTriggerWait Property#
Exposure Trigger Wait signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.FlashWindow Property#
Flash Window signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.FrameBurstActive Property#
Frame Burst Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.FrameBurstTriggerWait Property#
Frame Burst Trigger Wait signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.FrameEnd Property#
Frame End is selected as the trigger source for sequencer set advance.
Applies to: ace USB
PLCamera.SequencerTriggerSourceEnum.FrameStart Property#
Frame Start signals can be used to advance to the next sequence set.
Applies to: ace USB
PLCamera.SequencerTriggerSourceEnum.FrameTriggerWait Property#
Frame Trigger Wait signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Line1 Property#
Line 1 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Line2 Property#
Line 2 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Line3 Property#
Line 3 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Line4 Property#
Line 4 signals can be used to advance to the next sequence set.
Applies to: ace USB
PLCamera.SequencerTriggerSourceEnum.Name Property#
The full name of SequencerTriggerSource
PLCamera.SequencerTriggerSourceEnum.Off Property#
The sequencer can't be triggered.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.PeriodicSignal1 Property#
Periodic Signal 1 signals can be used to advance to the next sequence set.
Applies to: ace 2 GigE
PLCamera.SequencerTriggerSourceEnum.SoftwareSignal1 Property#
Software Signal 1 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.SoftwareSignal2 Property#
Software Signal 2 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.SoftwareSignal3 Property#
Software Signal 3 signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB, ace USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Timer1Active Property#
Timer 1 Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Timer1End Property#
Timer 1 End signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Timer2Active Property#
Timer 2 Active signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress
PLCamera.SequencerTriggerSourceEnum.Timer2End Property#
Timer 2 End signals can be used to advance to the next sequence set.
Applies to: ace 2 CXP, ace 2 GigE, ace 2 USB and boost CoaXPress