Resulting Acquisition Line Rate#
例如,如果您想知道两次触发之间必须等待多长时间,这将很有用。
The line rate is expressed in hertz (Hz).
该功能的使用#
Why Check the Resulting Acquisition Line Rate#
Optimizing the Line Rate#
When the camera is configured for free run image acquisition and continuous acquisition, knowing the resulting acquisition line rate is useful if you want to optimize the line rate for your imaging application. You can adjust the camera settings limiting the line rate until the resulting acquisition line rate reaches the desired value.
优化触发图像采集#
When the camera is configured for triggered image acquisition, knowing the resulting acquisition line rate is useful if you want to trigger the camera as often as possible without overtriggering. You can calculate how long you must wait after each trigger signal by taking the reciprocal of the resulting acquisition line rate: 1 / Resulting Acquisition Line Rate.
Example: If the resulting acquisition line rate is 100000 Hz, you must wait for a minimum of 1/100000 = 10 µs after each trigger signal.
Checking the Resulting Acquisition Line Rate#
To check the resulting acquisition line rate, i.e., the estimated line rate with the current camera settings, get the value of the BslResultingAquisitionLineRate parameter. The value is expressed in hertz (Hz).
The parameter value takes all factors limiting the line rate into account.
信息
- On some camera models, the
ResultingFramePeriodparameter is also available. It allows you to determine the resulting frame period, which is the reciprocal of the resulting frame rate (1 / frame rate). - Checking the resulting acquisition line rate works when the camera is idle as well as when the camera is acquiring images.
- If you want to check the resulting acquisition line rate of Basler cameras that aren't connected to your computer at the moment, use the online Basler Frame Rate Calculator.
Factors Limiting the Line Rate#
Several factors may limit the line rate on a Basler camera:
- Acquisition Line Rate: If the Acquisition Line Rate feature is enabled, the camera's line rate is limited by the acquisition line rate. For example, if you enable the Acquisition Line Rate feature and set an acquisition line rate of 100000 Hz, the camera's line rate will never be higher than 100000 Hz.
- Bandwidth Assigned: Bandwidth limitations can reduce the line rate, especially when more than one camera is connected to a computer. The extent of the reduction depends on the camera model, the number of cameras connected to the computer, and the computer's hardware.
- Binning: If available, sensor binning can increase the line rate.
- Camera Operation Mode: If the
CameraOperationModeparameter is available and set toLongExposure, the line rate decreases. - Device Link Throughput: If the
DeviceLinkThroughputLimitModeparameter is available and set toOn, it limits the available bandwidth for data transmission to theDeviceLinkThroughputLimitparameter value. This also limits the line rate. - Exposure Time: If you use very long exposure times, you can acquire fewer lines per second.
- Field Output Mode: If available, using the Field 0 Output Mode or Field 1 Output Mode increases the camera's line rate.
- Image ROI: if you use a large image ROI, you can acquire fewer lines per second. On most cameras, decreasing the image ROI height increases the line rate. On some cameras, decreasing the image ROI width also increases the line rate.
- Parameter Limits: On some cameras, you can use the Remove Parameter Limits feature to remove the line rate limitation.
- Sensor Bit Depth: On some cameras, you can decrease the sensor bit depth to increase the line rate.
- Sensor Readout Mode: On some cameras, you can enable a fast sensor readout mode that allows you to increase the line rate. This can, however, have adverse effects on image quality.
- Sensor Shutter Mode: If the Global Reset Release shutter mode is selected, overlapped image acquisition is not possible. This decreases the camera's line rate.
- Stacked Zone Imaging: If available, using the Stacked Zone Imaging feature increases the line rate.
- Transfer Bit Depth: On some cameras, you can decrease the transfer bit depth to increase the line rate.
外部链接#
- Basler Frame Rate Calculator (baslerweb.com)
(Not available for racer 2 XL cameras.)
示例代码#
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
double d = 0;
/* Get the resulting acquisition line rate */
errRes = PylonDeviceGetFloatFeature(hdev, "BslResultingAcquisitionLineRate", &d);
CHECK(errRes);
您也可以使用 pylon Viewer 轻松设置参数。