Skip to content
STAGING SERVER
DEVELOPMENT SERVER

Basler_UniversalEventParams#

Classes#

Name
class Basler_UniversalEventParams::CUniversalEventParams_Params
A parameter class containing all parameters as members that are available for pylon event grabbers.
class Basler_UniversalEventParams::CUniversalEventParams_Params_v11_0_0
A parameter class containing all parameters as members that are available for pylon event grabbers.

Types#

Name
enum StatusEnums { Status_Closed, Status_Open}
Valid values for Status.

Types Documentation#

enum StatusEnums#

Enumerator Value Description
Status_Closed The low level event grabber is closed - Applies to: GigE.
Status_Open The low level event grabber is open - Applies to: GigE.

Valid values for Status.