Skip to content
STAGING SERVER
DEVELOPMENT SERVER

GenApi#

Contains definitions of the types of GenICam GenApi modules. More…

Classes#

Name
class GenApi::CBaseRefT
class GenApi::CBooleanRefT
class GenApi::CCategoryRefT
class GenApi::CCommandRefT
class GenApi::CEnumEntryRefT
class GenApi::CEnumerationTRef
class GenApi::CFloatPtr
SmartPointer for IFloat interface pointer.
class GenApi::CFloatRefT
class GenApi::CGeneric_XMLLoaderParams
Empty base class used by class CNodeMapRef as generic template argument.
class GenApi::CIntegerRefT
class GenApi::CNodeCallback
callback body instance for INode pointers
class GenApi::CNodeMapRef
Smartpointer for NodeMaps with create function.
class GenApi::CNodeMapRefT
Smartpointer template for NodeMaps with create function.
class GenApi::CPointer
Encapsulates a GenApi pointer dealing with the dynamic_cast automatically.
class GenApi::CPortRefT
class GenApi::CRegisterRefT
class GenApi::CSelectorRefT
class GenApi::CStringRefT
class GenApi::CValueRefT
class GenApi::EAccessModeClass
EAccessModeClass holds conversion methods for the access mode enumeration.
class GenApi::ECachingModeClass
ECachingModeClass holds conversion methods for the caching mode enumeration.
class GenApi::EDisplayNotationClass
Holds conversion methods for the notation type of floats.
class GenApi::EEndianessClass
EEndianessClass holds conversion methods for the endianess enumeration.
class GenApi::EGenApiSchemaVersionClass
helper class converting EGenApiSchemaVersion from and to string
class GenApi::EInputDirectionClass
Holds conversion methods for the notation type of floats.
class GenApi::ENameSpaceClass
Holds conversion methods for the namespace enumeration.
class GenApi::ERepresentationClass
ERepresentationClass holds conversion methods for the representation enumeration.
class GenApi::ESignClass
ESignClass holds conversion methods for the sign enumeration.
class GenApi::ESlopeClass
Holds conversion methods for the converter formulas.
class GenApi::EStandardNameSpaceClass
Holds conversion methods for the standard namespace enumeration.
class GenApi::EVisibilityClass
EVisibilityClass holds conversion methods for the visibility enumeration.
class GenApi::EYesNoClass
Holds conversion methods for the standard namespace enumeration.
class GenApi::FileProtocolAdapter
Adapter between the std::iostreambuf and the SFNC Features representing the device filesystem.
class GenApi::Function_NodeCallback
Container for a function pointer.
struct GenApi::IBase
Base interface common to all nodes.
struct GenApi::IBoolean
Interface for Boolean properties.
struct GenApi::ICategory
Gives access to a category node.
struct GenApi::ICommand
class GenApi::IDevFileStreamBase
class GenApi::IDevFileStreamBuf
struct GenApi::IEnumEntry
Interface of single enum value.
struct GenApi::IEnumeration
Interface for enumeration properties.
struct GenApi::IEnumerationT
Interface for enumeration properties.
struct GenApi::IFileProtocolAdapter
Adapter between the std::iostreambuf and the SFNC Features representing the device filesystem.
struct GenApi::IFloat
Interface for float properties.
struct GenApi::IInteger
Interface for integer properties.
struct GenApi::INode
Interface common to all nodes.
struct GenApi::INodeMap
Interface to access the node map.
struct GenApi::IPort
Interface for ports.
struct GenApi::IRegister
Interface for registers.
struct GenApi::ISelector
Interface for groups of features selected by a single one.
struct GenApi::IString
Interface for string properties.
struct GenApi::IValue
Interface for value properties.
class GenApi::Member_NodeCallback
Container for a member function pointer.
class GenApi::node_vector
A vector of INode pointers.
class GenApi::ODevFileStreamBase
class GenApi::ODevFileStreamBuf
class GenApi::value_vector
A vector of IValue pointers.

Types#

Name
enum _ECallbackType { cbPostInsideLock = 1, cbPostOutsideLock = 2}
the type of callback
enum _ESign
enum _EAccessMode
enum _EVisibility
enum _ECachingMode
enum _ERepresentation
enum _EEndianess
enum _ENameSpace
enum _EStandardNameSpace
enum _EYesNo
enum _ESlope
enum _EXMLValidation { xvLoad = 0x00000001L, xvCycles = 0x00000002L, xvSFNC = 0x00000004L, xvDefault = 0x00000000L, xvAll = 0xffffffffL, _UndefinedEXMLValidation = 0x8000000L}
typedef describing the different validity checks which can be performed on an XML file
enum _EDisplayNotation
enum _EInterfaceType
enum _ELinkType { ctParentNodes, ctReadingChildren, ctWritingChildren, ctInvalidatingChildren, ctDependingNodes, ctTerminalNodes, ctValueChangingChildren}
typedef for link type
enum _EIncMode
enum _EInputDirection
enum _EGenApiSchemaVersion { v1_0 = 1, v1_1 = 2, _Undefined = -1}
GenApi schema version.
typedef value_vector FeatureList_t
a list of feature references
typedef CBaseRefT< IBase > CBaseRef
typedef CBooleanRefT< IBoolean > CBooleanRef
typedef CCategoryRefT< ICategory > CCategoryRef
typedef CCommandRefT< ICommand > CCommandRef
typedef CEnumEntryRefT< IEnumEntry > CEnumEntryRef
typedef CFloatRefT< IFloat > CFloatRef
typedef CIntegerRefT< IInteger > CIntegerRef
typedef node_vector NodeList_t
a list of node references
typedef intptr_t CallbackHandleType
the callback handle for nodes
typedef CPortRefT< IPort > CPortRef
typedef CRegisterRefT< IRegister > CRegisterRef
typedef CSelectorRefT< ISelector > CSelectorRef
typedef CStringRefT< IString > CStringRef
typedef CValueRefT< IValue > CValueRef
typedef enum GenApi::_ECallbackType ECallbackType
the type of callback
typedef CPointer< IBase > CBasePtr
SmartPointer for IBase interface pointer.
typedef CPointer< INode > CNodePtr
SmartPointer for INode interface pointer.
typedef CPointer< IValue > CValuePtr
SmartPointer for IValue interface pointer.
typedef CPointer< ICategory > CCategoryPtr
SmartPointer for ICategory interface pointer.
typedef CPointer< IBoolean > CBooleanPtr
SmartPointer for IBoolean interface pointer.
typedef CPointer< IInteger > CIntegerPtr
SmartPointer for IInteger interface pointer.
typedef CPointer< IString > CStringPtr
SmartPointer for IString interface pointer.
typedef CPointer< IRegister > CRegisterPtr
SmartPointer for IRegister interface pointer.
typedef CPointer< IEnumeration > CEnumerationPtr
SmartPointer for IEnumeration interface pointer.
typedef CPointer< IEnumEntry > CEnumEntryPtr
SmartPointer for IEnumEntry interface pointer.
typedef CPointer< IPort > CPortPtr
SmartPointer for IPort interface pointer.
typedef CPointer< IPortReplay > CPortReplayPtr
SmartPointer for IPortReplay interface pointer.
typedef CPointer< IPortRecorder > CPortRecorderPtr
SmartPointer for IPortRecorder interface pointer.
typedef CPointer< IPortWriteList, IPortWriteList > CPortWriteListPtr
SmartPointer for IPortWriteList interface pointer.
typedef CPointer< IChunkPort > CChunkPortPtr
SmartPointer for IChunkPort interface pointer.
typedef CPointer< INodeMap, INodeMap > CNodeMapPtr
SmartPointer for INodeMap interface pointer.
typedef CPointer< IDeviceInfo, INodeMap > CDeviceInfoPtr
SmartPointer for IDeviceInfo interface pointer.
typedef CPointer< IUserData, INodeMap > CNodeMapUserDataPtr
SmartPointer for IUserData interface pointer.
typedef CPointer< IUserData > CNodeUserDataPtr
SmartPointer for IUserData interface pointer.
typedef CPointer< ISelector > CSelectorPtr
SmartPointer for ISelector interface pointer.
typedef CPointer< ICommand > CCommandPtr
SmartPointer for ICommand interface pointer.
typedef CPointer< IPortConstruct > CPortConstructPtr
SmartPointer for IPortConstruct interface pointer.
typedef enum GenApi::_ESign ESign
typedef enum GenApi::_EAccessMode EAccessMode
typedef enum GenApi::_EVisibility EVisibility
typedef enum GenApi::_ECachingMode ECachingMode
typedef enum GenApi::_ERepresentation ERepresentation
typedef enum GenApi::_EEndianess EEndianess
typedef enum GenApi::_ENameSpace ENameSpace
typedef enum GenApi::_EStandardNameSpace EStandardNameSpace
typedef enum GenApi::_EYesNo EYesNo
typedef GenICam::gcstring_vector StringList_t
typedef enum GenApi::_ESlope ESlope
typedef enum GenApi::_EXMLValidation EXMLValidation
typedef describing the different validity checks which can be performed on an XML file
typedef enum GenApi::_EDisplayNotation EDisplayNotation
typedef enum GenApi::_EInterfaceType EInterfaceType
typedef enum GenApi::_ELinkType ELinkType
typedef for link type
typedef enum GenApi::_EIncMode EIncMode
typedef enum GenApi::_EInputDirection EInputDirection
typedef enum GenApi::_EGenApiSchemaVersion EGenApiSchemaVersion
GenApi schema version.

Functions#

Name
bool IsReadable(EAccessMode AccessMode)
Tests if readable.
bool IsReadable(const IBase * p)
Checks if a node is readable.
bool IsReadable(const IBase & r)
Checks if a node is readable.
bool IsWritable(EAccessMode AccessMode)
Tests if writable.
bool IsWritable(const IBase * p)
Checks if a node is writable.
bool IsWritable(const IBase & r)
Checks if a node is writable.
bool IsImplemented(EAccessMode AccessMode)
Tests if implemented.
bool IsImplemented(const IBase * p)
Checks if a node is implemented.
bool IsImplemented(const IBase & r)
Checks if a node is implemented.
bool IsAvailable(EAccessMode AccessMode)
Tests if available.
bool IsAvailable(const IBase * p)
Checks if a node is available.
bool IsAvailable(const IBase & r)
Checks if a node is available.
EAccessMode Combine(EAccessMode Peter, EAccessMode Paul)
Computes which access mode the two guards allow together.
bool IsVisible(EVisibility Visibility, EVisibility MaxVisiblity)
Tests Visibility.
EVisibility Combine(EVisibility Peter, EVisibility Paul)
Computes which visibility the two guards allow together.
bool IsCacheable(ECachingMode CachingMode)
Tests Cacheability.
ECachingMode Combine(ECachingMode Peter, ECachingMode Paul)
Computes which CachingMode results from a combination.
template <class Function >
CNodeCallback *
make_NodeCallback(INode * pNode, Function function, ECallbackType CallbackType)
make a new callback object for C functions
template <class Function >
intptr_t
Register(INode * pNode, Function f, ECallbackType CallbackType =cbPostInsideLock)
Register a C-function as a callback.
template <class Client ,class Member >
CNodeCallback *
make_NodeCallback(INode * pNode, Client & client, Member member, ECallbackType CallbackType)
make a new callback object for member functions
template <class Client ,class Member >
intptr_t
Register(INode * pNode, Client & c, Member m, ECallbackType CallbackType =cbPostInsideLock)
Register a C++-member function a callback.
void Deregister(GenApi::CallbackHandleType pCallbackInfo)
Unregistering callback by handle.
GenICam::gcstring GetInterfaceName(IBase * pBase)
template <class T ,class B >
bool
IsReadable(const CPointer< T, B > & ptr)
Checks if a node is readable.
template <class T ,class B >
bool
IsWritable(const CPointer< T, B > & ptr)
Checks if a node is Writable.
template <class T ,class B >
bool
IsImplemented(const CPointer< T, B > & ptr)
Checks if a node is Implemented.
template <class T ,class B >
bool
IsAvailable(const CPointer< T, B > & ptr)
Checks if a node is Available.

Detailed Description#

Contains definitions of the types of GenICam GenApi modules.

GenApi is an alias for a more complex namespace name, e.g. GenApi_3_1_Basler_pylon. Throughout this documentation, only the alias GenApi is used. For programming, we also recommend to only use the alias.

Forward declarations can be defined as follows:

#include <GenApi/GenApiNamespace.h>

//...

namespace GENAPI_NAMESPACE
{
    interface INodeMap;
}

Alternatively, the GenICam library provides a header file that contains most of the forward declarations:

#include <GenICamFwd.h>

Types Documentation#

enum _ECallbackType#

Enumerator Value Description
cbPostInsideLock 1
cbPostOutsideLock 2 > callback is fired on leaving the tree inside the lock-guarded area > >

the type of callback

enum _ESign#

Enumerator Value Description
Signed Integer is signed.
Unsigned Integer is unsigned.
_UndefinedSign Object is not yet initialized.

signed or unsigned integers

enum _EAccessMode#

Enumerator Value Description
NI Not implemented.
NA Not available.
WO Write Only.
RO Read Only.
RW Read and Write.
_UndefinedAccesMode Object is not yet initialized.
_CycleDetectAccesMode used internally for AccessMode cycle detection

access mode of a node

enum _EVisibility#

Enumerator Value Description
Beginner 0 Always visible.
Expert 1 Visible for experts or Gurus.
Guru 2 Visible for Gurus.
Invisible 3 Not Visible.
_UndefinedVisibility 99 Object is not yet initialized.

recommended visibility of a node

enum _ECachingMode#

Enumerator Value Description
NoCache Do not use cache.
WriteThrough Write to cache and register.
WriteAround Write to register, write to cache on read.
_UndefinedCachingMode Not yet initialized.

caching mode of a register

enum _ERepresentation#

Enumerator Value Description
Linear Slider with linear behavior.
Logarithmic Slider with logarithmic behaviour.
Boolean Check box.
PureNumber Decimal number in an edit control.
HexNumber Hex number in an edit control.
IPV4Address IP-Address.
MACAddress MAC-Address.
_UndefinedRepresentation

recommended representation of a node value

enum _EEndianess#

Enumerator Value Description
BigEndian Register is big endian.
LittleEndian Register is little endian.
_UndefinedEndian Object is not yet initialized.

Endianess of a value in a register

enum _ENameSpace#

Enumerator Value Description
Custom name resides in custom namespace
Standard name resides in one of the standard namespaces
_UndefinedNameSpace Object is not yet initialized.

Defines if a node name is standard or custom

enum _EStandardNameSpace#

Enumerator Value Description
None name resides in custom namespace
GEV name resides in GigE Vision namespace
IIDC name resides in 1394 IIDC namespace
CL name resides in camera link namespace
USB name resides in USB namespace
_UndefinedStandardNameSpace Object is not yet initialized.

Defines from which standard namespace a node name comes from

enum _EYesNo#

Enumerator Value Description
Yes 1 yes
No 0 no
_UndefinedYesNo 2 Object is not yet initialized.

Defines the choices of a Yes/No alternatives

enum _ESlope#

Enumerator Value Description
Increasing strictly monotonous increasing
Decreasing strictly monotonous decreasing
Varying slope changes, e.g. at run-time
Automatic slope is determined automatically by probing the function
_UndefinedESlope Object is not yet initialized.

typedef for formula type

enum _EXMLValidation#

Enumerator Value Description
xvLoad 0x00000001L Creates a dummy node map.
xvCycles 0x00000002L checks for write and dependency cycles (implies xvLoad)
xvSFNC 0x00000004L checks for conformance with the standard feature naming convention (SFNC)
xvDefault 0x00000000L checks performed if nothing else is said
xvAll 0xffffffffL all possible checks
_UndefinedEXMLValidation 0x8000000L Object is not yet initialized.

typedef describing the different validity checks which can be performed on an XML file

The enum values for a bitfield of length uint32_t

enum _EDisplayNotation#

Enumerator Value Description
fnAutomatic the notation if either scientific or fixed depending on what is shorter
fnFixed the notation is fixed, e.g. 123.4
fnScientific the notation is scientific, e.g. 1.234e2
_UndefinedEDisplayNotation Object is not yet initialized.

typedef for float notation

enum _EInterfaceType#

Enumerator Value Description
intfIValue IValue interface.
intfIBase IBase interface.
intfIInteger IInteger interface.
intfIBoolean IBoolean interface.
intfICommand ICommand interface.
intfIFloat IFloat interface.
intfIString IString interface.
intfIRegister IRegister interface.
intfICategory ICategory interface.
intfIEnumeration IEnumeration interface.
intfIEnumEntry IEnumEntry interface.
intfIPort IPort interface.

typedef for interface type

enum _ELinkType#

Enumerator Value Description
ctParentNodes All nodes for which this node is at least an invalidating child.
ctReadingChildren All nodes which can be read from.
ctWritingChildren All nodes which can write a value further down the node stack.
ctInvalidatingChildren All directly connected nodes which invalidate this node.
ctDependingNodes All directly or indirectly connected nodes which are invalidated by this nodes (i.e. which are dependent on this node)
ctTerminalNodes All indirectly connected terminal nodes.
ctValueChangingChildren All child node used to compute the value.

typedef for link type

For details see GenICam Wiki : GenApi/SoftwareArchitecture/NodeDependencies

enum _EIncMode#

Enumerator Value Description
noIncrement
fixedIncrement
listIncrement

typedef for increment mode

enum _EInputDirection#

Enumerator Value Description
idFrom Indicates a swiss knife that it is used as worker for a converter computing FROM.
idTo Indicates a swiss knife that it is used as worker for a converter computing TO.
idNone SwissKnife is not used within a converter.

typedef for link type

enum _EGenApiSchemaVersion#

Enumerator Value Description
v1_0 1
v1_1 2
_Undefined -1

GenApi schema version.

typedef FeatureList_t#

typedef value_vector GenApi::FeatureList_t;

a list of feature references

typedef CBaseRef#

typedef CBaseRefT<IBase> GenApi::CBaseRef;

Reference to an IBase pointer

typedef CBooleanRef#

typedef CBooleanRefT<IBoolean> GenApi::CBooleanRef;

Reference to an IBoolean pointer

typedef CCategoryRef#

typedef CCategoryRefT<ICategory> GenApi::CCategoryRef;

Reference to an ICategory pointer

typedef CCommandRef#

typedef CCommandRefT<ICommand> GenApi::CCommandRef;

Reference to an ICommand pointer

typedef CEnumEntryRef#

typedef CEnumEntryRefT<IEnumEntry> GenApi::CEnumEntryRef;

Reference to an IEnumEntry pointer

typedef CFloatRef#

typedef CFloatRefT<IFloat> GenApi::CFloatRef;

Reference to an IFloat pointer

typedef CIntegerRef#

typedef CIntegerRefT<IInteger> GenApi::CIntegerRef;

Reference to an IInteger pointer

typedef NodeList_t#

typedef node_vector GenApi::NodeList_t;

a list of node references

typedef CallbackHandleType#

typedef intptr_t GenApi::CallbackHandleType;

the callback handle for nodes

typedef CPortRef#

typedef CPortRefT<IPort> GenApi::CPortRef;

Reference to an IEnumEntry pointer

typedef CRegisterRef#

typedef CRegisterRefT<IRegister> GenApi::CRegisterRef;

Reference to an IRegister pointer

typedef CSelectorRef#

typedef CSelectorRefT<ISelector> GenApi::CSelectorRef;

Reference to an ISelector pointer

typedef CStringRef#

typedef CStringRefT<IString> GenApi::CStringRef;

Reference to an IString pointer

typedef CValueRef#

typedef CValueRefT<IValue> GenApi::CValueRef;

Reference to an IValue pointer

typedef ECallbackType#

typedef enum GenApi::_ECallbackType  GenApi::ECallbackType;

the type of callback

typedef CBasePtr#

typedef CPointer<IBase> GenApi::CBasePtr;

SmartPointer for IBase interface pointer.

typedef CNodePtr#

typedef CPointer<INode> GenApi::CNodePtr;

SmartPointer for INode interface pointer.

typedef CValuePtr#

typedef CPointer<IValue> GenApi::CValuePtr;

SmartPointer for IValue interface pointer.

typedef CCategoryPtr#

typedef CPointer<ICategory> GenApi::CCategoryPtr;

SmartPointer for ICategory interface pointer.

typedef CBooleanPtr#

typedef CPointer<IBoolean> GenApi::CBooleanPtr;

SmartPointer for IBoolean interface pointer.

typedef CIntegerPtr#

typedef CPointer<IInteger> GenApi::CIntegerPtr;

SmartPointer for IInteger interface pointer.

typedef CStringPtr#

typedef CPointer<IString> GenApi::CStringPtr;

SmartPointer for IString interface pointer.

typedef CRegisterPtr#

typedef CPointer<IRegister> GenApi::CRegisterPtr;

SmartPointer for IRegister interface pointer.

typedef CEnumerationPtr#

typedef CPointer<IEnumeration> GenApi::CEnumerationPtr;

SmartPointer for IEnumeration interface pointer.

typedef CEnumEntryPtr#

typedef CPointer<IEnumEntry> GenApi::CEnumEntryPtr;

SmartPointer for IEnumEntry interface pointer.

typedef CPortPtr#

typedef CPointer<IPort> GenApi::CPortPtr;

SmartPointer for IPort interface pointer.

typedef CPortReplayPtr#

typedef CPointer<IPortReplay> GenApi::CPortReplayPtr;

SmartPointer for IPortReplay interface pointer.

typedef CPortRecorderPtr#

typedef CPointer<IPortRecorder> GenApi::CPortRecorderPtr;

SmartPointer for IPortRecorder interface pointer.

typedef CPortWriteListPtr#

typedef CPointer<IPortWriteList, IPortWriteList> GenApi::CPortWriteListPtr;

SmartPointer for IPortWriteList interface pointer.

typedef CChunkPortPtr#

typedef CPointer<IChunkPort> GenApi::CChunkPortPtr;

SmartPointer for IChunkPort interface pointer.

typedef CNodeMapPtr#

typedef CPointer<INodeMap, INodeMap> GenApi::CNodeMapPtr;

SmartPointer for INodeMap interface pointer.

typedef CDeviceInfoPtr#

typedef CPointer<IDeviceInfo, INodeMap> GenApi::CDeviceInfoPtr;

SmartPointer for IDeviceInfo interface pointer.

typedef CNodeMapUserDataPtr#

typedef CPointer<IUserData, INodeMap> GenApi::CNodeMapUserDataPtr;

SmartPointer for IUserData interface pointer.

typedef CNodeUserDataPtr#

typedef CPointer<IUserData> GenApi::CNodeUserDataPtr;

SmartPointer for IUserData interface pointer.

typedef CSelectorPtr#

typedef CPointer<ISelector> GenApi::CSelectorPtr;

SmartPointer for ISelector interface pointer.

typedef CCommandPtr#

typedef CPointer<ICommand> GenApi::CCommandPtr;

SmartPointer for ICommand interface pointer.

typedef CPortConstructPtr#

typedef CPointer<IPortConstruct> GenApi::CPortConstructPtr;

SmartPointer for IPortConstruct interface pointer.

typedef ESign#

typedef enum GenApi::_ESign  GenApi::ESign;

signed or unsigned integers

typedef EAccessMode#

typedef enum GenApi::_EAccessMode  GenApi::EAccessMode;

access mode of a node

typedef EVisibility#

typedef enum GenApi::_EVisibility  GenApi::EVisibility;

recommended visibility of a node

typedef ECachingMode#

typedef enum GenApi::_ECachingMode  GenApi::ECachingMode;

caching mode of a register

typedef ERepresentation#

typedef enum GenApi::_ERepresentation  GenApi::ERepresentation;

recommended representation of a node value

typedef EEndianess#

typedef enum GenApi::_EEndianess  GenApi::EEndianess;

Endianess of a value in a register

typedef ENameSpace#

typedef enum GenApi::_ENameSpace  GenApi::ENameSpace;

Defines if a node name is standard or custom

typedef EStandardNameSpace#

typedef enum GenApi::_EStandardNameSpace  GenApi::EStandardNameSpace;

Defines from which standard namespace a node name comes from

typedef EYesNo#

typedef enum GenApi::_EYesNo  GenApi::EYesNo;

Defines the choices of a Yes/No alternatives

typedef StringList_t#

typedef GenICam::gcstring_vector GenApi::StringList_t;

A list of strings

typedef ESlope#

typedef enum GenApi::_ESlope  GenApi::ESlope;

typedef for formula type

typedef EXMLValidation#

typedef enum GenApi::_EXMLValidation  GenApi::EXMLValidation;

typedef describing the different validity checks which can be performed on an XML file

The enum values for a bitfield of length uint32_t

typedef EDisplayNotation#

typedef enum GenApi::_EDisplayNotation  GenApi::EDisplayNotation;

typedef for float notation

typedef EInterfaceType#

typedef enum GenApi::_EInterfaceType  GenApi::EInterfaceType;

typedef for interface type

typedef ELinkType#

typedef enum GenApi::_ELinkType  GenApi::ELinkType;

typedef for link type

For details see GenICam Wiki : GenApi/SoftwareArchitecture/NodeDependencies

typedef EIncMode#

typedef enum GenApi::_EIncMode  GenApi::EIncMode;

typedef for increment mode

typedef EInputDirection#

typedef enum GenApi::_EInputDirection  GenApi::EInputDirection;

typedef for link type

typedef EGenApiSchemaVersion#

typedef enum GenApi::_EGenApiSchemaVersion  GenApi::EGenApiSchemaVersion;

GenApi schema version.

Functions Documentation#

function IsReadable#

inline bool IsReadable(
    EAccessMode AccessMode
)

Tests if readable.

function IsReadable#

inline bool IsReadable(
    const IBase * p
)

Checks if a node is readable.

function IsReadable#

inline bool IsReadable(
    const IBase & r
)

Checks if a node is readable.

function IsWritable#

inline bool IsWritable(
    EAccessMode AccessMode
)

Tests if writable.

function IsWritable#

inline bool IsWritable(
    const IBase * p
)

Checks if a node is writable.

function IsWritable#

inline bool IsWritable(
    const IBase & r
)

Checks if a node is writable.

function IsImplemented#

inline bool IsImplemented(
    EAccessMode AccessMode
)

Tests if implemented.

function IsImplemented#

inline bool IsImplemented(
    const IBase * p
)

Checks if a node is implemented.

function IsImplemented#

inline bool IsImplemented(
    const IBase & r
)

Checks if a node is implemented.

function IsAvailable#

inline bool IsAvailable(
    EAccessMode AccessMode
)

Tests if available.

function IsAvailable#

inline bool IsAvailable(
    const IBase * p
)

Checks if a node is available.

function IsAvailable#

inline bool IsAvailable(
    const IBase & r
)

Checks if a node is available.

function Combine#

inline EAccessMode Combine(
    EAccessMode Peter,
    EAccessMode Paul
)

Computes which access mode the two guards allow together.

function IsVisible#

inline bool IsVisible(
    EVisibility Visibility,
    EVisibility MaxVisiblity
)

Tests Visibility.

CAVE : this relys on the EVisibility enum's coding

function Combine#

inline EVisibility Combine(
    EVisibility Peter,
    EVisibility Paul
)

Computes which visibility the two guards allow together.

function IsCacheable#

inline bool IsCacheable(
    ECachingMode CachingMode
)

Tests Cacheability.

function Combine#

inline ECachingMode Combine(
    ECachingMode Peter,
    ECachingMode Paul
)

Computes which CachingMode results from a combination.

function make_NodeCallback#

template <class Function >
CNodeCallback * make_NodeCallback(
    INode * pNode,
    Function function,
    ECallbackType CallbackType
)

make a new callback object for C functions

function Register#

template <class Function >
intptr_t Register(
    INode * pNode,
    Function f,
    ECallbackType CallbackType =cbPostInsideLock
)

Register a C-function as a callback.

function make_NodeCallback#

template <class Client ,
class Member >
CNodeCallback * make_NodeCallback(
    INode * pNode,
    Client & client,
    Member member,
    ECallbackType CallbackType
)

make a new callback object for member functions

function Register#

template <class Client ,
class Member >
intptr_t Register(
    INode * pNode,
    Client & c,
    Member m,
    ECallbackType CallbackType =cbPostInsideLock
)

Register a C++-member function a callback.

function Deregister#

void Deregister(
    GenApi::CallbackHandleType pCallbackInfo
)

Unregistering callback by handle.

function GetInterfaceName#

inline GenICam::gcstring GetInterfaceName(
    IBase * pBase
)

Returns the name of the main interface as string DEPRECATED, use IBase::GetPrincipalInterfaceType() instead

function IsReadable#

template <class T ,
class B >
inline bool IsReadable(
    const CPointer< T, B > & ptr
)

Checks if a node is readable.

function IsWritable#

template <class T ,
class B >
inline bool IsWritable(
    const CPointer< T, B > & ptr
)

Checks if a node is Writable.

function IsImplemented#

template <class T ,
class B >
inline bool IsImplemented(
    const CPointer< T, B > & ptr
)

Checks if a node is Implemented.

function IsAvailable#

template <class T ,
class B >
inline bool IsAvailable(
    const CPointer< T, B > & ptr
)

Checks if a node is Available.