Skip to content
STAGING SERVER
DEVELOPMENT SERVER

IIntegerParameter Interface#

Interface class for integer parameters.

Syntax#

C#

public interface IIntegerParameter : IParameter

VB

Public Interface IIntegerParameter
    Inherits IParameter

The IIntegerParameter type exposes the following members.

Properties#

NameDescription
Public propertyAdvanced The advanced parameter settings, if available. (Inherited from IParameter.)
Public propertyFullName The full name of the parameter including path information. (Inherited from IParameter.)
Public propertyIsEmpty Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable. (Inherited from IParameter.)
Public propertyIsReadable Indicates if the parameter is readable. (Inherited from IParameter.)
Public propertyIsWritable Indicates if the parameter is writable. (Inherited from IParameter.)
Public propertyName The name of the parameter without path information. (Inherited from IParameter.)
 

Methods#

NameDescription
Public methodGetIncrement Gets the increment value of the current parameter.
Public methodGetMaximum Gets the maximum value of the current parameter.
Public methodGetMinimum Gets the minimum value of the current parameter.
Public methodGetValue Gets the current parameter value.
Public methodParseAndSetValue Parses the value as string and sets the value. (Inherited from IParameter.)
Public methodSetValue Sets the provided value.
Public methodToString The parameter value as a string. (Inherited from IParameter.)
 

Events#

NameDescription
Public eventParameterChanged This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed. (Inherited from IParameter.)
Public eventParameterValueChanged This event fires after the parameter value has changed. (Inherited from IParameter.)
 

Extension Methods#

NameDescription
Public Extension MethodGetValueOrDefault Gets the parameter value if the parameter is readable. Otherwise, returns the default value. (Defined by IIntegerParameterExtensions.)
Public Extension MethodGetValuePercentOfRange Returns the current value in percent of minimum/maximum range. (Defined by IIntegerParameterExtensions.)
Public Extension MethodSetToMaximum Sets the parameter value to the maximum possible value. (Defined by IIntegerParameterExtensions.)
Public Extension MethodSetToMinimum Sets the parameter value to the minimum possible value. (Defined by IIntegerParameterExtensions.)
Public Extension MethodSetValue Sets the provided value. The value is automatically corrected if needed. (Defined by IIntegerParameterExtensions.)
Public Extension MethodSetValuePercentOfRange Sets the provided value to a value within the range, using this formula (simplified): ((maxRange - minRange) * (percentOfRange / 100.0)) + minRange. The computed value is always corrected to the nearest valid value. (Defined by IIntegerParameterExtensions.)
Public Extension MethodTrySetToMaximum Sets the parameter value to the maximum possible value if the parameter is readable and writable. (Defined by IIntegerParameterExtensions.)
Public Extension MethodTrySetToMinimum Sets the parameter value to the minimum possible value if the parameter is readable and writable. (Defined by IIntegerParameterExtensions.)
Public Extension MethodTrySetValue(Int64)Overloaded.
Sets the value passed if the parameter is writable. The value must be in the valid range and the increment must be correct. (Defined by IIntegerParameterExtensions.)
Public Extension MethodTrySetValue(Int64, IntegerValueCorrection)Overloaded.
Sets the provided value if the parameter is writable and readable. The value is automatically corrected if needed. (Defined by IIntegerParameterExtensions.)
Public Extension MethodTrySetValuePercentOfRange If the parameter is writable and readable, the provided value in percentage of range (simplified): ((max - min) * (percentOfRange / 100.0)) + min is set. The computed value is always corrected to the nearest valid value. (Defined by IIntegerParameterExtensions.)
 

IIntegerParameter.GetIncrement Method#

Gets the increment value of the current parameter.

Syntax#

C#

long GetIncrement()

VB

Function GetIncrement As Long

Return Value#

Type: Int64
Returns the increment value of the current parameter.

Remarks#

Preconditions: The parameter must be readable.

Thread Safety: This method is synchronized with the source of the parameter collection, if any.

Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.

IIntegerParameter.GetMaximum Method#

Gets the maximum value of the current parameter.

Syntax#

C#

long GetMaximum()

VB

Function GetMaximum As Long

Return Value#

Type: Int64
Returns the maximum value of the current parameter.

Remarks#

Preconditions: The parameter must be readable.

Thread Safety: This method is synchronized with the source of the parameter collection, if any.

Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.

IIntegerParameter.GetMinimum Method#

Gets the minimum value of the current parameter.

Syntax#

C#

long GetMinimum()

VB

Function GetMinimum As Long

Return Value#

Type: Int64
Returns the minimum value of the current parameter.

Remarks#

Preconditions: The parameter must be readable.

Thread Safety: This method is synchronized with the source of the parameter collection, if any.

Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.

IIntegerParameter.GetValue Method#

Gets the current parameter value.

Syntax#

C#

long GetValue()

VB

Function GetValue As Long

Return Value#

Type: Int64
Returns the current parameter value.

Remarks#

Preconditions: The parameter must be readable.

Thread Safety: This method is synchronized with the source of the parameter collection, if any.

Error Safety: Can throw exceptions if the parameter is not readable or if reading the value fails.

IIntegerParameter.SetValue Method#

Sets the provided value.

Syntax#

C#

void SetValue(
    long value
)

VB

Sub SetValue ( 
    value As Long
)

Parameters#

 

value
Type: System.Int64
The value to set.

Remarks#

Preconditions:
 

  • The parameter must be writable.
  • The value passed must be >= GetMinimum().
  • The value passed must be <= GetMaximum().
  • The value passed must be aligned to the increment returned by GetIncrement().
  Thread Safety: This method is synchronized with the source of the parameter collection, if any.

Error Safety: Can throw exceptions if writing the value fails, if the value is out of bounds, if the alignment is not correct, or if the parameter is not writable.