Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.BslImmediateTriggerModeEnum Class#

Enables the Immediate Trigger mode. If this mode is enabled, exposure starts immediately after triggering, but changes to image parameters become effective with a short delay, i.e., after one or more images have been acquired.

Applies to: dart USB and pulse USB

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslImmediateTriggerModeEnum

Constructors#

 NameDescription
Public methodPLCamera.BslImmediateTriggerModeEnum Initializes a new instance of the PLCamera.BslImmediateTriggerModeEnum class
 

Properties#

 NameDescription
Public propertyName The full name of BslImmediateTriggerMode (Overrides ParameterListEnum.Name.)
Public propertyOff

The Immediate Trigger mode is disabled. This increases the exposure start delay, but changes to image parameters become effective immediately.

Applies to: dart USB and pulse USB

Public propertyOn

The Immediate Trigger mode is enabled. This reduces the exposure start delay.

Applies to: dart USB and pulse USB

 

Methods#

 NameDescription
Public methodToString The full name of BslImmediateTriggerMode (Overrides Object.ToString()()()().)
 

PLCamera.BslImmediateTriggerModeEnum.ToString Method#

The full name of BslImmediateTriggerMode

Return Value#

Type: String
Returns the full name of BslImmediateTriggerMode

PLCamera.BslImmediateTriggerModeEnum Constructor#

Initializes a new instance of the PLCamera.BslImmediateTriggerModeEnum class

PLCamera.BslImmediateTriggerModeEnum.Name Property#

The full name of BslImmediateTriggerMode

PLCamera.BslImmediateTriggerModeEnum.Off Property#

The Immediate Trigger mode is disabled. This increases the exposure start delay, but changes to image parameters become effective immediately.

Applies to: dart USB and pulse USB

PLCamera.BslImmediateTriggerModeEnum.On Property#

The Immediate Trigger mode is enabled. This reduces the exposure start delay.

Applies to: dart USB and pulse USB