PLCamera.ClTapGeometryEnum Class#
Applies to: CameraLink
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.ClTapGeometryEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.ClTapGeometryEnum | Initializes a new instance of the PLCamera.ClTapGeometryEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Geometry1X | The tap geometry is set to 1 zone in horizontal direction with one tap. Applies to: CameraLink |
![]() | Geometry1X_1Y | The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X_2YE | The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction. Applies to: CameraLink |
![]() | Geometry1X10 | The tap geometry is set to 1 zone in horizontal direction with ten taps. Applies to: CameraLink |
![]() | Geometry1X10_1Y | The tap geometry is set to 1 zone in horizontal direction with ten taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X2 | The tap geometry is set to 1 zone in horizontal direction with two taps. Applies to: CameraLink |
![]() | Geometry1X2_1Y | The tap geometry is set to 1 zone in horizontal direction with two taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X3 | The tap geometry is set to 1 zone in horizontal direction with three taps. Applies to: CameraLink |
![]() | Geometry1X3_1Y | The tap geometry is set to 1 zone in horizontal direction with three taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X4 | The tap geometry is set to 1 zone in horizontal direction with four taps. Applies to: CameraLink |
![]() | Geometry1X4_1Y | The tap geometry is set to 1 zone in horizontal direction with four taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X6 | The tap geometry is set to 1 zone in horizontal direction with six taps. Applies to: CameraLink |
![]() | Geometry1X6_1Y | The tap geometry is set to 1 zone in horizontal direction with six taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Geometry1X8 | The tap geometry is set to 1 zone in horizontal direction with eight taps. Applies to: CameraLink |
![]() | Geometry1X8_1Y | The tap geometry is set to 1 zone in horizontal direction with eight taps and 1 zone in vertical direction with 1 tap. Applies to: CameraLink |
![]() | Name | The full name of ClTapGeometry (Overrides ParameterListEnum.Name.) |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of ClTapGeometry (Overrides Object.ToString()()()().) |
PLCamera.ClTapGeometryEnum.ToString Method#
The full name of ClTapGeometry
Return Value#
Type: String
Returns the full name of ClTapGeometry
PLCamera.ClTapGeometryEnum Constructor#
Initializes a new instance of the PLCamera.ClTapGeometryEnum class
PLCamera.ClTapGeometryEnum.Geometry1X Property#
The tap geometry is set to 1 zone in horizontal direction with one tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X10 Property#
The tap geometry is set to 1 zone in horizontal direction with ten taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X10_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with ten taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X2 Property#
The tap geometry is set to 1 zone in horizontal direction with two taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X2_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with two taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X3 Property#
The tap geometry is set to 1 zone in horizontal direction with three taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X3_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with three taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X4 Property#
The tap geometry is set to 1 zone in horizontal direction with four taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X4_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with four taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X6 Property#
The tap geometry is set to 1 zone in horizontal direction with six taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X6_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with six taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X8 Property#
The tap geometry is set to 1 zone in horizontal direction with eight taps.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X8_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with eight taps and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Geometry1X_2YE Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction.
Applies to: CameraLink
PLCamera.ClTapGeometryEnum.Name Property#
The full name of ClTapGeometry