PLCamera.CxpSendReceiveSelectorEnum Class#
Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP
Visibility: Expert
Selected by: CxpConnectionSelector
Selecting Parameters: CxpConnectionTestPacketCount
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpSendReceiveSelectorEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.CxpSendReceiveSelectorEnum | Initializes a new instance of the PLCamera.CxpSendReceiveSelectorEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Name | The full name of CxpSendReceiveSelector (Overrides ParameterListEnum.Name.) |
![]() | Receive | The receive features can be configured. Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | Send | The send features can be configured. Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of CxpSendReceiveSelector (Overrides Object.ToString()()()().) |
PLCamera.CxpSendReceiveSelectorEnum.ToString Method#
The full name of CxpSendReceiveSelector
Return Value#
Type: String
Returns the full name of CxpSendReceiveSelector
PLCamera.CxpSendReceiveSelectorEnum Constructor#
Initializes a new instance of the PLCamera.CxpSendReceiveSelectorEnum class
PLCamera.CxpSendReceiveSelectorEnum.Name Property#
The full name of CxpSendReceiveSelector
PLCamera.CxpSendReceiveSelectorEnum.Receive Property#
The receive features can be configured.
Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpSendReceiveSelectorEnum.Send Property#
The send features can be configured.
Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP