PLCamera.DeviceTapGeometryEnum Class#
Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.DeviceTapGeometryEnum
Constructors#
| Name | Description | |
|---|---|---|
![]()  | PLCamera.DeviceTapGeometryEnum | Initializes a new instance of the PLCamera.DeviceTapGeometryEnum class | 
Properties#
| Name | Description | |
|---|---|---|
![]()  | Geometry_1X_1Y |   The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap. Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP  | 
![]()  | Geometry_1X_2YE |   The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction. Applies to: boost V CoaXPress  | 
![]()  | Name | The full name of DeviceTapGeometry (Overrides ParameterListEnum.Name.) | 
Methods#
| Name | Description | |
|---|---|---|
![]()  | ToString | The full name of DeviceTapGeometry (Overrides Object.ToString()()()().) | 
PLCamera.DeviceTapGeometryEnum.ToString Method#
The full name of DeviceTapGeometry
Return Value#
Type: String
Returns the full name of DeviceTapGeometry
PLCamera.DeviceTapGeometryEnum Constructor#
Initializes a new instance of the PLCamera.DeviceTapGeometryEnum class
PLCamera.DeviceTapGeometryEnum.Geometry_1X_1Y Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 1 zone in vertical direction with 1 tap.
Applies to: ace 2 CXP, boost CoaXPress, boost V CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.DeviceTapGeometryEnum.Geometry_1X_2YE Property#
The tap geometry is set to 1 zone in horizontal direction with one tap and 2 zones in vertical direction with 1 tap with end extraction.
Applies to: boost V CoaXPress
PLCamera.DeviceTapGeometryEnum.Name Property#
The full name of DeviceTapGeometry