Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.RemoveParameterLimitSelectorEnum Class#

Sets the parameter whose factory limits can be removed. The factory limits can be removed using the Remove Limits parameter.

Applies to: ace USB

Visibility: Guru

Selecting Parameters: RemoveParameterLimit

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.RemoveParameterLimitSelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.RemoveParameterLimitSelectorEnum Initializes a new instance of the PLCamera.RemoveParameterLimitSelectorEnum class
 

Properties#

 NameDescription
Public propertyAutoTargetValue

The factory limits of the AutoTargetValue parameter can be removed.

Applies to: ace USB

Public propertyBlackLevel

The factory limits of the BlackLevel parameter can be removed.

Applies to: ace USB

Public propertyExposureOverhead

The factory limits of the ExposureOverhead parameter can be removed.

Applies to: ace USB

Public propertyExposureTime

The factory limits of the Exposure Time parameter can be removed.

Applies to: ace USB

Public propertyGain

The factory limits of the Gain parameter can be removed.

Applies to: ace USB

Public propertyName The full name of RemoveParameterLimitSelector (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of RemoveParameterLimitSelector (Overrides Object.ToString()()()().)
 

PLCamera.RemoveParameterLimitSelectorEnum.ToString Method#

The full name of RemoveParameterLimitSelector

Return Value#

Type: String
Returns the full name of RemoveParameterLimitSelector

PLCamera.RemoveParameterLimitSelectorEnum Constructor#

Initializes a new instance of the PLCamera.RemoveParameterLimitSelectorEnum class

PLCamera.RemoveParameterLimitSelectorEnum.AutoTargetValue Property#

The factory limits of the AutoTargetValue parameter can be removed.

Applies to: ace USB

PLCamera.RemoveParameterLimitSelectorEnum.BlackLevel Property#

The factory limits of the BlackLevel parameter can be removed.

Applies to: ace USB

PLCamera.RemoveParameterLimitSelectorEnum.ExposureOverhead Property#

The factory limits of the ExposureOverhead parameter can be removed.

Applies to: ace USB

PLCamera.RemoveParameterLimitSelectorEnum.ExposureTime Property#

The factory limits of the Exposure Time parameter can be removed.

Applies to: ace USB

PLCamera.RemoveParameterLimitSelectorEnum.Gain Property#

The factory limits of the Gain parameter can be removed.

Applies to: ace USB

PLCamera.RemoveParameterLimitSelectorEnum.Name Property#

The full name of RemoveParameterLimitSelector