PLChunkData Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.PLChunkData
Properties#
| Name | Description | |
|---|---|---|
![]() ![]() | BslChunkAutoBrightnessStatus | Indicates the status of the target brightness adjustments performed by the Exposure Auto and Gain Auto auto functions. Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert |
![]() ![]() | BslChunkEncoderValue | Value of encoders position counter. Applies to: racer 2S 5GigE and racer 2S GigE Visibility: Expert |
![]() ![]() | BslChunkTimestampSelector | Sets which information should be included in the Chunk Timestamp Value chunk. Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert Selecting Parameters: BslChunkTimestampValue |
![]() ![]() | BslChunkTimestampValue | Value of the timestamp when the image was acquired. Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert Selected by: BslChunkTimestampSelector |
![]() ![]() | ChunkBslLineRatio | Returns the exposure ratio of the selected output line. Applies to: Stereo ace Visibility: Expert Selected by: ChunkLineSelector |
![]() ![]() | ChunkBslMaxDepth | Maximum depth that was used. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkBslMinDepth | Minimum depth that was used. This can be higher than anticipated due to camera or memory requirements. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkBslNoise | Returns the noise of the image. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkBslReducedDepthRange | Signals if the depth range had to be reduced due to memory limits. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkComponentID | Returns the component of the payload image. This can be used to identify the image component of a generic part in a multi-part transfer. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkComponentIDValue | Returns a unique Identifier value that corresponds to the selected chunk component. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkComponents | Returns the bitmask of components contained in this block. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkComponentSelector | Selects the Component from which to retreive data from. Applies to: Stereo ace Visibility: Expert Selecting Parameters: ChunkComponentID, ChunkComponentIDValue, ChunkDecimationHorizontal, ChunkDecimationVertical, ChunkHeight, ChunkOffsetX, ChunkOffsetY, ChunkPartIndex, ChunkPixelFormat, ChunkScan3dFocalLength, ChunkScan3dPrincipalPointU, ChunkScan3dPrincipalPointV, ChunkWidth |
![]() ![]() | ChunkCounterSelector | Sets which counter to retrieve chunk data from. Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert Selecting Parameters: ChunkCounterValue |
![]() ![]() | ChunkCounterValue | Value of the selected chunk counter. Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkCounterSelector |
![]() ![]() | ChunkDecimationHorizontal | Horizontal sub-sampling of the image. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkDecimationVertical | Vertical sub-sampling of the image. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkDynamicRangeMax | Maximum possible pixel value in the acquired image. Applies to: ace 2 GigE and ace GigE Visibility: Beginner |
![]() ![]() | ChunkDynamicRangeMin | Minimum possible pixel value in the acquired image. Applies to: ace 2 GigE and ace GigE Visibility: Beginner |
![]() ![]() | ChunkExposureTime | Exposure time used to acquire the image. Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkExposureTimeSelector |
![]() ![]() | ChunkExposureTimeSelector | Sets which exposure time to retrieve chunk data from. Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert Selecting Parameters: ChunkExposureTime |
![]() ![]() | ChunkFramecounter | Value of the Frame counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkFrameID | Unique identifier of the current frame. The frame ID starts at 0 and keeps incrementing by 1 for each exposed image until the camera is powered off. The maximum value is 2^48. Applies to: Stereo ace, ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert |
![]() ![]() | ChunkFramesPerTriggerCounter | Value of the Frames per Trigger counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkFrameTriggerCounter | Value of the Frame Trigger counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkFrameTriggerIgnoredCounter | Value of the Frame Trigger Ignored counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkGain | Gain used during image acquisition. Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkGainSelector |
![]() ![]() | ChunkGainAll | Gain All value of the acquired image. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkGainSelector | Sets which gain channel to retrieve chunk data from. Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Expert Selecting Parameters: ChunkGain |
![]() ![]() | ChunkHeight | AOI height of the acquired image. Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkComponentSelector |
![]() ![]() | ChunkInputStatusAtLineTriggerBitsPerLine | Number of bits per line used for the Input Status At Line Trigger parameter. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkInputStatusAtLineTriggerIndex | Index number used for the Input Status At Line Trigger parameter. The index number can be used to get the state of the camera's input lines when a specific line was acquired. For example, if you want to know the state of the camera's input lines when line 30 was acquired, set the index to 30, then retrieve the value of Status Index parameter. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkInputStatusAtLineTriggerValue | Value indicating the status of the camera's input lines when a specific line was acquired. The information is stored in a 4-bit value (bit 0 = input line 1 state, bit 1 = input line 2 state etc.). For more information, see the Status Index parameter documentation. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkLineSelector | Selects the output for which to read the LineSource. Applies to: Stereo ace Visibility: Expert Selecting Parameters: ChunkBslLineRatio, ChunkLineSource, ChunkLineStatus |
![]() ![]() | ChunkLineSource | Line source for selected line. Applies to: Stereo ace Visibility: Expert Selected by: ChunkLineSelector |
![]() ![]() | ChunkLineStatus | Returns the current status of the selected input or output Line. Applies to: Stereo ace Visibility: Expert Selected by: ChunkLineSelector |
![]() ![]() | ChunkLineStatusAll | Bit field that indicates the status of all of the camera's input and output lines when the image was acquired. Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Beginner |
![]() ![]() | ChunkLineTriggerCounter | Value of the Line Trigger counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkLineTriggerEndToEndCounter | Value of the Line Trigger End to End counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkLineTriggerIgnoredCounter | Value of the Line Trigger Ignored counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkOffsetX | X offset of the AOI of the acquired image. Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkComponentSelector |
![]() ![]() | ChunkOffsetY | Y offset of the AOI of the acquired image. Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkComponentSelector |
![]() ![]() | ChunkPartIndex | Returns index of the image part in this block depending on selected component. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkPayloadCRC16 | CRC checksum of the acquired image. The checksum is calculated using all of the image data and all of the appended chunks except for the checksum itself. Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE Visibility: Beginner |
![]() ![]() | ChunkPixelDynamicRangeMax | Maximum possible pixel value in the acquired image. Applies to: ace 2 GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Expert |
![]() ![]() | ChunkPixelDynamicRangeMin | Minimum possible pixel value in the acquired image. Applies to: ace 2 GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Expert |
![]() ![]() | ChunkPixelFormat | Indicates the pixel format of the acquired image. Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkComponentSelector |
![]() ![]() | ChunkScan3dBaseline | Baseline of the stereo cameras in m. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkScan3dCoordinateOffset | Returns the offset when transforming a pixel from relative coordinates to world coordinates. Applies to: Stereo ace Visibility: Expert Selected by: ChunkScan3dCoordinateSelector |
![]() ![]() | ChunkScan3dCoordinateScale | Returns the scale factor when transforming a pixel from relative coordinates to world coordinates. Applies to: Stereo ace Visibility: Expert Selected by: ChunkScan3dCoordinateSelector |
![]() ![]() | ChunkScan3dCoordinateSelector | Selects which Coordinate to retrieve data from. Applies to: Stereo ace Visibility: Expert Selecting Parameters: ChunkScan3dCoordinateOffset, ChunkScan3dCoordinateScale, ChunkScan3dInvalidDataFlag, ChunkScan3dInvalidDataValue |
![]() ![]() | ChunkScan3dDistanceUnit | Returns the Distance Unit of the payload image. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkScan3dFocalLength | Focal length of the camera in pixels. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkScan3dInvalidDataFlag | Returns if a specific non-valid data flag is used in the payload image. Applies to: Stereo ace Visibility: Expert Selected by: ChunkScan3dCoordinateSelector |
![]() ![]() | ChunkScan3dInvalidDataValue | Returns the value which identifies a non-valid pixel. Applies to: Stereo ace Visibility: Expert Selected by: ChunkScan3dCoordinateSelector |
![]() ![]() | ChunkScan3dOutputMode | Returns the Calibrated Mode of the payload image. Applies to: Stereo ace Visibility: Expert |
![]() ![]() | ChunkScan3dPrincipalPointU | Horizontal position of the principal point. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkScan3dPrincipalPointV | Vertical position of the principal point. Applies to: Stereo ace Visibility: Expert Selected by: ChunkComponentSelector |
![]() ![]() | ChunkSequencerSetActive | Index of the active sequencer set. Applies to: ace 2 GigE, ace 2 USB and ace USB Visibility: Beginner |
![]() ![]() | ChunkSequenceSetIndex | Sequence set index number related to the acquired image. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkShaftEncoderCounter | Value of the Shaft Encoder counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkStride | Number of bytes of data between the beginning of one line in the acquired image and the beginning of the next line in the acquired image. Applies to: ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner |
![]() ![]() | ChunkTimestamp | Value of the timestamp when the image was acquired. Applies to: Stereo ace, ace GigE and ace USB Visibility: Beginner |
![]() ![]() | ChunkTriggerinputcounter | Value of the Trigger Input counter when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkVirtLineStatusAll | Status of all of the camera's virtual input and output lines when the image was acquired. Applies to: ace GigE Visibility: Beginner |
![]() ![]() | ChunkWidth | Width of the AOI of the acquired image. Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE Visibility: Beginner Selected by: ChunkComponentSelector |
PLChunkData.BslChunkAutoBrightnessStatus Property#
Indicates the status of the target brightness adjustments performed by the Exposure Auto and Gain Auto auto functions.
Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
PLChunkData.BslChunkEncoderValue Property#
Value of encoders position counter.
Applies to: racer 2S 5GigE and racer 2S GigE
Visibility: Expert
PLChunkData.BslChunkTimestampSelector Property#
Sets which information should be included in the Chunk Timestamp Value chunk.
Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
Selecting Parameters: BslChunkTimestampValue
PLChunkData.BslChunkTimestampValue Property#
Value of the timestamp when the image was acquired.
Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
Selected by: BslChunkTimestampSelector
PLChunkData.ChunkBslLineRatio Property#
Returns the exposure ratio of the selected output line.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkLineSelector
PLChunkData.ChunkBslMaxDepth Property#
Maximum depth that was used.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkBslMinDepth Property#
Minimum depth that was used. This can be higher than anticipated due to camera or memory requirements.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkBslNoise Property#
Returns the noise of the image.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkBslReducedDepthRange Property#
Signals if the depth range had to be reduced due to memory limits.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkComponentID Property#
Returns the component of the payload image. This can be used to identify the image component of a generic part in a multi-part transfer.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkComponentIDValue Property#
Returns a unique Identifier value that corresponds to the selected chunk component.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkComponents Property#
Returns the bitmask of components contained in this block.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkComponentSelector Property#
Selects the Component from which to retreive data from.
Applies to: Stereo ace
Visibility: Expert
Selecting Parameters: ChunkComponentID, ChunkComponentIDValue, ChunkDecimationHorizontal, ChunkDecimationVertical, ChunkHeight, ChunkOffsetX, ChunkOffsetY, ChunkPartIndex, ChunkPixelFormat, ChunkScan3dFocalLength, ChunkScan3dPrincipalPointU, ChunkScan3dPrincipalPointV, ChunkWidth
PLChunkData.ChunkCounterSelector Property#
Sets which counter to retrieve chunk data from.
Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
Selecting Parameters: ChunkCounterValue
PLChunkData.ChunkCounterValue Property#
Value of the selected chunk counter.
Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkCounterSelector
PLChunkData.ChunkDecimationHorizontal Property#
Horizontal sub-sampling of the image.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkDecimationVertical Property#
Vertical sub-sampling of the image.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkDynamicRangeMax Property#
Maximum possible pixel value in the acquired image.
Applies to: ace 2 GigE and ace GigE
Visibility: Beginner
PLChunkData.ChunkDynamicRangeMin Property#
Minimum possible pixel value in the acquired image.
Applies to: ace 2 GigE and ace GigE
Visibility: Beginner
PLChunkData.ChunkExposureTime Property#
Exposure time used to acquire the image.
Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkExposureTimeSelector
PLChunkData.ChunkExposureTimeSelector Property#
Sets which exposure time to retrieve chunk data from.
Applies to: ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
Selecting Parameters: ChunkExposureTime
PLChunkData.ChunkFramecounter Property#
Value of the Frame counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkFrameID Property#
Unique identifier of the current frame. The frame ID starts at 0 and keeps incrementing by 1 for each exposed image until the camera is powered off. The maximum value is 2^48.
Applies to: Stereo ace, ace 2 GigE, ace 2 USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
PLChunkData.ChunkFramesPerTriggerCounter Property#
Value of the Frames per Trigger counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkFrameTriggerCounter Property#
Value of the Frame Trigger counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkFrameTriggerIgnoredCounter Property#
Value of the Frame Trigger Ignored counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkGain Property#
Gain used during image acquisition.
Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkGainSelector
PLChunkData.ChunkGainAll Property#
Gain All value of the acquired image.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkGainSelector Property#
Sets which gain channel to retrieve chunk data from.
Applies to: ace 2 GigE, ace 2 USB, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
Selecting Parameters: ChunkGain
PLChunkData.ChunkHeight Property#
AOI height of the acquired image.
Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkComponentSelector
PLChunkData.ChunkInputStatusAtLineTriggerBitsPerLine Property#
Number of bits per line used for the Input Status At Line Trigger parameter.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkInputStatusAtLineTriggerIndex Property#
Index number used for the Input Status At Line Trigger parameter. The index number can be used to get the state of the camera's input lines when a specific line was acquired. For example, if you want to know the state of the camera's input lines when line 30 was acquired, set the index to 30, then retrieve the value of Status Index parameter.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkInputStatusAtLineTriggerValue Property#
Value indicating the status of the camera's input lines when a specific line was acquired. The information is stored in a 4-bit value (bit 0 = input line 1 state, bit 1 = input line 2 state etc.). For more information, see the Status Index parameter documentation.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkLineSelector Property#
Selects the output for which to read the LineSource.
Applies to: Stereo ace
Visibility: Expert
Selecting Parameters: ChunkBslLineRatio, ChunkLineSource, ChunkLineStatus
PLChunkData.ChunkLineSource Property#
Line source for selected line.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkLineSelector
PLChunkData.ChunkLineStatus Property#
Returns the current status of the selected input or output Line.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkLineSelector
PLChunkData.ChunkLineStatusAll Property#
Bit field that indicates the status of all of the camera's input and output lines when the image was acquired.
Applies to: Stereo ace, ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
PLChunkData.ChunkLineTriggerCounter Property#
Value of the Line Trigger counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkLineTriggerEndToEndCounter Property#
Value of the Line Trigger End to End counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkLineTriggerIgnoredCounter Property#
Value of the Line Trigger Ignored counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkOffsetX Property#
X offset of the AOI of the acquired image.
Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkComponentSelector
PLChunkData.ChunkOffsetY Property#
Y offset of the AOI of the acquired image.
Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkComponentSelector
PLChunkData.ChunkPartIndex Property#
Returns index of the image part in this block depending on selected component.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkPayloadCRC16 Property#
CRC checksum of the acquired image. The checksum is calculated using all of the image data and all of the appended chunks except for the checksum itself.
Applies to: ace 2 GigE, ace 2 USB, ace GigE, ace USB, dart GigE, dart USB, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
PLChunkData.ChunkPixelDynamicRangeMax Property#
Maximum possible pixel value in the acquired image.
Applies to: ace 2 GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
PLChunkData.ChunkPixelDynamicRangeMin Property#
Minimum possible pixel value in the acquired image.
Applies to: ace 2 GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Expert
PLChunkData.ChunkPixelFormat Property#
Indicates the pixel format of the acquired image.
Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkComponentSelector
PLChunkData.ChunkScan3dBaseline Property#
Baseline of the stereo cameras in m.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkScan3dCoordinateOffset Property#
Returns the offset when transforming a pixel from relative coordinates to world coordinates.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkScan3dCoordinateSelector
PLChunkData.ChunkScan3dCoordinateScale Property#
Returns the scale factor when transforming a pixel from relative coordinates to world coordinates.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkScan3dCoordinateSelector
PLChunkData.ChunkScan3dCoordinateSelector Property#
Selects which Coordinate to retrieve data from.
Applies to: Stereo ace
Visibility: Expert
Selecting Parameters: ChunkScan3dCoordinateOffset, ChunkScan3dCoordinateScale, ChunkScan3dInvalidDataFlag, ChunkScan3dInvalidDataValue
PLChunkData.ChunkScan3dDistanceUnit Property#
Returns the Distance Unit of the payload image.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkScan3dFocalLength Property#
Focal length of the camera in pixels.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkScan3dInvalidDataFlag Property#
Returns if a specific non-valid data flag is used in the payload image.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkScan3dCoordinateSelector
PLChunkData.ChunkScan3dInvalidDataValue Property#
Returns the value which identifies a non-valid pixel.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkScan3dCoordinateSelector
PLChunkData.ChunkScan3dOutputMode Property#
Returns the Calibrated Mode of the payload image.
Applies to: Stereo ace
Visibility: Expert
PLChunkData.ChunkScan3dPrincipalPointU Property#
Horizontal position of the principal point.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkScan3dPrincipalPointV Property#
Vertical position of the principal point.
Applies to: Stereo ace
Visibility: Expert
Selected by: ChunkComponentSelector
PLChunkData.ChunkSequencerSetActive Property#
Index of the active sequencer set.
Applies to: ace 2 GigE, ace 2 USB and ace USB
Visibility: Beginner
PLChunkData.ChunkSequenceSetIndex Property#
Sequence set index number related to the acquired image.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkShaftEncoderCounter Property#
Value of the Shaft Encoder counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkStride Property#
Number of bytes of data between the beginning of one line in the acquired image and the beginning of the next line in the acquired image.
Applies to: ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
PLChunkData.ChunkTimestamp Property#
Value of the timestamp when the image was acquired.
Applies to: Stereo ace, ace GigE and ace USB
Visibility: Beginner
PLChunkData.ChunkTriggerinputcounter Property#
Value of the Trigger Input counter when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkVirtLineStatusAll Property#
Status of all of the camera's virtual input and output lines when the image was acquired.
Applies to: ace GigE
Visibility: Beginner
PLChunkData.ChunkWidth Property#
Width of the AOI of the acquired image.
Applies to: Stereo ace, ace 2 GigE, ace GigE, dart GigE, racer 2S 5GigE and racer 2S GigE
Visibility: Beginner
Selected by: ChunkComponentSelector