PLEventGrabber.StatusEnum Class#
Applies to: GigE
Visibility: Guru
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLEventGrabber.StatusEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLEventGrabber.StatusEnum | Initializes a new instance of the PLEventGrabber.StatusEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Closed | The low level event grabber is closed. Applies to: GigE |
![]() | Name | The full name of Status (Overrides ParameterListEnum.Name.) |
![]() | Open | The low level event grabber is open. Applies to: GigE |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of Status (Overrides Object.ToString()()()().) |
PLEventGrabber.StatusEnum.ToString Method#
The full name of Status
Return Value#
Type: String
Returns the full name of Status
PLEventGrabber.StatusEnum Constructor#
Initializes a new instance of the PLEventGrabber.StatusEnum class
PLEventGrabber.StatusEnum.Closed Property#
The low level event grabber is closed.
Applies to: GigE
PLEventGrabber.StatusEnum.Name Property#
The full name of Status
PLEventGrabber.StatusEnum.Open Property#
The low level event grabber is open.
Applies to: GigE