PLTransportLayer.LineTriggerModeEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.LineTriggerModeEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLTransportLayer.LineTriggerModeEnum | Initializes a new instance of the PLTransportLayer.LineTriggerModeEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | AsyncExternalTrigger | Trigger mode is set to Async External Trigger. Applies to: CoaXPress |
![]() | AsyncGatedTrigger | Trigger mode is set to Async Gated Trigger. Applies to: CoaXPress |
![]() | GrabberControlled | Line trigger mode is controlled by the grabber Applies to: CoaXPress |
![]() | GrabberControlledGated | Trigger mode is controlled by the grabber in gated mode. Applies to: CoaXPress |
![]() | Name | The full name of LineTriggerMode (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of LineTriggerMode (Overrides Object.ToString()()()().) |
PLTransportLayer.LineTriggerModeEnum.ToString Method#
The full name of LineTriggerMode
Return Value#
Type: String
Returns the full name of LineTriggerMode
PLTransportLayer.LineTriggerModeEnum Constructor#
Initializes a new instance of the PLTransportLayer.LineTriggerModeEnum class
PLTransportLayer.LineTriggerModeEnum.AsyncExternalTrigger Property#
Trigger mode is set to Async External Trigger.
Applies to: CoaXPress
PLTransportLayer.LineTriggerModeEnum.AsyncGatedTrigger Property#
Trigger mode is set to Async Gated Trigger.
Applies to: CoaXPress
PLTransportLayer.LineTriggerModeEnum.GrabberControlled Property#
Line trigger mode is controlled by the grabber
Applies to: CoaXPress
PLTransportLayer.LineTriggerModeEnum.GrabberControlledGated Property#
Trigger mode is controlled by the grabber in gated mode.
Applies to: CoaXPress
PLTransportLayer.LineTriggerModeEnum.Name Property#
The full name of LineTriggerMode